Power Amplifier (PA) Utility#
RAIL PA Utility#
This optional software component can be enabled to include default functionality related to PA configuration.
When using a Silicon Labs-developed board, the configuration options for this software component are set up automatically based on the selected board. When using a custom board, manually configure the configuration options.
Configuration Options#
The following configuration options can be changed:
PA Configuration
Initial PA power
PA ramp time
PA ramp time is a hardware approximation aimed at being as close to the desired ramp time as possible without going over the specified time.
Milli-volts provided to the PA supply pin (PA_VDD)
2.4 GHz PA selection (for applicable devices)
Sub-1 GHz PA selection (for applicable devices)
PA Curve Configuration
Header file containing custom PA curves
Header file containing PA curve type types
PA Calibration Configuration
Apply PA Calibration Factory Offset
PA calibration offset ensures that PA power remains consistent chip-to-chip. These adjustments occur automatically when the PA is in use, and the application is not notified when these adjustments occur.
See these documents for in-depth explanations of how to configure and use the available PA features:
AN1127: Power Amplifier Power Conversion Functions in RAIL 2.x