You are viewing documentation for version:
2.17.2
A state structure for BLE.
This structure must be allocated in application global read-write memory that persists for the duration of BLE usage. It cannot be allocated in read-only memory or on the call stack.
Public Attributes# uint32_t
The value used to initialize the CRC algorithm.
uint32_t
The access address used for the connection.
uint16_t
The logical channel used.
bool
Indicates whether the whitening engine should be off.
uint16_t
The value used to initialize the whitening algorithm.
Public Attribute Documentation# crcInit# uint32_t RAIL_BLE_State_t::crcInit The value used to initialize the CRC algorithm.
accessAddress# uint32_t RAIL_BLE_State_t::accessAddress The access address used for the connection.
channel# uint16_t RAIL_BLE_State_t::channel The logical channel used.
disableWhitening# bool RAIL_BLE_State_t::disableWhitening Indicates whether the whitening engine should be off.
whiteInit# uint16_t RAIL_BLE_State_t::whiteInit The value used to initialize the whitening algorithm.