Contains arguments for RAIL_BLE_ConfigAox() function.
Public Attributes#
AoX options.
Size of the raw AoX CTE (continuous tone extension) data capture buffer in bytes.
Address to where the received CTE is written.
Address to first element of antenna pattern array.
Number of entries in the antenna pattern array.
Public Attribute Documentation#
cteBuffSize#
uint16_t RAIL_BLE_AoxConfig_t::cteBuffSize
Size of the raw AoX CTE (continuous tone extension) data capture buffer in bytes.
Note this value should be a multiple of 4 as each IQ sample requires 4 bytes.
cteBuffAddr#
uint32_t* RAIL_BLE_AoxConfig_t::cteBuffAddr
Address to where the received CTE is written.
Buffer must be 32-bit aligned.
antArrayAddr#
uint8_t* RAIL_BLE_AoxConfig_t::antArrayAddr
Address to first element of antenna pattern array.
Array must be in RAM. Each element of the array contains an antenna number. The switching pattern is defined by the order of antennas in this array.
antArraySize#
uint8_t RAIL_BLE_AoxConfig_t::antArraySize
Number of entries in the antenna pattern array.