Allows the user to specify direct mode parameters using RAIL_ConfigDirectMode().

Public Attributes#

bool

Enable synchronous RX DOUT using DCLK vs.

bool

Enable synchronous TX DIN using DCLK vs.

uint8_t

RX Data output (DOUT) GPIO port.

uint8_t

RX Data output (DOUT) GPIO pin.

uint8_t

Data clock (DCLK) GPIO port.

uint8_t

Data clock (DCLK) GPIO pin.

uint8_t

TX Data input (DIN) GPIO port.

uint8_t

TX Data input (DIN) GPIO pin.

uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

syncRx#

bool RAIL_DirectModeConfig_t::syncRx

Enable synchronous RX DOUT using DCLK vs.

asynchronous RX DOUT.


Definition at line 5480 of file common/rail_types.h

syncTx#

bool RAIL_DirectModeConfig_t::syncTx

Enable synchronous TX DIN using DCLK vs.

asynchronous TX DIN.


Definition at line 5482 of file common/rail_types.h

doutPort#

uint8_t RAIL_DirectModeConfig_t::doutPort

RX Data output (DOUT) GPIO port.


Definition at line 5485 of file common/rail_types.h

doutPin#

uint8_t RAIL_DirectModeConfig_t::doutPin

RX Data output (DOUT) GPIO pin.


Definition at line 5487 of file common/rail_types.h

dclkPort#

uint8_t RAIL_DirectModeConfig_t::dclkPort

Data clock (DCLK) GPIO port.

Only used in synchronous mode.


Definition at line 5490 of file common/rail_types.h

dclkPin#

uint8_t RAIL_DirectModeConfig_t::dclkPin

Data clock (DCLK) GPIO pin.

Only used in synchronous mode.


Definition at line 5492 of file common/rail_types.h

dinPort#

uint8_t RAIL_DirectModeConfig_t::dinPort

TX Data input (DIN) GPIO port.


Definition at line 5495 of file common/rail_types.h

dinPin#

uint8_t RAIL_DirectModeConfig_t::dinPin

TX Data input (DIN) GPIO pin.


Definition at line 5497 of file common/rail_types.h

doutLoc#

uint8_t RAIL_DirectModeConfig_t::doutLoc

DeprecatedNo longer used (ignored).


Definition at line 5500 of file common/rail_types.h

dclkLoc#

uint8_t RAIL_DirectModeConfig_t::dclkLoc

DeprecatedNo longer used (ignored).


Definition at line 5502 of file common/rail_types.h

dinLoc#

uint8_t RAIL_DirectModeConfig_t::dinLoc

DeprecatedNo longer used (ignored).


Definition at line 5504 of file common/rail_types.h