Release Notes
RAIL Library 2.6.2
February 21, 2019
Release Highlights
- General bugfixes and improvements
Release Details
RAIL Library 2.6.1
January 17, 2019
Release Highlights
- Resolved critical issues with the EFR32xG21 platform
- The chip could hang coming out of reset if it was shutdown or idled at specific points in time.
- Auto-ACK timings were incorrectly computed at high transmit power levels.
- General bugfixes and improvements
Release Details
RAIL Library 2.6.0 GA
December 14, 2018
Release Highlights
- Bugfixes and general improvements
- Added IEEE802.15.4 PHY configurations that support antenna diversity and improved WiFi coexistence performance.
- Improved support for the EFR32xG21 chips.
- Added support for Preamble Sense and Low Duty Cycle Receive modes. Note that these are still intended for advanced users only and will require help from the support team to properly configure.