RAIL_AntennaConfig_t Struct Reference
A configuration for antenna selection.
#include <
rail_chip_specific.h
>
Data Fields | |
bool | ant0PinEn |
Antenna 0 Pin Enable. | |
bool | ant1PinEn |
Antenna 1 Pin Enable. | |
uint8_t | ant0Loc |
Antenna 0 location for pin/port. | |
GPIO_Port_TypeDef | ant0Port |
Antenna 0 output GPIO port. | |
uint8_t | ant0Pin |
Antenna 0 output GPIO pin. | |
uint8_t | ant1Loc |
Antenna 1 location for pin/port. | |
GPIO_Port_TypeDef | ant1Port |
Antenna 1 output GPIO port. | |
uint8_t | ant1Pin |
Antenna 1 output GPIO pin. |
A configuration for antenna selection.
Definition at line 653
of file rail_chip_specific.h
.
The documentation for this struct was generated from the following file:
- chip/efr32/efr32xg1x/
rail_chip_specific.h