Configure the port and pin of the thermistor.
Note
This configuration is chip OPN dependent.
DeprecatedRAIL 2.x synonym of sl_rail_hfxo_thermistor_config_t.
Public Attributes#
uint8_t
The GPIO port to access the thermistor.
uint8_t
The GPIO pin to set the thermistor.
Public Attribute Documentation#
port#
uint8_t RAIL_HFXOThermistorConfig_t::port
The GPIO port to access the thermistor.
DeprecatedRAIL 2.x synonym of sl_rail_hfxo_thermistor_config_t::port.
pin#
uint8_t RAIL_HFXOThermistorConfig_t::pin
The GPIO pin to set the thermistor.
DeprecatedRAIL 2.x synonym of sl_rail_hfxo_thermistor_config_t::pin.