Structure to configure RFSENSE Selective(OOK) mode.

DeprecatedRAIL 2.x synonym of sl_rail_rf_sense_selective_ook_config_t.

Public Attributes#

The frequency band(s) on which to sense the RF energy.

uint8_t

Sync word length in bytes, 1-4 bytes.

uint32_t

Sync Word Value.

The callback function, called when RF is sensed.

Public Attribute Documentation#

band#

RAIL_RfSenseBand_t RAIL_RfSenseSelectiveOokConfig_t::band

The frequency band(s) on which to sense the RF energy.

To stop RF Sense, specify RAIL_RFSENSE_OFF.

DeprecatedRAIL 2.x synonym of sl_rail_rf_sense_selective_ook_config_t::band.


syncWordNumBytes#

uint8_t RAIL_RfSenseSelectiveOokConfig_t::syncWordNumBytes

Sync word length in bytes, 1-4 bytes.

Note

DeprecatedRAIL 2.x synonym of sl_rail_rf_sense_selective_ook_config_t::sync_word_bytes.


syncWord#

uint32_t RAIL_RfSenseSelectiveOokConfig_t::syncWord

Sync Word Value.

To use HW default sync word, set to RAIL_RFSENSE_USE_HW_SYNCWORD.

DeprecatedRAIL 2.x synonym of sl_rail_rf_sense_selective_ook_config_t::sync_word.


cb#

RAIL_RfSense_CallbackPtr_t RAIL_RfSenseSelectiveOokConfig_t::cb

The callback function, called when RF is sensed.

Note

DeprecatedRAIL 2.x synonym of sl_rail_rf_sense_selective_ook_config_t::cb.