Configuration information for FEM Voltage Detection plugin.

A structure of type RAIL_VdetConfig_t is passed to RAIL_ConfigVdet().

DeprecatedRAIL 2.x synonym of sl_rail_vdet_config_t.

Public Attributes#

Mode for the VDET.

Resolution to use for the capture.

uint32_t

Delay in microseconds for the capture from Tx Start in RAIL_VDET_MODE_AUTOMATIC.

Public Attribute Documentation#

mode#

RAIL_Vdet_Mode_t RAIL_VdetConfig_t::mode

Mode for the VDET.

DeprecatedRAIL 2.x synonym of sl_rail_vdet_config_t::mode.


resolution#

RAIL_Vdet_Resolution_t RAIL_VdetConfig_t::resolution

Resolution to use for the capture.

DeprecatedRAIL 2.x synonym of sl_rail_vdet_config_t::resolution.


delayUs#

uint32_t RAIL_VdetConfig_t::delayUs

Delay in microseconds for the capture from Tx Start in RAIL_VDET_MODE_AUTOMATIC.

Minimum 5 us, maximum 100000 us.

DeprecatedRAIL 2.x synonym of sl_rail_vdet_config_t::delay_us.