A channel configuration group structure, which defines a group of radio configurations.
This structure allows grouping multiple radio PHY configurations together, enabling switching between them during runtime.
Public Attributes#
The array of radio PHY configurations in this group.
uint32_t
The number of radio PHY configurations (words) in the phy_config_group array.
Public Attribute Documentation#
phy_config_group#
sl_rail_radio_config_t sl_rail_channel_config_group_t::phy_config_group
The array of radio PHY configurations in this group.
Each configuration defines the parameters for a specific radio setup.
phy_config_group_length#
uint32_t sl_rail_channel_config_group_t::phy_config_group_length
The number of radio PHY configurations (words) in the phy_config_group array.