RAIL sync words and length configuration.
Public Attributes#
uint8_t
Sync word length in bits, between 2 and 32, inclusive.
uint32_t
Sync Word 0.
uint32_t
Sync Word 1.
Public Attribute Documentation#
sync_word_bits#
uint8_t sl_rail_sync_word_config_t::sync_word_bits
Sync word length in bits, between 2 and 32, inclusive.
sync_word_0#
uint32_t sl_rail_sync_word_config_t::sync_word_0
Sync Word 0.
Note
Only the least-significant sync_word_bits bits are used, which are sent or received on air least-significant-bit first.
sync_word_1#
uint32_t sl_rail_sync_word_config_t::sync_word_1
Sync Word 1.
Note
Only the least-significant sync_word_bits bits are used, which are sent or received on air least-significant-bit first.