Public Attributes#
uint8_t
uint8_t
uint32_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint16_t
Public Attribute Documentation#
min_main_mode_steps#
uint8_t sl_rtl_cs_params::min_main_mode_steps
Minimum number of CS main mode steps to be executed before a sub mode step. Currently only value 2 is supported. Field is ignored if sub mode is set to SL_RTL_CS_MODE_NONE.
max_main_mode_steps#
uint8_t sl_rtl_cs_params::max_main_mode_steps
Minimum number of CS main mode steps to be executed before a sub mode step. Currently only value 2 is supported. Field is ignored if sub mode is set to SL_RTL_CS_MODE_NONE.
main_mode_repetition#
uint32_t sl_rtl_cs_params::main_mode_repetition
Number of main modes repeated from previous subevent (0, 1, 2, 3).
num_antenna_paths#
uint8_t sl_rtl_cs_params::num_antenna_paths
Number of antenna paths supported by the local controller for the CS tone exchanges. - Range: 1 to 4. The number of antenna paths used during the phase measurement stage of the CS step. - Value: 0. Phase measurement does not occur during the CS step, therefore ignored.
connection_interval#
uint16_t sl_rtl_cs_params::connection_interval
Connection interval in units of 1.25 ms