Net commands 



#




Use the net commands to retrieve and configure IP settings for the adapter.
Commands | Description |
|---|---|
Perform DNS lookup for a given hostname. | |
Retrieves the MAC address of the adapter. | |
Show the current IP configuration. | |
Set or show IP address. | |
Set or show DNS server address. | |
Set or show gateway address. | |
Enable the DHCP client. | |
Configure IP configuration. | |
Show a list of ports and active connections. |
net dnslookup#
Performs a DNS lookup for a given hostname.
Command Line Syntax
$ net dnslookup <hostname>Command Line Example
$ net dnslookup google.com
Host name : google.com
IP Address : 142.250.74.142
IP address = 142.250.74.142net mac#
Gets the MAC address of the adapter.
Command Line Syntax
$ net macCommand Line Example
$ net mac
MAC Address: A0:C4:5E:31:81:3Cnet ip#
Shows the currently active IP configuration.
Command Line Syntax
$ net ipCommand Line Example
$ net ip
IP Address : 192.168.1.34/24
DNS Server : 192.168.162.10
Gateway : 192.168.1.1
Configured using DHCP.net ip addr#
Sets or shows the IP address using CIDR notation, (e.g. 192.168.0.1/24).
If DHCP is currently enabled, this will disable DHCP. If the IP address is not supplied, the active IP address will be shown.
Command Line Syntax
$ net ip addr [ipAddr]Command Line Example
$ net ip addr 192.168.0.1/24
Setting IP Address to 192.168.0.1/24...
IP Address : 192.168.0.1/24net ip dns#
Sets or shows the DNS server address.
If DHCP is currently enabled, the configuration will be stored, but DHCP will not be disabled. If the DNS server address is not specified, the active DNS server address will be shown.
Command Line Syntax
$ net ip dns [dnsAddr]Command Line Example
$ net ip dns 192.168.0.10
DNS Server : 192.168.0.10net ip gw#
Sets or shows the gateway address.
If DHCP is currently enabled, the configuration will be stored, but DHCP will not be disabled. If the gateway address is not specified, the active gateway address will be shown.
Command Line Syntax
$ net ip gw [gwAddr]Command Line Example
$ net ip gw 235.6.12.1
Gateway : 235.6.12.1net ip dhcp#
Enables the DHCP client.
If 'enable' is not specified, the current state of the configuration is shown. The IP address must be manually set to disable DHCP.
Command Line Syntax
$ net ip dhcp ['enable']Command Line Examples
$ net ip dhcp
Configured manually.
$ net ip dhcp enable
Configured using DHCP.net ip config#
Configures multiple IP configuration parameters simultaneously. The IP address must be given in CIDR notation.
Command Line Syntax
$ net ip config <ip> <gateway> [dns]Command Line Example
$ net ip config 192.168.0.3/24 192.168.0.1 8.8.8.8.
Setting IP Address to 192.168.0.3/24...
IP Address : 192.168.0.3/24
DNS Server : 8.8.8.8
Gateway : 192.168.0.1
Configured manually.net ip conn#
Shows a list of available ports on the adapter and the connected clients.
Command Line Syntax
$ net ip connCommand Line Example
$ net ip conn
# Name Type ClientIP ServerIP LastEvent PipeFull PipeBroken SendErrors
-------------------------------------------------------------------------------------------------------------
0 BGT UDP 192.168.1.40:61887 0.0.0.0:4920 00:00:00:21 0 0 0
1 BCC TCP 0.0.0.0:0 0.0.0.0:4901 00:00:57:46 0 0 0
2 ADMIN TCP 192.168.1.53:49974 0.0.0.0:4902 00:00:00:12 0 0 0
3 DCH TCP 0.0.0.0:0 0.0.0.0:4905 00:00:57:46 0 0 0
4 VUART TCP 0.0.0.0:0 0.0.0.0:4900 00:00:57:46 0 0 0