Debug Commands 

#


Use the debug commands to inspect the debug configuration and to change the debug mode.
For more information about debugging using the board controller, see the debugging overview.
Commands | Description |
|---|---|
Get information about the current debug configuration. | |
Get or set the debug mode. |
dbg info#
Gets information about the current debug configuration.
Command Line Syntax
$ dbg info
Command Line Example
$ dbg info ------ Debug Interface Status ------ Set mode : MCU Active mode : MCU Target Voltage : 3.27 V External cable state : Disconnected # debug connections : 0 AEM current : 4.73 mA
dbg mode#
Gets or sets the debug mode. Will store the debug mode by default if the option --nostore is not supplied.
Command Line Syntax
$ dbg mode [dbgMode] [--nostore]
Command Line Examples
$ dbg mode Current debug mode: MCU $ dbg mode out Debug interface mode changed to OUT. Debug interface mode saved. $ dbg mode mcu --nostore Debug interface mode changed to MCU.