Time Commands 



#




Use the time commands to view status and set client, server, or disabled mode.
For more information about the time synchronization service, see the time synchronization overview.
Command | Description |
|---|---|
Get information about the time sync service. | |
Set the time sync service to client mode. | |
Set the time sync service to server mode. | |
Disable the time sync service. |
time info#
Gets information about the time sync service. The information printed depends on which mode is active.
Command Line Syntax
$ time info
Command Line Example
$ time info ------ Time Sync Service Status ------ Time service mode : client [3] Current local time : 61051618150 us Current time : 2412841592984 us Server address : 10.7.1.13:4904 Last sync successful : Yes Last round-trip time : 115 us Drift per second : 6.19 us/s Polling interval : 9376 ms Time since last sync : 7572 ms Sent : 4 packets Send errors : 0 packets Received : 4 packets Receive errors : 0 packets
time client#
Sets the time sync service to client mode. The server IP address must be the IP address of another adapter where the time sync service is enabled. If no server port is specified, the default port 4904 is used.
Command Line Syntax
$ time client <serverIpAddress> [serverIpPort]
Command Line Example
$ time client 192.168.1.10 4904 Client IP address: 192.168.1.10 Client IP port : 4904 Time service switched to mode: Client
time server#
Sets the time sync service to server mode.
Command Line Syntax
$ time server
Command Line Example
$ time server Time service switched to mode: Server
time disable#
Disable the time sync service.
Command Line Syntax
$ time disable
Command Line Example
$ time disable Time service switched to mode: disable