Serial Commands 

#


Use the serial commands to get information about and configure the serial configuration.
For more information about the supported serial communication protocols see VCOM and Auxiliary UART.
Commands | Description |
|---|---|
Get information about the serial configuration. | |
Configure the serial configuration. | |
Manually control serial handshake lines. | |
Get serial communication stats. | |
Enable serial communication. | |
Disable serial communication. |
serial vcom#
Gets information about the currently selected serial configuration. Shows the active configuration as well as the configuration stored in persistent memory.
Command Line Syntax
$ serial vcom
Command Line Examples
$ serial vcom ----- Virtual COM port ----- Stored port speed : 115200 Active port speed : 487603 Stored handshake : auto Actual handshake : disabled $ serial vcom ----- Aux uart ----- Stored port speed : 115200 Active port speed : 115200 Stored aux uart mode : enabled Actual aux uart mode : enabled $ serial vcom ----- Virtual COM port ----- Stored port speed : 115200 Active port speed : 115234 Stored handshake : aux Actual handshake : rts RTS Asserted - Ready to Receive. ----- Aux uart ----- Stored port speed : 115200 Active port speed : N/A Stored aux uart mode : enabled Actual aux uart mode : disabled $ serial vcom ----- Virtual COM port ----- Stored port speed : 115200 Active port speed : N/A Stored handshake : cts Actual handshake : aux ----- Aux uart ----- Stored port speed : 115200 Active port speed : 115200 Stored aux uart mode : disabled Actual aux uart mode : enabled
serial vcom config#
Configures the serial configuration. You can change the handshake type, the baud rate, or both. By default, the configuration is stored in persistent memory. To skip this, use the --nostore option.
Supported handshake types and baud rates depend on the adapter type. Handshake signals are described from the board controller’s perspective; RTS is an input to the board controller, and CTS is an output from it.
Supported baud rates range from 9600 to 3,686,400. Baud rate configuration for the auxiliary UART is supported only on EKs and DKs.
Handshake type | Description | Supported on |
|---|---|---|
rts | Enable RTS hardware flow control |
|
cts | Enable CTS hardware flow control |
|
rtscts | Enable RTS and CTS hardware flow control |
|
disable | Disable hardware flow control |
|
auto | Automatically set hardware flow control at boot |
|
aux | Enables auxilary UART and disables VCOM |
|
Command Line Syntax
$ serial vcom config [--nostore] [handshake <handshakeType>] [speed <bitrate>]
Command Line Examples
$ serial vcom config --nostore handshake rtscts speed 486000 Baudrate set to 486000 bps Actual baud rate: 487603 Hz RTS handshake enabled CTS handshake enabled Aux uart disabled $ serial vcom config speed 115200 Baudrate set to 115200 bps Actual baud rate: 115234 Hz Serial configuration saved
serial vcom ctrl#
Manually controls serial handshake lines. The command supports asserting and deasserting either RTS or CTS or both at the same time.
Command Line Syntax
$ serial vcom ctrl [rts <assert/deassert>] [cts <assert/deassert>]
Command Line Examples
$ serial vcom ctrl rts assert RTS asserted $ serial vcom ctrl cts assert rts deassert RTS deasserted CTS asserted
serial vcom stats#
Gets serial communication stats.
Command Line Syntax
$ serial vcom stats
Command Line Example
$ serial vcom stats ### Target to Host ### From target: 1818 bytes Discarded: 106 bytes Forwarded: 1712 bytes By transport: CDC: 1712 bytes Conn: 0 bytes Appdata: 0 bytes Last transport: CDC ### Host to Target ### From host: 21 bytes Discarded: 0 bytes Forwarded: 21 bytes By transport: CDC: 21 bytes Conn: 0 bytes Appdata: 0 bytes Last transport: CDC
serial vcom enable#
Enable serial communication. It is not possible to enable serial communication while the currently selected debug mode is in.
Command Line Syntax
$ serial vcom enable
Command Line Example
$ serial vcom enable Enabling VCOM.
serial vcom disable#
Disable serial communication.
Command Line Syntax
$ serial vcom disable
Command Line Example
$ serial vcom disable Disabling VCOM.