Discovery Commands 



#




Use the discovery commands to show the UDP discovery message and manage the discovery key.
For more information about UDP discovery see the UDP Discovery overview.
Commands | Description |
|---|---|
Get UDP discovery message. | |
Set or get UDP discovery key. |
discovery#
Gets the discovery message that will be broadcasted to other devices over UDP.
Command Line Syntax
$ discovery
Command Line Example
$ discovery adapter type=wstk adapter nick=Wpk-jig adapter jlinksn=440266234 adapter netif=0.0.0.0 board=BRD4002A Rev.A06 board list=[0:4002:A:A06];[1:4182:A:B04] connection status=UP connection address=0.0.0.0:0 connection time=00:00:28:07 debug mode=MCU discovery key=00000000 firmware type=wpkappl firmware version=1v6p1b373 node type=NotSet node EUI=NotSet
discovery key#
Sets or gets the discovery key used to identify the adapter. Supports decimal and hex input in the range 0 - 0xFFFFFFFF. This is stored in persistent memory.
Command Line Syntax
$ discovery key [get] $ discovery key [set <discoveryKey>]
Command Line Examples
$ discovery key set 0xBEEFCAFE Discovery key = 3203386110 : BEEFCAFEh $ discovery key Discovery key = BEEFCAFEh