Component Editor#

Click the gear symbol next to an installed configurable component name, or Configure on the component description to open the Component Editor.

proj conf component editor start

The Component Editor opens in a new tab. The changes you can make depend on the component.

proj conf component editor

Changes made here are autosaved in native source format in the associated source files.

proj conf component editor autosave

Click View Source to open an editor on the configuration file. If a component has multiple configuration files, the control is View Source Files

proj conf component editor source