Bluetooth LE SDK Example and Middleware Version 11.0.2 - Release Notes (May 4, 2026)#
The Bluetooth SDK is an advanced Bluetooth 6.1-compliant stack that provides all of the core functionality along with multiple API to simplify development. The core functionality offers both standalone mode, allowing a developer to create and run their application directly on the SoC, or, in NCP mode, allowing for the use of an external host MCU.
Click here for earlier releases.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Added in 11.0.2#
None.
Added in 11.0.1#
Channel Sounding: added support for max_procedure_count=1 in Real Time Fast mode.
Added in 11.0.0#
Host examples shown on Studio Launcher page.
Most bootloader-aware example applications converted to standalone to simplify early development.
API Changes#
None.
Bug Fixes#
Fixed in 11.0.2#
Improved ESL AP scalability
Fixed in 11.0.1#
Targeted quality improvements and bug fixes.
Fixed in 11.0.0#
Various Electronic Shelf Label (ESL) related bug fixes.
Various Channel Sounding (CS) related bug fixes.
Targeted quality improvements and bug fixes.
Chip Enablement#
Added in 11.0.2#
BRD4002A has reached End of Life (EOL). Its successor is BRD4002B.
BRD4002A has reached End of Life (EOL). Its successor is BRD4002B.
Added in 11.0.1#
None.
Added in 11.0.0#
Added xGM270S SiP module support.
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
None.
Enhancements#
Added in 11.0.2#
Electronic Shelf Label (ESL) Access Point (AP): improved scalability by removing per-tag threading timers, optimizing tag object memory usage, and replacing linear registry lookups with indexed data structures.
Added in 11.0.1#
Electronic Shelf Label (ESL) Access Point (AP): refactored event dispatcher to follow the Observer pattern.
Electronic Shelf Label (ESL) Access Point (AP): improved ping performance.
Added in 11.0.0#
The "Log" component now enables the compiler to optimize out filtered out (or masked out) loggings. If a project uses any related API (app_log_filter_threshold_enable, app_log_filter_threshold_set, app_log_filter_mask_enable, app_log_filter_mask_set), turn on the "Enable runtime configuration" setting in the Log configuration.
Removed Features#
None.
Deprecated Features#
None.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
None.
Modified APIs#
None.
Removed APIs#
None.
Deprecated APIs#
None.
Bug Fixes#
Fixed in 11.0.2#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1606142 | NCP MCU host corrupted BGAPI events. | None | NCP; generic software issue |
Fixed in 11.0.1#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1589062 | ESL: image transfer fails if ESL Tag NVM Image storage is used instead of ESL Tag RAM Image. | None | All; generic software issue |
| 1566100 | ESL AP: fixed a rare ESL AP script crash triggered by unsuccessful EAD decryption. | None | NCP; generic software issue |
| 1581223 | Corrupted BGAPI events on NCP-host running on EFR32. | None | NCP; generic software issue |
| 1569678 | Unvalidated input in Bluetooth secure NCP-host app leads to integer underflow. | None | NCP; generic software issue |
Fixed in 11.0.0#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1557180 | ESL AP: PAwR default timing parameters have been changed to avoid ESL tags losing sync during network deployment. | None | All; generic software issue |
Chip Enablement#
Added in 11.0.2#
None.
Added in 11.0.1#
None.
Added in 11.0.0#
| Chip Family | OPNs / Boards / OPN Combinations | Supported Software Variants (if applicable) | Supported Modes | Supported Host Interfaces |
|---|---|---|---|---|
| xGM270S | Board: BRD2715A, BRD4356A | Standard | SoC, NCP, RCP | N/A |
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
New Examples#
None.
Modified Examples#
Modified in 11.0.2#
| Example Name | Changes | Supported Software Variants if applicable | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
bt_soc_thermometer |
The Si7021 RHT sensor has reached end-of-life and is replaced by the Sensirion SHT40 sensor. | Standard | SoC | BRD4002A is replaced by BRD4002B. | N/A |
|
bt_aoa_ncp_locator |
Fixed an issue where the bt_aoa_ncp_locator example could not handle messages from multiple tags when using connection-oriented CTE for AoA and the MQTT protocol.
|
Standard | NCP | BRD4185A | N/A |
Modified in 11.0.1#
| Example Name | Changes | Supported Software Variants if applicable | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
All NCP-host examples |
Added dynamic log filtering to NCP-host examples using app_log_cli. | Standard | NCP | All supported. | UART |
Modified in 11.0.0#
| Example Name | Changes | Supported Software Variants if applicable | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
All NCP-host examples |
|
Standard | NCP |
External Hosts:
|
UART |
|
bt_rcp example |
This example requires flow-control. | Standard | RCP | Radio boards with flow control pins routed out supported only. | UART |
|
bt_rcp_cpc example |
Security is enabled by default in the bt_rcp_cpc sample application. | Standard | RCP | All supported. | UART |
Removed Examples#
Removed in 11.0.2#
None.
Removed in 11.0.1#
None.
Removed in 11.0.0#
Removed Example Name | Was Deprecated? | Note |
|---|---|---|
NCP-host positioning GUI example | Yes | |
NCP-host daemon example | No | Functionality covered by adding |
Deprecated Examples#
None.
Known Issues and Limitations#
| ID | Issue or Limitation Description | GitHub / Salesforce Reference (if any) | Workaround (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|---|
| 1543819 | The automated upgrade is not possible for bt_cs_ncp and bt_cs_soc_initiator examples. | None | Upgrade from 2025.6.x has to be carried out manually. The recommended way to upgrade your project is to create a new project from sisdk-2025.12.x and migrate your changes (e.g. application logic) on top of that. | All |
| 1565117 | IAR toolchain is not supported by Solution Examples | None | None | SoC |
| 1566100 | ESL sporadic crash after EAD decryption error | None | None | All |
| 1568416 | ESL Access point (AP) "exclusive mode" does not filter the ESL tags in some cases | None | None | All |