Bluetooth LE SDK Host Stack Version 11.0.2 - Release Notes (May 4, 2026)#
The Bluetooth Host Stack is a Bluetooth 6.1-compliant stack that provides the core functionality along with multiple API to simplify development. The core functionality offers both standalone mode, allowing a developer to create and run their application directly on the SoC, or NCP mode, allowing for the use of an external host MCU.
Click here for earlier releases.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Added in 11.0.2#
None.
Added in 11.0.1#
None.
Added in 11.0.0#
Bluetooth host qualification for Core specification 6.1.
PAwR event counter reporting.
Channel classification reporting for a remote peripheral device.
Support for larger BGAPI payload size in NCP applications with compile-time configurability.
API Changes#
Changed in 11.0.2#
Note.
Changed in 11.0.1#
Connection Analyzer now reports RSSI in sl_bt_evt_connection_analyzer_report at every connection interval.
Changed in 11.0.0#
The parameter list of an API function is declared as 'void' explicitly if the function has no parameters.
Added parameters for NADM capabilities in commands sl_bt_cs_read_local_supported_capabilities and sl_bt_evt_cs_read_remote_supported_capabilities_complete.
Bug Fixes#
Fixed in 11.0.2#
None.
Fixed in 11.0.1#
Fixed TrustZone build failure when using External Bonding Database.
Fixed in 11.0.0#
Improved L2CAP and ATT packet validation and error handling.
Chip Enablement#
None.
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
Added in 11.0.2#
None.
Added in 11.0.1#
None.
Added in 11.0.0#
The Bluetooth host stack has been improved and qualified for Core specification 6.1.
Support PAwR event counter reporting with new feature component bluetooth_feature_linklayer_interface.
Support reporting the channel classification of a remote peripheral device.
New component bgapi_service_feature_system provides the System class APIs of the BGAPI Service. Command sl_bgapi_system_get_max_payload_sizes can be used to get the maximum payload sizes that BGAPI Protocol is configured to support in the application.
The static GATT database supports the "Write Without Response" property so that the descriptor value could be updated by remote GATT clients using Write Command.
The dynamic GATT database has a new descriptor property flag SL_BT_GATTDB_DESCRIPTOR_WRITE_NO_RESPONSE so that the descriptor value could be updated by remote GATT clients using Write Command.
Enhancements#
Added in 11.0.2#
None.
Added in 11.0.1#
Connection Analyzer now reports RSSI in sl_bt_evt_connection_analyzer_report at every connection interval. Even if the Peripheral packet sniffing fails, the event is generated with the Peripheral RSSI marked as invalid.
Added in 11.0.0#
None.
Removed Features#
None.
Deprecated Features#
None.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
Added in 11.0.2#
None.
Added in 11.0.1#
None.
Added in 11.0.0#
New API Signature | Deprecated API replaced by this (if any) |
|---|---|
sl_status_t sl_bt_linklayer_event_info_reporting_enable | N/A |
N/A | |
N/A |
Modified APIs#
Modified in 11.0.2#
None.
Modified in 11.0.1#
Old API | Modified |
|---|---|
The analyzer now generates a report at every connection interval. When a central or peripheral packet could not be observed, the RSSI for the role is reported as unavailable (127). Previously, when this device was in central role, the analyzer generated a report only after the peripheral responded to the central in a connection event. |
Modified in 11.0.0#
Removed APIs#
Removed in 11.0.2#
None.
Removed in 11.0.1#
None.
Removed in 11.0.0#
Removed API Name | Was Deprecated? |
|---|---|
void sl_bt_system_reset | Yes |
sl_status_t sl_bt_sm_set_bonding_key | Yes |
Deprecated APIs#
None.
Bug Fixes#
Fixed in 11.0.2#
None.
Fixed in 11.0.1#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1565402 | Fixed an issue where sli_bt_external_bondingdb_config.c in the bluetooth_feature_external_bonding_database component included the sl_mbedtls_config.h header, which could not be found when using TrustZone. This resolves a build failure caused by the missing header file. | None | All; generic software issue |
Fixed in 11.0.0#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1521108 | In ATT_EXECUTE_WRITE_REQ handling, the GATT server now ensures either all prepared write requests are successfully written in the GATT database or nothing will be written. Previously, successful writes before an error would remain in the database, leaving it in an inconsistent state. | None | All; generic software issue |
| 1521428 | Improved the L2CAP CoC signaling packet validation by adding the length checks for all L2CAP command types and checking both L2CAP header length and SDU length. | None | All; generic software issue |
| 1564484 | Fixed an issue where the device could enter EM2 even when the LF clock accuracy was below the threshold required for reliable Bluetooth connections. | None | All; generic software issue |
Impact of Release Changes#
Impact Statements and Migrations from 10.x to 11.0.0#
| Change | Migration Guide | Affected Software Variants if applicable | Affected Modes | Affected OPNs / Boards / OPN Combinations | Affected Host Interfaces |
|---|---|---|---|---|---|
| The parameter list of an API function is declared as 'void' explicitly if the function has no parameters | Code that correctly calls with no arguments will continue to work. If there happens to be code calling such functions with arguments, remove the arguments. | All | All | Hardware agnostic | N/A |
| New parameters nadm_sounding_capability and nadm_random_capability in commands sl_bt_cs_read_local_supported_capabilities | The implementation that invokes this API should provide valid pointers for the new parameters, or provide NULL if the capability values are unused. | All | All | Hardware agnostic | N/A |
| New data fields nadm_sounding_capability and nadm_random_capability in event sl_bt_evt_cs_read_remote_supported_capabilities_complete | Rebuild NCP host applications on Simplicity SDK 2025.12. | All | NCP | Hardware agnostic | N/A |
Known Issues and Limitations#
| ID | Issue or Limitation Description | GitHub / Salesforce Reference (if any) | Workaround (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|---|
| 1417141 | The OTA DFU fast mode in the Bootloader with Apploader is unreliable due to the chance of packet losses. | None | Use OTA DFU reliable mode. | All |
| 1562916 | The device does not enter EM2 when Bluetooth is used on radio boards brd2704a, brd4319a and brd4337a due to LFRCO precision mode is not enabled by default. | None | Enable LFRCO precision mode by overriding configuration SL_CLOCK_MANAGER_LFRCO_PRECISION to cmuPrecisionHigh in the application project. | All |