Simplicity SDK Platform - Micrium OS Version 5.18.2 (February 18, 2026) - Release Notes#

Simplicity SDK Platform Version 5.2.3

Simplicity SDK Version 2025.6.3

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

Added in 5.18.2#

None.

Added in 5.18.1#

None.

Added in 5.18.0#

  • Improved support for main stack overflow detection.

  • Added support for GCC Link Time Optimization (LTO).

API Changes#

None.

Bug Fixes#

Fixed in 5.18.2#

Micrium OS CMSIS-RTOS: Fixed osMessageQueueGet() with osWaitForever not waiting indefinitely.

Fixed in 5.18.1#

None.

Fixed in 5.18.0#

Resolved false positive link time warnings in the MicriumOS CMSIS-RTOS layer when Link Time Optimization (LTO) is enabled.

Chip Enablement#

Added in 5.18.2#

None.

Added in 5.18.1#

None.

Added in 5.18.0#

  • Added support for the EFR32BG29 and EFR32MG29 devices (Series 2).

  • Added support for the EFR32BG22L devices (EFR32BG22L122F352GM32).

  • Added support for the EFR32BG24L devices (EFR32BG24L010F768IM40 and EFR32BG24L210F768IM40).

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

New Features#

Added in 5.18.2#

None.

Added in 5.18.1#

Restricted Micrium OS usage to Series 2 devices.

Added in 5.18.0#

Added support for GCC Link Time Optimization (LTO).

Enhancements#

Added in 5.18.2#

None.

Added in 5.18.1#

None.

Added in 5.18.0#

Improved support for main stack overflow detection utilizing the MSPLIM register.

Removed Features#

None.

Deprecated Features#

None.

API Changes#

New APIs | Modified APIs | Removed APIs | Deprecated APIs

New APIs#

None.

Modified APIs#

None.

Removed APIs#

None.

Deprecated APIs#

None.

Bug Fixes#

Fixed in 5.18.2#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1503571 Micrium OS CMSIS-RTOS: Fixed an issue where calling osMessageQueueGet() with osWaitForever did not wait indefinitely and could return osErrorTimeout after approximately 28 hours. 00332342 Series 2 Devices

Fixed in 5.18.1#

None.

Fixed in 5.18.0#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1426961 Fixed link time warnings in the MicriumOS CMSIS-RTOS layer by reworking code implementation, eliminating false positive warnings that occurred only when Link Time Optimization (LTO) was activated. None. Series 2 Devices

Chip Enablement#

None.

Application Example Changes#

New Examples | Modified Examples | Removed Examples | Deprecated Examples

New Examples#

None.

Modified Examples#

None.

Removed Examples#

None.

Deprecated Examples#

None.

Known Issues and Limitations#

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1166857 OSTaskQPost doesn't send a message to current task when called with a null pointer as argument. None. None. All Devices