Edit

Install Simplicity Studio#

Note: If you have used the Simplicity Installer (UI) or the Silicon Labs Tool (SLT-CLI) installer to install previous versions and related tools, clean your system to ensure you get a proper baseline installation. Follow these instructions to manually uninstall previous versions.

Use the Simplicity Installer#

This section provides instructions for installing Simplicity Studio and Tools using the Simplicity Installer. Start by following the steps in the section for your operating system, and then continue with the section common to all operating systems.

Note: If you previously installed Simplicity Studio 6 Beta using the beta Simplicity Installer, we recommend downloading and using the latest GA Simplicity Installer to complete your installation. After installing the GA version, you can manage all future updates through the Package Manager.

Windows Installation#

  1. Download the Windows Simplicity Installer from the Simplicity Studio v6 page.

  2. Double-click SimplicityInstaller-x.x.x-windows-x64.exe to launch the installation wizard.

  3. Continue by following Simplicity Studio Installation Steps Common to All Operating Systems.

Mac Installation#

  1. Download the Mac Simplicity Installer from the Simplicity Studio v6 page.

  2. Open the Finder and navigate to Downloads.

  3. Double-click the DMG file.

  4. Drag the application icon from the DMG window into the Applications folder.

  5. Once the copy process has finished, eject the DMG.

  6. Delete the DMG file from the Downloads directory.

  7. Continue by following Simplicity Studio Installation Steps Common to All Operating Systems.

  8. On macOS, navigate to your Applications folder (/Users/<username>/Applications/SiliconLabs) and locate the Simplicity Studio shortcut to launch the application. For more details, refer to the workaround described in the release notes.

Linux Installation#

  1. Download the Linux Simplicity Installer from the Simplicity Studio v6 page.

  2. Install the Simplicity Installer using one of the following methods:

    • Using the Ubuntu App Center: Double-click the downloaded .deb package to install it with the Ubuntu App Center application. When prompted, enter the administrator password.

    • Using the Terminal: Open a terminal window and navigate to the folder containing the downloaded .deb package (by default, the user's Downloads folder) using the cd command. Then, run the following command to install the package with apt: sudo apt install ./SimplicityInstaller-VERSION-linux-x64.deb

  3. Run /opt/SimplicityInstaller/simplicityinstaller to launch the Installer.

  4. Continue by following Simplicity Studio Installation Steps Common to All Operating Systems.

Simplicity Studio Installation Steps Common to All Operating Systems#

When the Simplicity Installer opens, the following installation tracks display:

  • Technology Install: Install Simplicity Studio, tools, and SDKs by selecting one or more technology types, such as Bluetooth, Matter, Proprietary, Thread, Wi-Fi, Wi-SUN, and Zigbee.

  • Full Install: Install all files, tools, and SDK technology types available in Simplicity Studio.

  • Demos Only: Try out sample apps on a device. This track consists of these components:

    • A demo SDK with sample apps you can flash to your device

    • The Simplicity Device Manager, which is required to flash apps to your device

    • The base, or minimum, installation files for Simplicity Studio

  • Advanced: Choose the packages you want to install.

    Note: Some packages are only available after you select Log In and sign into your Silicon Labs account. For more information, see Advanced Track

installation tracksinstallation tracks

To continue the installation:

  1. Select the installation track that you want.

  2. Complete the steps for that installation track.

  3. Install VS Code and the VS Code extension.

Note: If you encounter issues during the installation process, you can download and review the installation log files by clicking the Export Logs icon in the upper-right corner of Simplicity Installer. Export LogsExport Logs

Full Install Track#

  1. Click the Full Install tile.

    Full Install tileFull Install tile

    Note: If you decide to customize your installation at this point instead of doing a full installation, click Customize Install and continue with the steps for the Advanced installation.

    Customize Install linkCustomize Install link

  2. Accept the license by checking the Terms & Services box at the bottom of the page, and then click INSTALL.

    Accept the terms and services check box and Install buttonAccept the terms and services check box and Install button

  3. The installation process starts immediately. Follow the current status on the progress bar at the top of the page.

    Installation progress barInstallation progress bar

  4. When the installation is completed, "The installation was successful!" message displays.

    Successful installation messageSuccessful installation message

  5. (optional) Export recipes.

  6. Click LAUNCH STUDIO in the lower-right corner of the page of the Installer to start Simplicity Studio. A desktop shortcut for Simplicity Studio is also available.

Technology Install Track#

  1. Click the Technology Install tile.

    Technology Install tileTechnology Install tile

    The technology types available for installation display in two columns: required and optional packages.

    Technology typesTechnology types

  2. Select the packages you want to install by clicking on each tile, or if you want to install all of them, check the Select All box at the top of the list.

  3. Click NEXT to go to the next page.

  4. Review the list of packages you selected. If you need to add more, click BACK, select the packages, and then click NEXT to continue.

  5. Accept the license by checking the Terms & Services box at the bottom of the page, and then click INSTALL.

    Accept the terms and services check box and Install buttonAccept the terms and services check box and Install button

  6. The installation process starts immediately. Follow the current status on the progress bar at the top of the page.

    Installation progress barInstallation progress bar

  7. When the installation is completed, "The installation was successful!" message displays.

  8. Click LAUNCH STUDIO in the lower-right corner of the page of the Installer to start Simplicity Studio. A desktop shortcut for Simplicity Studio is also available.

Demos Only Track#

  1. Click the Demos Only tile.

    Demos Only installation tileDemos Only installation tile

    A list of available demo packages for installation is displayed.

    Demo packagesDemo packages

    Note: If you decide to customize your installation at this point instead of doing a full installation, click Customize Install and continue with the steps for the Advanced installation.

    Customize Install linkCustomize Install link

  2. Accept the license by checking the Terms & Services box at the bottom of the page, and then click INSTALL.

    Accept the terms and services check box and Install buttonAccept the terms and services check box and Install button

  3. The installation process starts immediately. Follow the current status on the progress bar at the top of the page.

    Installation progress barInstallation progress bar

  4. When the installation is completed, "The installation was successful!" message displays.

    Successful installation messageSuccessful installation message

  5. Click LAUNCH STUDIO in the lower-right corner of the page of the Installer to start Simplicity Studio. A desktop shortcut for Simplicity Studio is also available.

Advanced Track#

  1. Click the Advanced tile.

    Advanced installation tileAdvanced installation tile

    A list of available packages displays.

    Available packages in the Advanced installation trackAvailable packages in the Advanced installation track

    Note: In this release, external SDK extension packages, such as Peripheral Examples, are now discoverable in the list of available packages. To locate these examples, enter peripheral in the search field.

  2. (optional) Search for a package by entering the name of the package in the Search field. The package names containing a match display below the Search field as you type.

    Search for packagesSearch for packages

    Click the X at the right of the Search field to clear your search terms.

  3. Do one of the following:

    • Select one or more packages by checking the boxes next to each package name.

      Select single packages to installSelect single packages to install

    • Include all available packages by checking the Select All box at the top of the package list.

      Select all packages to installSelect all packages to install

    • Sign in to your account to view all packages available to your account, including packages with restricted access. After you sign in, you can also install any package that displays the Log In button.

      To sign in, follow these steps:

      1. Select Log In.

        Log inLog in

      2. When prompted, verify your device code, and then select Connect.

        Connect pageConnect page

      3. On the Silicon Labs sign-in page, enter your email address and password, and then select Log In.

        LoginLogin

      4. On the Authorization Successful page, select Continue.

      5. When prompted, select Reload to refresh the package list.

    Packages that become available after you sign in are identified by an open lock icon. Install these packages the same way that you install any other package. If a package displays a Contact Sales button, it is not authorized for your account. Select Contact Sales to request access.

  4. Accept the license by checking the Terms & Services box at the bottom of the page, and then click INSTALL.

    Accept the terms and services check box and Install buttonAccept the terms and services check box and Install button

  5. The installation process starts immediately. Follow the current status on the progress bar at the top of the page.

    Installation progress barInstallation progress bar

  6. When the installation is completed, "The installation was successful!" message displays.

    Successful installation messageSuccessful installation message

  7. (optional) Import or export recipes.

  8. Click LAUNCH STUDIO in the lower-right corner of the page of the Installer to start Simplicity Studio. A desktop shortcut for Simplicity Studio is also available.

Install VS Code and the VS Code Extension#

The Visual Studio Code extension for Simplicity Studio is the primary companion tool for application development in Simplicity Studio 6. It enables developers to edit, build, and debug projects directly in VS Code.

Important: Simplicity Studio VS Code extension v1.6.1 or later is required for compatibility with Simplicity Studio 6.

Simplicity Studio 6 is still required for:

  • Creating new projects

  • Managing project configuration using the Project Configurator and other UI-based tools

You can install the Simplicity Studio extension for VS Code:

  • Directly from the VS Code Marketplace (preferred method)

For detailed installation instructions and usage guidance, see Simplicity Studio Extension for VS Code.