File List

Here is a list of all documented files with brief descriptions:

bus
 wf200_bus.cCommon bus operations that are independent of the underlying physical bus
 wf200_bus.h
 wf200_bus_sdio.cBus low level operations that dependent on the underlying physical bus: SDIO implementation
 wf200_bus_spi.cBus low level operations that dependent on the underlying physical bus : SPI implementation
firmware
 2.0.0
   basic_types.hThis file contains the basic types definitions used for both LMAC/UMAC APIs
   general_api.hThis file contains the type definitions for WLAN general API structures, enums, and other types
   wf200_pds.hPDS configuration specific to a hardware configuration
   wfm_api.hThis file contains the different includes for UMAC API definition
   wfm_cmd_api.h
   wfm_wf200.h
   wfm_wf200_A0.h
   wfm_wf200_B0.h
   wfm_wf200_C0.h
 wf200_registers.hRegister definitions for the WF200 chip
sl
   sl_status.h
   sl_wifi_status.h
wf200.cWF200 Full MAC driver
wf200.hDefinitions of the FMAC driver functions
wf200_configuration.hDefines various values related to the bus communication between WF200 and the host MCU
wf200_constants.hContains defines, enums, structures and functions used by wf200 drive
wf200_host_api.hContains the definitions of the functions to be implemented by the host MCU