Configuring the Driver in Wi-Fi Monitor Mode#
The Steps for operating the device in Monitor Mode are outlined below.
To install the driver, run the following commands:
# insmod rsi_91x.ko rsi_zone_enabled=1 dev_oper_mode=1 driver_mode_value=7Insert the SDIO interface ko.
# insmod rsi_sdio.koMake sure that interface is down. If not, run the following command to bring down the interface:
# ifconfig <interface_name> downTo change the default interface to monitor, run the following command:
# iwconfig < interface_name> mode monitor OR # iw dev <interface_name> set type monitorTo bring up the interface, run the following command:
# ifconfig <interface_name> upSet the channel in which you want to capture the on air packets.
# iwconfig <interface_name> channel < channel no> OR # iw dev <interface_name> set channel <channel no>Use any network packet analysis tool to see captured packets.
# wireshark & OR # tcpdump &
Note: Install wireshark in the system, if it is not found.