Configuring the Driver in Wi-Fi Station Mode#
This section provides the steps to configure Wi-Fi station mode in different security modes (WPA3 & Enterprise mode), Selective scan using wpa_supplicant, and Configure station using the Network Manager CLI. Refer to the Configure in Wi-Fi Station Mode section for details on open and WPA2-PSK security modes, as well as steps to configure Wi-Fi Station mode using a startup script or manual commands.
For WPA3 security mode:
To connect in WPA3, compile the latest supplicant (following the instructions in latest supplicant) with the following flags enabled in the wpa_supplicant .config file.
CONFIG_SAE=y CONFIG_IEEE80211W=yUse the following network block in sta_settings.conf file for WPA3 configuration
pmf=2 network={ ssid="<SSID of Access Point>" key_mgmt=SAE psk=<passphrase specified in the Access Point> ieee80211w=2 }Note: WPA3 Enterprise security mode is not supported in this release.
For WPA2-EAP TLS (Enterprise mode) mode:
network={ ssid="<SSID of Access Point>" key_mgmt=WPA-EAP eap=TLS anonymous_identity="tlsuser" identity="test" password=<passphrase specified in the Access Point> ca_cert="/etc/certs/wifiuser.pem" client_cert="/etc/certs/wifiuser.pem" private_key_passwd=<private key password> private_key="/etc/certs/wifiuser.key" pairwise=CCMP TKIP group=CCMP TKIP proto=WPA2 WPA priority=20 }In EAP-TLS, copy the client certificates in a path and configure the path in network block, as shown above. See the Wi-Fi Enterprise Security section for Radius Server configuration.
For WPA2-EAP PEAP (Enterprise mode) mode:
network={ ssid="<SSID of Access Point>" key_mgmt=WPA-EAP eap=PEAP anonymous_identity="peapuser" identity="test" password=<passphrase specified in the Access Point> pairwise=CCMP TKIP group=CCMP TKIP proto=WPA2 WPA priority=20 }For WPA2-EAP TTLS (Enterprise mode) mode:
network={ ssid="<SSID of Access Point>" key_mgmt=WPA-EAP eap=TTLS anonymous_identity="ttlsuser" identity="test" password=<passphrase specified in the Access Point> pairwise=CCMP TKIP group=CCMP TKIP proto=WPA2 WPA priority=20 }
For Hidden / Stealth SSID:
To connect to an Access Point whose SSID is not broadcast (Hidden), add the following line to the network block.
scan_ssid=1
For example :
network={ ssid="<SSID of Access Point>" scan_ssid=1 key_mgmt=NONE }
For Selective Scan:
To enable the selective scan, add freq_list parameter outside the network block. freq_list is a space-separated list of frequencies in MHz which limits the frequencies that will be scanned.
freq_list=2412 2437 2462
Example config file that will only scan on channel 1 and 36.
freq_list=2412 5180 network={ ssid="<SSID of Access Point>" key_mgmt=NONE }
Configure Station Using the Network Manager#
Below are the specific commands that can be used for connection using the Network Manager CLI(nmcli):
To check the network manager status (started or stopped), run the following command:
For fedora,
# service NetworkManager statusFor ubuntu,
# service network-manager statusIf the network manager is inactive or not started, start it with the following command:
For fedora,
# service NetworkManager startFor ubuntu,
# service network-manager startTo view the currently available network connections, run the following command:
# nmcli con showsample output:
NAME UUID TYPE DEVICE eth0 96a5deb0-5eb0-41e1-a7ed-38fea413f9c8 802-3-ethernet eth0 wlan0 91451385-4eb8-4080-8b82 802-11-wireless wlan0 > **Note**: Here wlan0 is the interface created and the interface name may vary between the host used.To view the list of access points, run the following command:
# nmcli dev wifi listSample output is shown below.
SSID MODE CHAN RATE SIGNAL BARS SECURITY ASUS Infra 11 54 Mbit/s 100 ▂▄▆█ WPA2 test123 Infra 8 54 Mbit/s 32 ▂▄__ WPA1 WPA2 cisco Infra 1 54 Mbit/s 30 ▂___ WPA1 WPA2 test Infra 13 54 Mbit/s 25 ▂___ --- Dlink Infra 1 54 Mbit/s 0 ____ WPA2 TP-LINK_E11946 Infra 7 54 Mbit/s 83 ▂▄▆█ WPA1 WPA2To connect to an AP with WPA/WPA2 security, run the following command:
# nmcli dev wifi connect <SSID> password <password> <interface_name> # For example : nmcli dev wifi connect ASUS password 12345678 wlan0In this case, ASUS is the AP’s SSID, password is 12345678, and interface_name is wlan0.
To connect to an AP without security, run the following command:
# nmcli dev wifi connect <SSID> <interface_name> # nmcli dev wifi connect test wlan0Here, 'test' is the SSID and interface_name is wlan0.
To retrieve the status of devices and connections, run the following command:
# nmcli dev statusSample output:
DEVICE TYPE STATE CONNECTION wlan0 wifi connected my-ssid eth0 ethernet unavailable --As can be seen, the STATE corresponding to wlan0 interface shows connected.
To enable a connection on interface (i.e., to make it active), using nmcli, run the following command. connection_name can be obtained from the command above.
# nmcli con up id <connection_name>To disable an interface using nmcli, run the following command:
# nmcli dev disconnect <interface_name>