DMA transfer structure.
Public Attributes#
uint32_t *
Source transfer address.
uint32_t *
Destination transfer address.
uint32_t
Source address increment size.
uint32_t
Destination address increment size.
uint32_t
Transfer data size.
uint32_t
Total transfer length.
uint8_t
DMA transfer type.
uint8_t
DMA transfer mode.
uint8_t
Peripheral signal which triggers DMA transfer (if 0, consider as software trigger)
Public Attribute Documentation#
src_addr#
uint32_t* sl_dma_xfer_t::src_addr
Source transfer address.
Definition at line
174
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_dma.h
dest_addr#
uint32_t* sl_dma_xfer_t::dest_addr
Destination transfer address.
Definition at line
175
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_dma.h
src_inc#
uint32_t sl_dma_xfer_t::src_inc
Source address increment size.
Definition at line
176
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_dma.h
dst_inc#
uint32_t sl_dma_xfer_t::dst_inc
Destination address increment size.
Definition at line
177
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_dma.h
xfer_size#
uint32_t sl_dma_xfer_t::xfer_size
Transfer data size.
Definition at line
178
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_dma.h
transfer_count#
uint32_t sl_dma_xfer_t::transfer_count
Total transfer length.
Definition at line
179
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_dma.h
transfer_type#
uint8_t sl_dma_xfer_t::transfer_type
DMA transfer type.
Definition at line
180
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_dma.h
dma_mode#
uint8_t sl_dma_xfer_t::dma_mode
DMA transfer mode.
Definition at line
181
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_dma.h
signal#
uint8_t sl_dma_xfer_t::signal
Peripheral signal which triggers DMA transfer (if 0, consider as software trigger)
Definition at line
182
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_dma.h