Generic SPI#
Modules#
Enumerations#
Enumeration for different GSPI callback events.
Enumeration for GSPI power state.
Enumeration for GSPI clock modes.
Enumeration for GSPI master modes.
Enumeration for GSPI slave select mode.
Enumeration for GSPI Master instance, enum for one member, future provision is provided.
Enumeration for GSPI Slave numbers.
Typedefs#
Renamed signal event structure.
Renamed status structure.
Renamed GSPI driver structure.
Created GSPI handle type.
Functions#
Set the clock for the GSPI peripheral, Configures the PLL clock and SOC clock with the value set by user in the clock configuration structure.
Initialize the GSPI.
Uninitialize the GSPI.
Change the power mode of GSPI, the supported modes are.
Receive data from the slave device.
Send data to the slave device.
Send and receive data to the slave device simultaneously.
Set main state i.e., activate/de-activate the main.
Register the user callback function.
Un-register the user callback function.
Get the release, sqa and dev version of GSPI.
Get the transfer status GSPI.
Get data receive count of the GSPI.
Get the transmit data count of GSPI.
Fetch the clock division factor.
Fetch the frame length i.e., bit width.
Set the slave number in multi-slave operation.
Enumeration Documentation#
gspi_event_typedef_t#
gspi_event_typedef_t
Enumeration for different GSPI callback events.
Enumerator | |
---|---|
SL_GSPI_TRANSFER_COMPLETE | Transfer complete event. |
SL_GSPI_DATA_LOST | Data lost event. |
SL_GSPI_MODE_FAULT | Mode fault event. |
56
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_gspi_power_state_t#
sl_gspi_power_state_t
Enumeration for GSPI power state.
Enumerator | |
---|---|
SL_GSPI_POWER_OFF | Power mode OFF. |
SL_GSPI_LOW_POWER | Low power mode. |
SL_GSPI_FULL_POWER | Full power mode. |
SL_GSPI_POWER_MODE_LAST | Last member of enum for validation. |
63
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
clock_mode_typedef_t#
clock_mode_typedef_t
Enumeration for GSPI clock modes.
Enumerator | |
---|---|
SL_GSPI_MODE_0 | Mode 0 CPOL0_CPHA0. |
SL_GSPI_MODE_3 | Mode 1 CPOL1_CPHA1. |
71
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
master_mode_typedef_t#
master_mode_typedef_t
Enumeration for GSPI master modes.
Enumerator | |
---|---|
SL_GSPI_MASTER_INACTIVE | Master mode inactive. |
SL_GSPI_MASTER_ACTIVE | Master mode active. |
SL_GSPI_MASTER_MODE_LAST | Last member of enum for validation. |
77
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
slave_select_mode_typedef_t#
slave_select_mode_typedef_t
Enumeration for GSPI slave select mode.
Enumerator | |
---|---|
SL_GSPI_MASTER_UNUSED | Master unused mode. |
SL_GSPI_MASTER_SW | Master software mode. |
SL_GSPI_MASTER_HW_OUTPUT | Master hardware output mode. |
SL_GSPI_SLAVE_SELECT_MODE_LAST | Last member of enum for validation. |
84
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_gspi_instance_t#
sl_gspi_instance_t
Enumeration for GSPI Master instance, enum for one member, future provision is provided.
Enumerator | |
---|---|
SL_GSPI_MASTER | GSPI Master Instance. |
SL_GSPI_INSTANCE_LAST_ENUM | Last member of enum for validation. |
92
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_gspi_slave_number_t#
sl_gspi_slave_number_t
Enumeration for GSPI Slave numbers.
Enumerator | |
---|---|
GSPI_SLAVE_0 | Slave No. 1. |
GSPI_SLAVE_1 | Slave No. 2. |
GSPI_SLAVE_2 | Slave No. 2. |
GSPI_SLAVE_LAST_ENUM | Last member of enum for validation. |
98
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
Typedef Documentation#
sl_gspi_signal_event_t#
typedef ARM_SPI_SignalEvent_t sl_gspi_signal_event_t
Renamed signal event structure.
50
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_gspi_status_t#
typedef ARM_SPI_STATUS sl_gspi_status_t
Renamed status structure.
51
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_gspi_driver_t#
typedef ARM_DRIVER_SPI sl_gspi_driver_t
Renamed GSPI driver structure.
52
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_gspi_handle_t#
typedef const void* sl_gspi_handle_t
Created GSPI handle type.
53
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
Function Documentation#
sl_si91x_gspi_configure_clock#
sl_status_t sl_si91x_gspi_configure_clock (sl_gspi_clock_config_t * clock_configuration)
Set the clock for the GSPI peripheral, Configures the PLL clock and SOC clock with the value set by user in the clock configuration structure.
N/A | clock_configuration | Pointer to the clock configuration structure |
Returns
status 0 if successful, else error code SL_STATUS_OK (0x0000) - Success SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid SL_STATUS_FAIL (0x0001) - The function is failed SL_STATUS_NOT_INITIALIZED (0x0011) - Clock is not initialized
147
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_si91x_gspi_init#
sl_status_t sl_si91x_gspi_init (sl_gspi_instance_t instance, sl_gspi_handle_t * gspi_handle)
Initialize the GSPI.
[in] | instance | GSPI Instance. |
[in] | gspi_handle | Double Pointer to the GSPI driver handle |
If the DMA is enabled, it also initializes the DMA. Pass the address of the pointer for storing the GSPI master handle, which can be used in future for other function calls.
Returns
status 0 if successful, else error code SL_STATUS_OK (0x0000) - Success SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid SL_STATUS_BUSY (0x0004) - Driver is busy
164
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_si91x_gspi_deinit#
sl_status_t sl_si91x_gspi_deinit (sl_gspi_handle_t gspi_handle)
Uninitialize the GSPI.
[in] | gspi_handle | Pointer to the GSPI driver handle |
If the DMA is enabled, it also uninitializes the DMA.
Returns
status 0 if successful, else error code SL_STATUS_OK (0x0000) - Success SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer
177
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_si91x_gspi_configure_power_mode#
sl_status_t sl_si91x_gspi_configure_power_mode (sl_gspi_handle_t gspi_handle, sl_gspi_power_state_t state)
Change the power mode of GSPI, the supported modes are.
[in] | gspi_handle | Pointer to the GSPI driver handle |
[in] | state | pointer to the configuration structure |
POWER_OFF
FULL_POWER
Returns
status 0 if successful, else error code SL_STATUS_OK (0x0000) - Success SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid SL_STATUS_FAIL (0x0001) - The function is failed SL_STATUS_NOT_SUPPORTED (0x000F) - Parameter is not supported
196
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_si91x_gspi_set_configuration#
sl_status_t sl_si91x_gspi_set_configuration (sl_gspi_handle_t gspi_handle, sl_gspi_control_config_t * control_configuration)
N/A | gspi_handle | |
N/A | control_configuration |
224
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_si91x_gspi_receive_data#
sl_status_t sl_si91x_gspi_receive_data (sl_gspi_handle_t gspi_handle, void * data, uint32_t data_length)
Receive data from the slave device.
[in] | gspi_handle | Pointer to the GSPI driver handle |
[in] | data | pointer to the variable which will store the received data |
[in] | data_length | (uint32_t) number of data items to receive |
sl_si91x_gspi_configure_clocksl_si91x_gspi_initsl_si91x_gspi_configure_power_mode sl_si91x_gspi_set_configuration sl_si91x_gspi_set_slave_number
Returns
status 0 if successful, else error code SL_STATUS_OK (0x0000) - Success SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid SL_STATUS_FAIL (0x0001) - The function is failed SL_STATUS_BUSY (0x0004) - Driver is busy
246
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_si91x_gspi_send_data#
sl_status_t sl_si91x_gspi_send_data (sl_gspi_handle_t gspi_handle, const void * data, uint32_t data_length)
Send data to the slave device.
[in] | gspi_handle | Pointer to the GSPI driver handle |
[in] | data | const pointer to the variable that has data which needs to be sent |
[in] | data_length | (uint32_t) number of data items to send |
sl_si91x_gspi_configure_clocksl_si91x_gspi_initsl_si91x_gspi_configure_power_mode sl_si91x_gspi_set_configuration sl_si91x_gspi_set_slave_number
Returns
status 0 if successful, else error code SL_STATUS_OK (0x0000) - Success SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid SL_STATUS_FAIL (0x0001) - The function is failed SL_STATUS_BUSY (0x0004) - Driver is busy
267
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_si91x_gspi_transfer_data#
sl_status_t sl_si91x_gspi_transfer_data (sl_gspi_handle_t gspi_handle, const void * data_out, void * data_in, uint32_t data_length)
Send and receive data to the slave device simultaneously.
[in] | gspi_handle | Pointer to the GSPI driver handle |
[in] | data_out | const pointer to the variable that has data which needs to be sent |
[in] | data_in | pointer to the variable which will store the received data |
[in] | data_length | (uint32_t) number of data items to receive |
sl_si91x_gspi_configure_clocksl_si91x_gspi_initsl_si91x_gspi_configure_power_mode sl_si91x_gspi_set_configuration sl_si91x_gspi_set_slave_number
Returns
status 0 if successful, else error code SL_STATUS_OK (0x0000) - Success SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid SL_STATUS_FAIL (0x0001) - The function is failed SL_STATUS_BUSY (0x0004) - Driver is busy
289
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_si91x_gspi_set_master_state#
sl_status_t sl_si91x_gspi_set_master_state (sl_gspi_handle_t gspi_handle, boolean_t value)
Set main state i.e., activate/de-activate the main.
[in] | gspi_handle | Pointer to the GSPI driver handle |
[in] | value | (boolean_t) Enable or Disable |
Returns
status 0 if successful, else error code SL_STATUS_OK (0x0000) - Success SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_BUSY (0x0004) - Driver is busy SL_STATUS_INVALID_MODE (0x0024) - Mode is invalid (Fails to activate master)
309
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_si91x_gspi_register_event_callback#
sl_status_t sl_si91x_gspi_register_event_callback (sl_gspi_handle_t gspi_handle, sl_gspi_signal_event_t callback_event)
Register the user callback function.
[in] | gspi_handle | Pointer to the GSPI driver handle |
[in] | callback_event | Pointer to the function which needs to be called at the time of interrupt |
Returns
status 0 if successful, else error code SL_STATUS_OK (0x0000) - Success SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_BUSY (0x0004) - Driver is busy
321
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_si91x_gspi_unregister_event_callback#
void sl_si91x_gspi_unregister_event_callback (void )
Un-register the user callback function.
[in] |
Returns
none
331
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_si91x_gspi_get_version#
sl_gspi_version_t sl_si91x_gspi_get_version (void )
Get the release, sqa and dev version of GSPI.
[in] |
Returns
(sl_gspi_version_t) type structure
340
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_si91x_gspi_get_status#
sl_gspi_status_t sl_si91x_gspi_get_status (sl_gspi_handle_t gspi_handle)
Get the transfer status GSPI.
[in] | gspi_handle | Pointer to the GSPI driver handle |
sl_si91x_gspi_configure_clocksl_si91x_gspi_initsl_si91x_gspi_configure_power_mode sl_si91x_gspi_set_configuration
Returns
sl_gspi_status_t type structure
353
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_si91x_gspi_get_rx_data_count#
uint32_t sl_si91x_gspi_get_rx_data_count (sl_gspi_handle_t gspi_handle)
Get data receive count of the GSPI.
[in] | gspi_handle | Pointer to the GSPI driver handle |
sl_si91x_gspi_configure_clocksl_si91x_gspi_initsl_si91x_gspi_configure_power_mode sl_si91x_gspi_set_configuration
Returns
uint32_t value of the RX data count
366
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_si91x_gspi_get_tx_data_count#
uint32_t sl_si91x_gspi_get_tx_data_count (void )
Get the transmit data count of GSPI.
[in] | Pointer to the GSPI driver handle |
sl_si91x_gspi_configure_clocksl_si91x_gspi_initsl_si91x_gspi_configure_power_mode sl_si91x_gspi_set_configuration
Returns
uint32_t value of the tx data count
379
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_si91x_gspi_get_clock_division_factor#
int32_t sl_si91x_gspi_get_clock_division_factor (sl_gspi_handle_t gspi_handle)
Fetch the clock division factor.
[in] | gspi_handle | Pointer to the GSPI driver handle |
Returns
factor(int32_t) The value of clock division factor
387
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_si91x_gspi_get_frame_length#
uint32_t sl_si91x_gspi_get_frame_length (void )
Fetch the frame length i.e., bit width.
[in] |
Returns
frame_length (uint32_t) The value of frame length
395
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
sl_si91x_gspi_set_slave_number#
__STATIC_INLINE sl_status_t sl_si91x_gspi_set_slave_number (uint8_t number)
Set the slave number in multi-slave operation.
[in] | number | Slave number |
For single slave also, this API needs to be called before transferring the data
Returns
none
405
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h