Structure to hold the parameters for the configuration of GSPI peripheral.
Public Attributes#
boolean_t
true to enable and false to disable swap read
boolean_t
true to enable and false to disable swap write
uint8_t
Bit width either 8 bit or 16 bit.
uint32_t
Mode 0 or Mode 3 of GSPI.
uint32_t
Slave select mode either software of hardware output.
uint32_t
Bitrate for setting the clock division factor.
Public Attribute Documentation#
swap_read#
boolean_t sl_gspi_control_config_t::swap_read
true to enable and false to disable swap read
Definition at line
107
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
swap_write#
boolean_t sl_gspi_control_config_t::swap_write
true to enable and false to disable swap write
Definition at line
108
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
bit_width#
uint8_t sl_gspi_control_config_t::bit_width
Bit width either 8 bit or 16 bit.
Definition at line
109
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
clock_mode#
uint32_t sl_gspi_control_config_t::clock_mode
Mode 0 or Mode 3 of GSPI.
Definition at line
110
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
slave_select_mode#
uint32_t sl_gspi_control_config_t::slave_select_mode
Slave select mode either software of hardware output.
Definition at line
111
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h
bitrate#
uint32_t sl_gspi_control_config_t::bitrate
Bitrate for setting the clock division factor.
Definition at line
112
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_gspi.h