Synchronous Serial Interface#
Modules#
Enumerations#
Enumeration for different SSI callback events.
Enumeration for different SSI peripheral clock modes.
Enumeration for different SSI peripheral device modes.
Enumeration for different SSI master slave select modes.
Enumeration for different SSI slave slave select modes.
Enumeration for different SSI instances.
Enumeration for SSI Slave numbers.
Typedefs#
renaming arm power state structure
renaming arm SPI status
Renaming SSI driver structure.
SSI Handle to be passed into APIs.
Callback typedef for SSI.
Variables#
Release version number.
sqa version number
dev version number
bit width either 8 or 16 bit
mode such as Master or Slave mode
clock mode such as CPOL0 CPHA1
Master SW or Master HW Output.
Slave SW or Slave HW Output.
baud rate for SSI
Clock Division Factor.
intf PLL control value
intf PLL clock frequency
intf PLL reference clock frequency
SoC PLL Clock frequency.
SoC PLL reference clock frequency.
SoC PLL count value.
Functions#
Configure the SSI clock.
Initialize the SSI master.
Control the SPI interface power.
Control the SPI interface.
Start receiving data from the SPI interface.
Start sending data from SPI interface.
Start sending/receiving bi-directional full duplex data to/from SPI secondary.
Get the SSI status.
Get the driver version.
Get RX transferred data count with connected device.
Get TX transferred data count with connected device.
Register the user event callback.
Unregister the user event callback.
Get the clock division factor.
Get the frame length (bit width).
Set the secondary number in multi-secondary operation.
Enumeration Documentation#
ssi_event_typedef_t#
ssi_event_typedef_t
Enumeration for different SSI callback events.
Enumerator | |
---|---|
SSI_EVENT_TRANSFER_COMPLETE | Transfer complete event. |
SSI_EVENT_DATA_LOST | Data lost event. |
SSI_EVENT_MODE_FAULT | Mode fault event. |
65
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
ssi_peripheral_clock_mode_t#
ssi_peripheral_clock_mode_t
Enumeration for different SSI peripheral clock modes.
Enumerator | |
---|---|
SL_SSI_PERIPHERAL_CPOL0_CPHA0 | SSI_PERIPHERAL MODE 0 CPOL0_CPHA0. |
SL_SSI_PERIPHERAL_CPOL0_CPHA1 | SSI_PERIPHERAL MODE 1 CPOL0_CPHA1. |
SL_SSI_PERIPHERAL_CPOL1_CPHA0 | SSI_PERIPHERAL MODE 2 CPOL1_CPHA0. |
SL_SSI_PERIPHERAL_CPOL1_CPHA1 | SSI_PERIPHERAL MODE 3 CPOL1_CPHA1. |
SL_SSI_PERIPHERAL_TI_SSI | SSI_PERIPHERAL MODE TI_SSI. |
SL_SSI_PERIPHERAL_MICROWIRE | SSI_PERIPHERAL MODE MICROWIRE. |
SL_SSI_PERIPHERAL_MODE_LAST | SSI_PERIPHERAL MODE_LAST. |
75
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
ssi_peripheral_device_mode_t#
ssi_peripheral_device_mode_t
Enumeration for different SSI peripheral device modes.
Enumerator | |
---|---|
SL_SSI_MASTER_ACTIVE | SSI DEVICE MODE MASTER. |
SL_SSI_SLAVE_ACTIVE | SSI DEVICE MODE SLAVE. |
SL_SSI_ULP_MASTER_ACTIVE | |
SL_SSI_MASTER_MODE_LAST |
88
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
ssi_master_ssm_t#
ssi_master_ssm_t
Enumeration for different SSI master slave select modes.
Enumerator | |
---|---|
SL_SSI_MASTER_UNUSED | SSI MASTER UNUSED. |
SL_SSI_MASTER_SW | SSI MASTER SW. |
SL_SSI_MASTER_HW_OUTPUT | SSI MASTER HW OUTPUT. |
SL_SSI_MASTER_SLAVE_SELECT_MODE_LAST |
99
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
ssi_slave_ssm_t#
ssi_slave_ssm_t
Enumeration for different SSI slave slave select modes.
Enumerator | |
---|---|
SL_SSI_SLAVE_HW | SSI SLAVE HW. |
SL_SSI_SLAVE_SW | SSI SLAVE SW. |
SL_SSI_SLAVE_MODE_SELECT_LAST | Last member of slave mode select. |
107
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_ssi_instance_t#
sl_ssi_instance_t
Enumeration for different SSI instances.
Enumerator | |
---|---|
SL_SSI_MASTER | SSI MASTER INSTANCE. |
SL_SSI_SLAVE | SSI SLAVE INSTANCE. |
SL_SSI_ULP_MASTER | SSI ULP MASTER INSTANCE. |
SL_SSI_INSTANCE_LAST_ENUM | Last member of enum for validation. |
114
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_ssi_slave_number_t#
sl_ssi_slave_number_t
Enumeration for SSI Slave numbers.
Enumerator | |
---|---|
SSI_SLAVE_0 | Slave No. 1. |
SSI_SLAVE_1 | Slave No. 2. |
SSI_SLAVE_2 | Slave No. 2. |
SSI_SLAVE_LAST_ENUM | Last member of enum for validation. |
147
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
Typedef Documentation#
sl_ssi_power_state_t#
typedef ARM_POWER_STATE sl_ssi_power_state_t
renaming arm power state structure
52
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_ssi_status_t#
typedef ARM_SPI_STATUS sl_ssi_status_t
renaming arm SPI status
53
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_ssi_driver_t#
typedef ARM_DRIVER_SPI sl_ssi_driver_t
Renaming SSI driver structure.
54
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_ssi_handle_t#
typedef const void* sl_ssi_handle_t
SSI Handle to be passed into APIs.
55
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_ssi_signal_event_t#
typedef ARM_SPI_SignalEvent_t sl_ssi_signal_event_t
Callback typedef for SSI.
56
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
Variable Documentation#
release#
uint8_t sl_ssi_version_t::release
Release version number.
59
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
major#
uint8_t sl_ssi_version_t::major
sqa version number
60
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
minor#
uint8_t sl_ssi_version_t::minor
dev version number
61
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
bit_width#
uint8_t sl_ssi_control_config_t::bit_width
bit width either 8 or 16 bit
125
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
device_mode#
uint32_t sl_ssi_control_config_t::device_mode
mode such as Master or Slave mode
126
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
clock_mode#
uint32_t sl_ssi_control_config_t::clock_mode
clock mode such as CPOL0 CPHA1
127
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
master_ssm#
uint32_t sl_ssi_control_config_t::master_ssm
Master SW or Master HW Output.
128
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
slave_ssm#
uint32_t sl_ssi_control_config_t::slave_ssm
Slave SW or Slave HW Output.
129
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
baud_rate#
uint32_t sl_ssi_control_config_t::baud_rate
baud rate for SSI
130
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
division_factor#
uint16_t sl_ssi_clock_config_t::division_factor
Clock Division Factor.
137
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
intf_pll_500_control_value#
uint16_t sl_ssi_clock_config_t::intf_pll_500_control_value
intf PLL control value
138
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
intf_pll_clock#
uint32_t sl_ssi_clock_config_t::intf_pll_clock
intf PLL clock frequency
139
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
intf_pll_reference_clock#
uint32_t sl_ssi_clock_config_t::intf_pll_reference_clock
intf PLL reference clock frequency
140
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
soc_pll_clock#
uint32_t sl_ssi_clock_config_t::soc_pll_clock
SoC PLL Clock frequency.
141
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
soc_pll_reference_clock#
uint32_t sl_ssi_clock_config_t::soc_pll_reference_clock
SoC PLL reference clock frequency.
142
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
soc_pll_mm_count_value#
uint8_t sl_ssi_clock_config_t::soc_pll_mm_count_value
SoC PLL count value.
143
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
Function Documentation#
sl_si91x_ssi_configure_clock#
sl_status_t sl_si91x_ssi_configure_clock (sl_ssi_clock_config_t * clock_config)
Configure the SSI clock.
[in] | clock_config | to clock config structure |
Returns
status 0 if successful, else error code.
SL_STATUS_OK (0x0000) - Success, timer clock-source parameters configured properly
162
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_si91x_ssi_init#
sl_status_t sl_si91x_ssi_init (sl_ssi_instance_t instance, sl_ssi_handle_t * ssi_handle)
Initialize the SSI master.
[in] | instance | (Master/Slave/ULP Master), ssi_handle |
N/A | ssi_handle |
Returns
status 0 if successful, else error code.
SL_STATUS_OK (0x0000) - Success, otherwise fail error code
172
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_si91x_ssi_deinit#
sl_status_t sl_si91x_ssi_deinit (sl_ssi_handle_t ssi_handle)
N/A | ssi_handle |
182
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_si91x_ssi_configure_power_mode#
sl_status_t sl_si91x_ssi_configure_power_mode (sl_ssi_handle_t ssi_handle, sl_ssi_power_state_t state)
Control the SPI interface power.
[in] | ssi_handle | handle, power state power off or full state. |
N/A | state |
Returns
status 0 if successful, else error code. SL_STATUS_INVALID_PARAMETER (0x0021) - power state is invalid SL_STATUS_OK (0x0000) - Success, otherwise error code on failure
192
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_si91x_ssi_set_configuration#
sl_status_t sl_si91x_ssi_set_configuration (sl_ssi_handle_t ssi_handle, sl_ssi_control_config_t * control_configuration)
Control the SPI interface.
[in] | ssi_handle | handle, pointer to control config structure. |
N/A | control_configuration |
Returns
status 0 if successful, else error code. SL_STATUS_INVALID_PARAMETER (0x0021) - invalid parameters SL_STATUS_OK (0x0000) - Success,
202
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_si91x_ssi_receive_data#
sl_status_t sl_si91x_ssi_receive_data (sl_ssi_handle_t ssi_handle, void * data, uint32_t data_length)
Start receiving data from the SPI interface.
[in] | ssi_handle | handle, pointer to Rx data buffer, length of data |
N/A | data | |
N/A | data_length |
Returns
status 0 if successful, else error code. SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_OK (0x0000) - Success
212
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_si91x_ssi_send_data#
sl_status_t sl_si91x_ssi_send_data (sl_ssi_handle_t ssi_handle, const void * data, uint32_t data_length)
Start sending data from SPI interface.
[in] | ssi_handle | handle, pointer to Tx data buffer, length of data |
N/A | data | |
N/A | data_length |
Returns
status 0 if successful, else error code. SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_OK (0x0000) - Success
222
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_si91x_ssi_transfer_data#
sl_status_t sl_si91x_ssi_transfer_data (sl_ssi_handle_t ssi_handle, const void * data_out, void * data_in, uint32_t data_length)
Start sending/receiving bi-directional full duplex data to/from SPI secondary.
[in] | ssi_handle | handle, pointer to Tx buffer, pointer to Rx buffer and data length |
N/A | data_out | |
N/A | data_in | |
N/A | data_length |
Returns
status 0 if successful, else error code. SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_OK (0x0000) - Success, otherwise error code on failure.
233
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_si91x_ssi_get_status#
sl_ssi_status_t sl_si91x_ssi_get_status (sl_ssi_handle_t ssi_handle)
Get the SSI status.
[in] | ssi_handle |
Get the SPI secondary status.
Returns
busy, data lost or mode fault returns as a bit field.
Returns
busy, data lost or mode fault
245
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_si91x_ssi_get_version#
sl_ssi_version_t sl_si91x_ssi_get_version (void )
Get the driver version.
[in] |
Returns
driver version.
254
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_si91x_ssi_get_rx_data_count#
uint32_t sl_si91x_ssi_get_rx_data_count (sl_ssi_handle_t ssi_handle)
Get RX transferred data count with connected device.
[in] | ssi_handle | handle |
Returns
transferred data count
270
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_si91x_ssi_get_tx_data_count#
uint32_t sl_si91x_ssi_get_tx_data_count (sl_ssi_handle_t ssi_handle)
Get TX transferred data count with connected device.
[in] | ssi_handle | handle |
Returns
transferred data count
278
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_si91x_ssi_register_event_callback#
sl_status_t sl_si91x_ssi_register_event_callback (sl_ssi_handle_t ssi_handle, sl_ssi_signal_event_t callback_event)
Register the user event callback.
[in] | ssi_handle | handle |
[in] | callback_event | pointer callback_event It will returns error if any callback is already registered. |
It registers the callback, i.e., stores the callback function address and pass to the variable that is called in Interrupt Handler. If another callback is registered without unregistering previous callback then, it returns an error code, so it is mandatory to unregister the callback before registering another callback.
292
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_si91x_gspi_unregister_event_callback#
void sl_si91x_gspi_unregister_event_callback (void )
Unregister the user event callback.
[in] |
It unregisters the callback, i.e., clears the callback function address and passes a NULL value to the variable.
301
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_si91x_ssi_get_clock_division_factor#
uint32_t sl_si91x_ssi_get_clock_division_factor (sl_ssi_handle_t ssi_handle)
Get the clock division factor.
[in] | ssi_handle | Pointer to the SSI driver handle |
Returns
factor(int32_t) Clock division factor
309
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_si91x_ssi_get_frame_length#
uint32_t sl_si91x_ssi_get_frame_length (sl_ssi_handle_t ssi_handle)
Get the frame length (bit width).
[in] | ssi_handle | Pointer to the SSI driver handle |
Returns
frame_length (uint32_t) Frame length
317
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
sl_si91x_ssi_set_slave_number#
__STATIC_INLINE sl_status_t sl_si91x_ssi_set_slave_number (uint8_t number)
Set the secondary number in multi-secondary operation.
[in] | number | Slave number |
For single secondary also, this API needs to be called before transferring the data.
Returns
none
327
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h