typedef for SSI control config struct
Public Attributes#
uint8_t
bit width either 8 or 16 bit
uint32_t
mode such as Master or Slave mode
uint32_t
clock mode such as CPOL0 CPHA1
uint32_t
Master SW or Master HW Output.
uint32_t
Slave SW or Slave HW Output.
uint32_t
baud rate for SSI
Public Attribute Documentation#
bit_width#
uint8_t sl_ssi_control_config_t::bit_width
bit width either 8 or 16 bit
Definition at line
125
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
device_mode#
uint32_t sl_ssi_control_config_t::device_mode
mode such as Master or Slave mode
Definition at line
126
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
clock_mode#
uint32_t sl_ssi_control_config_t::clock_mode
clock mode such as CPOL0 CPHA1
Definition at line
127
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
master_ssm#
uint32_t sl_ssi_control_config_t::master_ssm
Master SW or Master HW Output.
Definition at line
128
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
slave_ssm#
uint32_t sl_ssi_control_config_t::slave_ssm
Slave SW or Slave HW Output.
Definition at line
129
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h
baud_rate#
uint32_t sl_ssi_control_config_t::baud_rate
baud rate for SSI
Definition at line
130
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_ssi.h