You are viewing documentation for version:
Structure to hold the parameters of timer configurations.
Public Attributes#
uint8_t
timer number, SL_ULP_TIMER_NUMBER for default values
uint8_t
timer mode, SL_ULP_TIMER_MODE for default values
uint8_t
timer type, SL_ULP_TIMER_TYPE for default values
uint32_t
timer match value SL_ULP_TIMER_MATCH_VALUE(delay time) in microseconds
uint8_t
timer direction, SL_ULP_TIMER_DIRECTION for default values
Public Attribute Documentation#
timer_num#
uint8_t ulp_timer_config_t::timer_num
timer number, SL_ULP_TIMER_NUMBER for default values
timer_mode#
uint8_t ulp_timer_config_t::timer_mode
timer mode, SL_ULP_TIMER_MODE for default values
timer_type#
uint8_t ulp_timer_config_t::timer_type
timer type, SL_ULP_TIMER_TYPE for default values
timer_match_value#
uint32_t ulp_timer_config_t::timer_match_value
timer match value SL_ULP_TIMER_MATCH_VALUE(delay time) in microseconds
timer_direction#
uint8_t ulp_timer_config_t::timer_direction
timer direction, SL_ULP_TIMER_DIRECTION for default values