Public Attributes#

uint16_t

Event type 0x01 Connectable directed advertising (ADV_DIRECT_IND)

uint8_t

Address type of remote device.

uint8_t

Address of the remote device.

uint8_t

Directed address type.

uint8_t

Directed device address.

int8_t

rssi value

Public Attribute Documentation#

event_type#

uint16_t rsi_ble_event_directedadv_report_s::event_type

Event type 0x01 Connectable directed advertising (ADV_DIRECT_IND)


dev_addr_type#

uint8_t rsi_ble_event_directedadv_report_s::dev_addr_type

Address type of remote device.


dev_addr#

uint8_t rsi_ble_event_directedadv_report_s::dev_addr[RSI_DEV_ADDR_LEN]

Address of the remote device.


directed_addr_type#

uint8_t rsi_ble_event_directedadv_report_s::directed_addr_type

Directed address type.


directed_dev_addr#

uint8_t rsi_ble_event_directedadv_report_s::directed_dev_addr[RSI_DEV_ADDR_LEN]

Directed device address.


rssi#

int8_t rsi_ble_event_directedadv_report_s::rssi

rssi value