You are viewing documentation for version:3.1.0Public Attributes#uint8_tdev_addrBD Address of the remote device. uint16_tlocaledivediv of local device uint8_tlocalrandrand of local device uint8_tdev_addr_typeAddress type of remote device. Public Attribute Documentation#dev_addr#uint8_t rsi_bt_event_le_ltk_request_s::dev_addr[RSI_DEV_ADDR_LEN]BD Address of the remote device. localediv#uint16_t rsi_bt_event_le_ltk_request_s::localedivediv of local device localrand#uint8_t rsi_bt_event_le_ltk_request_s::localrand[8]rand of local device dev_addr_type#uint8_t rsi_bt_event_le_ltk_request_s::dev_addr_typeAddress type of remote device.