Public Attributes#

uint8_t

Remote device Address.

uint8_t

Status of the Encryption ENCRYPT_ENABLED BIT(0) --> To indicate or set encryption is enabled AUTH_LTK_OR_STK_ENC BIT(1) --> To indicate or set Authenticated Pairing and Encryption UN_AUTH_LTK_OR_STK_ENC BIT(2) --> To indicate or set UnAuthenticated pairing and Encryption AUTH_LTK_WITH_LE_SC_ENC BIT(3) --> To indicate or set Authenticated Pairing and Enc with LE SC.

uint8_t

BLE Secure Connections Enable/disable indication 0 --> Disable 1 --> Enable.

uint16_t

Local device EDIV.

uint8_t

Local RAND.

uint8_t

Local Long term Key.

uint8_t

Remote Device Address type.

Public Attribute Documentation#

dev_addr#

uint8_t rsi_bt_event_encryption_enabled_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device Address.


enabled#

uint8_t rsi_bt_event_encryption_enabled_s::enabled

Status of the Encryption ENCRYPT_ENABLED BIT(0) --> To indicate or set encryption is enabled AUTH_LTK_OR_STK_ENC BIT(1) --> To indicate or set Authenticated Pairing and Encryption UN_AUTH_LTK_OR_STK_ENC BIT(2) --> To indicate or set UnAuthenticated pairing and Encryption AUTH_LTK_WITH_LE_SC_ENC BIT(3) --> To indicate or set Authenticated Pairing and Enc with LE SC.


sc_enable#

uint8_t rsi_bt_event_encryption_enabled_s::sc_enable

BLE Secure Connections Enable/disable indication 0 --> Disable 1 --> Enable.


localediv#

uint16_t rsi_bt_event_encryption_enabled_s::localediv

Local device EDIV.


localrand#

uint8_t rsi_bt_event_encryption_enabled_s::localrand[8]

Local RAND.


localltk#

uint8_t rsi_bt_event_encryption_enabled_s::localltk[16]

Local Long term Key.


dev_addr_type#

uint8_t rsi_bt_event_encryption_enabled_s::dev_addr_type

Remote Device Address type.