< Device configuration for 91x
Public Attributes#
uint8_t
Boot option, si91x_load_image_types.
sl_mac_address_t *
mac address
Si91x Wi-Fi band.
Si91x region code.
Si91x boot configuration.
Public Attribute Documentation#
boot_option#
uint8_t sl_wifi_device_configuration_t::boot_option
Boot option, si91x_load_image_types.
Definition at line
899
of file components/si91x/inc/sl_wifi_device.h
mac_address#
sl_mac_address_t* sl_wifi_device_configuration_t::mac_address
mac address
Definition at line
900
of file components/si91x/inc/sl_wifi_device.h
band#
sl_si91x_band_mode_t sl_wifi_device_configuration_t::band
Si91x Wi-Fi band.
Definition at line
901
of file components/si91x/inc/sl_wifi_device.h
region_code#
sl_si91x_region_code_t sl_wifi_device_configuration_t::region_code
Si91x region code.
Definition at line
902
of file components/si91x/inc/sl_wifi_device.h
boot_config#
sl_si91x_boot_configuration_t sl_wifi_device_configuration_t::boot_config
Si91x boot configuration.
Definition at line
903
of file components/si91x/inc/sl_wifi_device.h