Wi-Fi performance profile.
Public Attributes#
Performance profile.
uint8_t
Set DTIM alignment required. si91x_dtim_alignment_types.
uint8_t
Default value to be used is 0.
uint16_t
Listen interval.
sl_wifi_twt_request_t
twt request.
sl_wifi_twt_selection_t
twt selection request
Public Attribute Documentation#
dtim_aligned_type#
uint8_t sl_wifi_performance_profile_t::dtim_aligned_type
Set DTIM alignment required. si91x_dtim_alignment_types.
num_of_dtim_skip#
uint8_t sl_wifi_performance_profile_t::num_of_dtim_skip
Default value to be used is 0.
twt_selection#
sl_wifi_twt_selection_t sl_wifi_performance_profile_t::twt_selection
twt selection request