Wi-Fi Client interface advance configuration.

Public Attributes#

uint32_t

< - BIT[0] of OKC is used to enable or disable opportunistic key caching (OKC), –0 – disable –1 – enable – When this is enabled, module will use cached PMKID to get MSK(Master Session Key) which is need for generating PMK which is needed for 4-way handshake.

uint32_t

Maximum number of retries before indicating join failure.

uint32_t

Scan interval between each retry.

uint32_t

Number of missed beacons that will trigger rejoin.

uint32_t

Retry enable or disable for first time joining.

Public Attribute Documentation#

eap_flags#

uint32_t sl_wifi_advanced_client_configuration_t::eap_flags

< - BIT[0] of OKC is used to enable or disable opportunistic key caching (OKC), –0 – disable –1 – enable – When this is enabled, module will use cached PMKID to get MSK(Master Session Key) which is need for generating PMK which is needed for 4-way handshake.

  • BIT[1] of OKC is used to enable or disable CA certification for PEAP connection. –0 – CA certificate is not required. –1 – CA certificate is required.

  • BIT[2-12] of OKC argument are used for Cipher list selection for EAP connection. All possible ciphers are listed below.

    BIT position

    Cipher selected

    2

    DHE-RSA-AES256-SHA256

    3

    DHE-RSA-AES128-SHA256

    4

    DHE-RSA-AES256-SHA

    5

    DHE-RSA-AES128-SHA

    6

    AES256-SHA256

    7

    AES128-SHA256

    8

    AES256-SHA

    9

    AES128-SHA

    10

    RC4-SHA

    11

    DES-CBC3-SHA

    12

    RC4-MD5

  • BIT[13-31] of OKC argument is reserved.

  • Note

    • When user sets BIT[1] and does not provide the CA certificate for PEAP connection then error is thrown. If user provides invalid CA certificate then also error is thrown. User can set either one or multiple bits from BIT[2-12] to provide the cipher's list. When user does not provide any value in OKC's BIT[2-12] then by default all the ciphers are selected. EAP Flags


max_retry_attempts#

uint32_t sl_wifi_advanced_client_configuration_t::max_retry_attempts

Maximum number of retries before indicating join failure.


scan_interval#

uint32_t sl_wifi_advanced_client_configuration_t::scan_interval

Scan interval between each retry.


beacon_missed_count#

uint32_t sl_wifi_advanced_client_configuration_t::beacon_missed_count

Number of missed beacons that will trigger rejoin.


first_time_retry_enable#

uint32_t sl_wifi_advanced_client_configuration_t::first_time_retry_enable

Retry enable or disable for first time joining.