Wi-Fi interface statistics.

Public Attributes#

uint32_t

Number of missed beacons.

uint32_t

Number of received beacons.

uint32_t

Multicast packets received.

uint32_t

Multicast packets transmitted.

uint32_t

Unicast packets received.

uint32_t

Unicast packets transmitted.

uint32_t

Number of packets dropped either at ingress or egress, due to lack of buffer memory to retain all packets.

Public Attribute Documentation#

beacon_lost_count#

uint32_t sl_wifi_statistics_t::beacon_lost_count

Number of missed beacons.


beacon_rx_count#

uint32_t sl_wifi_statistics_t::beacon_rx_count

Number of received beacons.


mcast_rx_count#

uint32_t sl_wifi_statistics_t::mcast_rx_count

Multicast packets received.


mcast_tx_count#

uint32_t sl_wifi_statistics_t::mcast_tx_count

Multicast packets transmitted.


ucast_rx_count#

uint32_t sl_wifi_statistics_t::ucast_rx_count

Unicast packets received.


ucast_tx_count#

uint32_t sl_wifi_statistics_t::ucast_tx_count

Unicast packets transmitted.


overrun_count#

uint32_t sl_wifi_statistics_t::overrun_count

Number of packets dropped either at ingress or egress, due to lack of buffer memory to retain all packets.