Wi-Fi advanced scan configuration options.
Public Attributes#
RSSI level to trigger advanced scan.
RSSI level to trigger advanced scan.
Time spent on each channel when performing active scan (milliseconds).
Time spent on each channel when performing passive scan (milliseconds).
Flag to start advanced scan immediately.
Flag to indicate to send multiple probes to AP. If set. a probe request would be sent to all access points in addition to connected SSID.
Public Attribute Documentation#
trigger_level#
int32_t sl_wifi_advanced_scan_configuration_t::trigger_level
RSSI level to trigger advanced scan.
trigger_level_change#
uint32_t sl_wifi_advanced_scan_configuration_t::trigger_level_change
RSSI level to trigger advanced scan.
active_channel_time#
uint16_t sl_wifi_advanced_scan_configuration_t::active_channel_time
Time spent on each channel when performing active scan (milliseconds).
passive_channel_time#
uint16_t sl_wifi_advanced_scan_configuration_t::passive_channel_time
Time spent on each channel when performing passive scan (milliseconds).
enable_instant_scan#
uint8_t sl_wifi_advanced_scan_configuration_t::enable_instant_scan
Flag to start advanced scan immediately.
enable_multi_probe#
uint8_t sl_wifi_advanced_scan_configuration_t::enable_multi_probe
Flag to indicate to send multiple probes to AP. If set. a probe request would be sent to all access points in addition to connected SSID.