ADC#

Modules#

sl_adc_threshold_config_t

sl_adc_fifo_thrld_config_t

sl_adc_clock_config_t

sl_adc_version_t

Enumerations#

enum
SL_ADC_SINGLE_ENDED
SL_ADC_DIFFERENTIAL
SL_ADC_INPUT_TYPE_LAST
}

Enumeration for ADC input type.

enum
SL_ADC_FIFO_MODE = ADC_FIFOMODE_ENABLE
SL_ADC_STATIC_MODE = ADC_STATICMODE_ENABLE
SL_ADC_OPERATION_MODE_LAST
}

Enumeration for ADC operation mode.

enum
SL_ADC_INTERNAL_DMA = INTERNAL_DMA_EN
SL_ADC_EXTERNAL_DMA = EXTERNAL_DMA_EN
SL_ADC_DMA_TYPE_LAST
}

Enumeration for ADC DMA type.

enum
SL_ADC_SINGLE_CHNL = DYNAMIC_MODE_DI
SL_ADC_MULTI_CHNL = DYNAMIC_MODE_EN
SL_ADC_CHANNEL_TYPE_LAST
}

Enumeration for ADC multiple channel selection.

enum
SL_ULP_TIMER_EXT_TRIGGER = ULP_TIMER_EXT_TRIGGER
SL_ULP_GPIO_EXT_TRIGGER = ULP_GPIO_EXT_TRIGGER
SL_M4_CT_EXT_TRIGGER = M4_CT_EXT_TRIGGER
SL_ADC_EXT_TRIGGER_TYPE_LAST
}

Enumeration for ADC external trigger type.

enum
SL_ADC_EXT_TRIGGER_1 = DETECTION1
SL_ADC_EXT_TRIGGER_2 = DETECTION2
SL_ADC_EXT_TRIGGER_3 = DETECTION3
SL_ADC_EXT_TRIGGER_4 = DETECTION4
SL_ADC_EXT_TRIGGER_LAST
}

Enumeration for ADC external trigger number.

enum
SL_ADC_EXT_TRIGGER_POS_EDGE = POSITIVE_EDGE
SL_ADC_EXT_TRIGGER_NEG_EDGE = NEGATIVE_EDGE
SL_ADC_EXT_TRIGGER_POS_NEG_EDGE = POS_NEG_EDGE
SL_ADC_EXT_TRIGGER_EDGE_LAST
}

Enumeration for ADC external trigger edge selection.

enum
SL_ADC_EXT_TRIGGER_SEL_1 = EXT_TRIGGER_SEL1
SL_ADC_EXT_TRIGGER_SEL_2 = EXT_TRIGGER_SEL2
SL_ADC_EXT_TRIGGER_SEL_3 = EXT_TRIGGER_SEL3
SL_ADC_EXT_TRIGGER_SEL_4 = EXT_TRIGGER_SEL4
SL_ADC_EXT_TRIGGER_SEL_LAST
}

Enumeration for ADC external trigger selection.

enum
SL_ADC_CHANNEL_0
SL_ADC_CHANNEL_1
SL_ADC_CHANNEL_2
SL_ADC_CHANNEL_3
SL_ADC_CHANNEL_4
SL_ADC_CHANNEL_5
SL_ADC_CHANNEL_6
SL_ADC_CHANNEL_7
SL_ADC_CHANNEL_8
SL_ADC_CHANNEL_9
SL_ADC_CHANNEL_10
SL_ADC_CHANNEL_11
SL_ADC_CHANNEL_12
SL_ADC_CHANNEL_13
SL_ADC_CHANNEL_14
SL_ADC_CHANNEL_15
}

Enumeration for ADC channel.

Typedefs#

typedef adc_ch_config_t

Renamed ADC channel configuration structure.

typedef adc_config_t

Renamed ADC configuration structure.

typedef adc_inter_config_t

Renamed ADC internal configuration structure.

typedef adc_extr_config_t

Renamed ADC external trigger configuration structure.

typedef void(*
sl_adc_callback_t)(uint8_t channel, uint8_t event)

Typedef for the function pointer of the callback function.

Functions#

sl_status_t
sl_si91x_adc_configure_clock(sl_adc_clock_config_t *clock_configuration)

Configure the ADC clock.

sl_status_t
sl_si91x_adc_init(sl_adc_channel_config_t adc_channel_config, sl_adc_config_t adc_config, float vref_value)

Initialize the ADC peripheral.

sl_status_t
sl_si91x_adc_set_channel_configuration(sl_adc_channel_config_t adc_channel_config, sl_adc_config_t adc_config)

Configure ADC channel parameters.

sl_status_t
sl_si91x_adc_register_event_callback(sl_adc_callback_t callback_event)

Register the user callback function.

void

Un-register the user callback function.

sl_status_t
sl_si91x_adc_configure_external_trigger(sl_adc_external_config_t adc_external_trigger)

Configure the ADC external trigger.

sl_status_t
sl_si91x_adc_configure_channel_sampling_rate(sl_adc_internal_config_t adc_internal_config, uint8_t channel_num)

Configure the ADC sampling rate for ADC channels.

sl_status_t
sl_si91x_adc_get_external_trigger_status(sl_adc_external_config_t adc_external_trigger, uint8_t *ext_trigger)

Read the ADC external trigger status.

sl_status_t
sl_si91x_adc_clear_external_trigger(sl_adc_external_config_t adc_external_trigger)

Clear the ADC external trigger status.

sl_status_t
sl_si91x_adc_configure_ping_pong_memory_address(sl_adc_internal_config_t adc_internal_config, uint8_t channel_num)

Configure the ADC ping and pong memory location and length.

sl_status_t
sl_si91x_adc_enable_ping_pong(uint8_t channel_num)

Enable ping pong for corresponding ADC channels.

sl_status_t
sl_si91x_adc_disable_ping_pong(uint8_t channel_num)

Disable ping pong for corresponding ADC channels.

sl_status_t

Enable internal DMA for corresponding ADC channels.

sl_status_t

Disable internal dma channel for corresponding ADC channels.

sl_status_t
sl_si91x_adc_configure_static_mode(sl_adc_channel_config_t adc_channel_config, uint8_t channel_num)

Configure the ADC in Static Mode.

sl_status_t
sl_si91x_adc_configure_fifo_mode(sl_adc_channel_config_t adc_channel_config, uint8_t channel_num)

Configure the ADC in FIFO Mode.

sl_status_t
sl_si91x_adc_channel_enable(uint8_t channel_num)

Enable the ADC channel.

sl_status_t
sl_si91x_adc_channel_disable(uint8_t channel_num)

Disable the ADC channel.

sl_status_t
sl_si91x_adc_set_power_mode(POWER_STATE state)

Set to Power On and off for ADC.

sl_status_t

Enable or Disable Noise averaging mode.

sl_status_t

Enable temp-sensor for ADC.

sl_status_t
sl_si91x_adc_fifo_threshold_configuration(sl_adc_config_t adc_config, sl_adc_fifo_thrld_config_t adc_fifo_threshold)

Configuring ADC fifo threshold.

sl_status_t
sl_si91x_adc_threshold_configuration(sl_adc_threshold_config_t adc_threshold)

Configure the ADC threshold to compare threshold value with ADC data.

sl_status_t
sl_si91x_adc_read_data(sl_adc_channel_config_t adcchconfig, uint8_t channel_num)

Read the ADC samples when ulp memories are used.

sl_status_t
sl_si91x_adc_read_data_static(sl_adc_channel_config_t adc_channel_config, sl_adc_config_t adc_config, uint16_t *adc_value)

Read the ADC samples when static mode is enabled.

uint32_t
sl_si91x_adc_get_sampling_rate(uint8_t channel_num)

Read the ADC sampling rate when static mode is enabled.

sl_status_t
sl_si91x_adc_deinit(sl_adc_config_t adc_config)

De-initialize the ADC.

sl_status_t
sl_si91x_adc_start(sl_adc_config_t adc_config)

Start the ADC operation.

sl_status_t
sl_si91x_adc_stop(sl_adc_config_t adc_config)

Stop the ADC operation.

Get the release, sqa and dev version of ADC.

Macros#

#define
SL_INTERNAL_DMA INTERNAL_DMA
#define
SL_ADC_STATIC_MODE_EVENT ADC_STATIC_MODE_CALLBACK
#define
SIGN_BIT BIT(11)

Enumeration Documentation#

sl_adc_input_type_typedef_t#

sl_adc_input_type_typedef_t

Enumeration for ADC input type.

Enumerator
SL_ADC_SINGLE_ENDED

Input type single ended.

SL_ADC_DIFFERENTIAL

Input type differential.

SL_ADC_INPUT_TYPE_LAST

Last member of enum for validation.


sl_adc_operation_mode_typedef_t#

sl_adc_operation_mode_typedef_t

Enumeration for ADC operation mode.

Enumerator
SL_ADC_FIFO_MODE

operation mode as fifo mode

SL_ADC_STATIC_MODE

operation mode as static mode

SL_ADC_OPERATION_MODE_LAST

Last member of enum for validation.


sl_adc_dma_type_typedef_t#

sl_adc_dma_type_typedef_t

Enumeration for ADC DMA type.

Enumerator
SL_ADC_INTERNAL_DMA

Internal DMA type.

SL_ADC_EXTERNAL_DMA

External DMA type.

SL_ADC_DMA_TYPE_LAST

Last member of enum for validation.


sl_adc_channel_type_typedef_t#

sl_adc_channel_type_typedef_t

Enumeration for ADC multiple channel selection.

Enumerator
SL_ADC_SINGLE_CHNL

Dynamic mode disable.

SL_ADC_MULTI_CHNL

Dynamic mode enable.

SL_ADC_CHANNEL_TYPE_LAST

Last member of enum for validation.


sl_adc_ext_trigger_type_t#

sl_adc_ext_trigger_type_t

Enumeration for ADC external trigger type.

Enumerator
SL_ULP_TIMER_EXT_TRIGGER

ULP timer external trigger type.

SL_ULP_GPIO_EXT_TRIGGER

ULP gpio external trigger type.

SL_M4_CT_EXT_TRIGGER

M4 CT external trigger type.

SL_ADC_EXT_TRIGGER_TYPE_LAST

Last member of enum for validation.


sl_adc_ext_trigger_num_t#

sl_adc_ext_trigger_num_t

Enumeration for ADC external trigger number.

Enumerator
SL_ADC_EXT_TRIGGER_1

External trigger detection 1.

SL_ADC_EXT_TRIGGER_2

External trigger detection 2.

SL_ADC_EXT_TRIGGER_3

External trigger detection 3.

SL_ADC_EXT_TRIGGER_4

External trigger detection 4.

SL_ADC_EXT_TRIGGER_LAST

Last member of enum for validation.


sl_adc_ext_trigger_edge_t#

sl_adc_ext_trigger_edge_t

Enumeration for ADC external trigger edge selection.

Enumerator
SL_ADC_EXT_TRIGGER_POS_EDGE

External trigger positive edge.

SL_ADC_EXT_TRIGGER_NEG_EDGE

External trigger negative edge.

SL_ADC_EXT_TRIGGER_POS_NEG_EDGE

External trigger positive and negative edge.

SL_ADC_EXT_TRIGGER_EDGE_LAST

Last member of enum for validation.


sl_adc_ext_trigger_sel_t#

sl_adc_ext_trigger_sel_t

Enumeration for ADC external trigger selection.

Enumerator
SL_ADC_EXT_TRIGGER_SEL_1

External trigger selection 1.

SL_ADC_EXT_TRIGGER_SEL_2

External trigger selection 2.

SL_ADC_EXT_TRIGGER_SEL_3

External trigger selection 3.

SL_ADC_EXT_TRIGGER_SEL_4

External trigger selection 4.

SL_ADC_EXT_TRIGGER_SEL_LAST

Last member of enum for validation.


sl_adc_channel_id_t#

sl_adc_channel_id_t

Enumeration for ADC channel.

Enumerator
SL_ADC_CHANNEL_0

ADC channel 1.

SL_ADC_CHANNEL_1

ADC channel 2.

SL_ADC_CHANNEL_2

ADC channel 3.

SL_ADC_CHANNEL_3

ADC channel 4.

SL_ADC_CHANNEL_4

ADC channel 5.

SL_ADC_CHANNEL_5

ADC channel 6.

SL_ADC_CHANNEL_6

ADC channel 7.

SL_ADC_CHANNEL_7

ADC channel 8.

SL_ADC_CHANNEL_8

ADC channel 9.

SL_ADC_CHANNEL_9

ADC channel 10.

SL_ADC_CHANNEL_10

ADC channel 11.

SL_ADC_CHANNEL_11

ADC channel 12.

SL_ADC_CHANNEL_12

ADC channel 13.

SL_ADC_CHANNEL_13

ADC channel 14.

SL_ADC_CHANNEL_14

ADC channel 15.

SL_ADC_CHANNEL_15

ADC channel 16.


Typedef Documentation#

sl_adc_channel_config_t#

typedef adc_ch_config_t sl_adc_channel_config_t

Renamed ADC channel configuration structure.


sl_adc_config_t#

typedef adc_config_t sl_adc_config_t

Renamed ADC configuration structure.


sl_adc_internal_config_t#

typedef adc_inter_config_t sl_adc_internal_config_t

Renamed ADC internal configuration structure.


sl_adc_external_config_t#

typedef adc_extr_config_t sl_adc_external_config_t

Renamed ADC external trigger configuration structure.


sl_adc_callback_t#

typedef void(* sl_adc_callback_t) (uint8_t channel, uint8_t event) )(uint8_t channel, uint8_t event)

Typedef for the function pointer of the callback function.


Function Documentation#

sl_si91x_adc_configure_clock#

sl_status_t sl_si91x_adc_configure_clock (sl_adc_clock_config_t * clock_configuration)

Configure the ADC clock.

Parameters
TypeDirectionArgument NameDescription
sl_adc_clock_config_t *[in]clock_configuration

: clock structure variables

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid

    • SL_STATUS_FAIL (0x0001) - The function is failed

    • SL_STATUS_NOT_INITIALIZED (0x0011) - Clock is not initialized


sl_si91x_adc_init#

sl_status_t sl_si91x_adc_init (sl_adc_channel_config_t adc_channel_config, sl_adc_config_t adc_config, float vref_value)

Initialize the ADC peripheral.

Parameters
TypeDirectionArgument NameDescription
sl_adc_channel_config_t[in]adc_channel_config

: ADC channels configuration structure variable.

sl_adc_config_t[in]adc_config

: ADC operation configuration structure variable.

float[in]vref_value

: Reference voltage.

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid

    • SL_STATUS_BUSY (0x0004) - The function is already active

    • SL_STATUS_INVALID_COUNT (0x002B) - Mismatch count

    • SL_STATUS_INVALID_RANGE (0x0028) - Mismatch Range


sl_si91x_adc_set_channel_configuration#

sl_status_t sl_si91x_adc_set_channel_configuration (sl_adc_channel_config_t adc_channel_config, sl_adc_config_t adc_config)

Configure ADC channel parameters.

Parameters
TypeDirectionArgument NameDescription
sl_adc_channel_config_t[in]adc_channel_config

: ADC channels configuration structure variable.

sl_adc_config_t[in]adc_config

: ADC operation configuration structure variable.

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid

    • SL_STATUS_INVALID_RANGE (0x0028) - Mismatch Range


sl_si91x_adc_register_event_callback#

sl_status_t sl_si91x_adc_register_event_callback (sl_adc_callback_t callback_event)

Register the user callback function.

Parameters
TypeDirectionArgument NameDescription
sl_adc_callback_t[in]callback_event

Pointer to the function which needs to be called at the time of interrupt

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer

    • SL_STATUS_BUSY (0x0004) - Driver is busy


sl_si91x_adc_unregister_event_callback#

void sl_si91x_adc_unregister_event_callback (void )

Un-register the user callback function.

Parameters
TypeDirectionArgument NameDescription
void[in]

Returns

  • none


sl_si91x_adc_configure_external_trigger#

sl_status_t sl_si91x_adc_configure_external_trigger (sl_adc_external_config_t adc_external_trigger)

Configure the ADC external trigger.

Parameters
TypeDirectionArgument NameDescription
sl_adc_external_config_t[in]adc_external_trigger

: ADC external trigger configuration structure variable.

This API is used to mux select to choose between ulp_timer, ulp_gpio, M4_timer based on this detection edge and channel trigger will interrupt.

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid


sl_si91x_adc_configure_channel_sampling_rate#

sl_status_t sl_si91x_adc_configure_channel_sampling_rate (sl_adc_internal_config_t adc_internal_config, uint8_t channel_num)

Configure the ADC sampling rate for ADC channels.

Parameters
TypeDirectionArgument NameDescription
sl_adc_internal_config_t[in]adc_internal_config

: Channel offset and frequency for each channel to set sampling rate.

uint8_t[in]channel_num

: Channel number

Returns

  • sl_status_t : Returns 'SL_STATUS_OK' on successful execution.


sl_si91x_adc_get_external_trigger_status#

sl_status_t sl_si91x_adc_get_external_trigger_status (sl_adc_external_config_t adc_external_trigger, uint8_t * ext_trigger)

Read the ADC external trigger status.

Parameters
TypeDirectionArgument NameDescription
sl_adc_external_config_t[in]adc_external_trigger

: ADC external trigger configuration structure variable.

uint8_t *[in]ext_trigger

: The status of external trigger will be store in this.

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid


sl_si91x_adc_clear_external_trigger#

sl_status_t sl_si91x_adc_clear_external_trigger (sl_adc_external_config_t adc_external_trigger)

Clear the ADC external trigger status.

Parameters
TypeDirectionArgument NameDescription
sl_adc_external_config_t[in]adc_external_trigger

: ADC external trigger configuration structure variable.

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid


sl_si91x_adc_configure_ping_pong_memory_address#

sl_status_t sl_si91x_adc_configure_ping_pong_memory_address (sl_adc_internal_config_t adc_internal_config, uint8_t channel_num)

Configure the ADC ping and pong memory location and length.

Parameters
TypeDirectionArgument NameDescription
sl_adc_internal_config_t[in]adc_internal_config

: ADC internal trigger configuration structure variable.

uint8_t[in]channel_num

: Channel number

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid


sl_si91x_adc_enable_ping_pong#

sl_status_t sl_si91x_adc_enable_ping_pong (uint8_t channel_num)

Enable ping pong for corresponding ADC channels.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]channel_num

: Channel number

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid


sl_si91x_adc_disable_ping_pong#

sl_status_t sl_si91x_adc_disable_ping_pong (uint8_t channel_num)

Disable ping pong for corresponding ADC channels.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]channel_num

: Channel number

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid


sl_si91x_adc_internal_per_channel_dma_enable#

sl_status_t sl_si91x_adc_internal_per_channel_dma_enable (uint8_t channel_num)

Enable internal DMA for corresponding ADC channels.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]channel_num

: Channel number

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid


sl_si91x_adc_internal_per_channel_dma_disable#

sl_status_t sl_si91x_adc_internal_per_channel_dma_disable (uint8_t channel_num)

Disable internal dma channel for corresponding ADC channels.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]channel_num

: Channel number

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid


sl_si91x_adc_configure_static_mode#

sl_status_t sl_si91x_adc_configure_static_mode (sl_adc_channel_config_t adc_channel_config, uint8_t channel_num)

Configure the ADC in Static Mode.

Parameters
TypeDirectionArgument NameDescription
sl_adc_channel_config_t[in]adc_channel_config

: ADC channels configuration structure variable.

uint8_tN/Achannel_num

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid

    • SL_STATUS_INVALID_RANGE (0x0028) - Mismatch Range


sl_si91x_adc_configure_fifo_mode#

sl_status_t sl_si91x_adc_configure_fifo_mode (sl_adc_channel_config_t adc_channel_config, uint8_t channel_num)

Configure the ADC in FIFO Mode.

Parameters
TypeDirectionArgument NameDescription
sl_adc_channel_config_t[in]adc_channel_config

: ADC channels configuration structure variable.

uint8_t[in]channel_num

: Channel number

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid

    • SL_STATUS_INVALID_RANGE (0x0028) - Mismatch Range


sl_si91x_adc_channel_enable#

sl_status_t sl_si91x_adc_channel_enable (uint8_t channel_num)

Enable the ADC channel.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]channel_num

: Channel number

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid


sl_si91x_adc_channel_disable#

sl_status_t sl_si91x_adc_channel_disable (uint8_t channel_num)

Disable the ADC channel.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]channel_num

: Channel number

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid


sl_si91x_adc_set_power_mode#

sl_status_t sl_si91x_adc_set_power_mode (POWER_STATE state)

Set to Power On and off for ADC.

Parameters
TypeDirectionArgument NameDescription
POWER_STATE[in]state

: ADC_POWER_ON - To powerup adc powergates, ADC_POWER_OFF - To powerdown adc powergates

Returns

  • status 0 if successful,

    • SL_STATUS_OK (0x0000) - Success


sl_si91x_adc_set_noise_average_mode#

sl_status_t sl_si91x_adc_set_noise_average_mode (boolean_t state)

Enable or Disable Noise averaging mode.

Parameters
TypeDirectionArgument NameDescription
boolean_t[in]state

: 1 - To enable noise averaging mode, 0 - To disable noise averaging mode

Returns

  • Returns 'SL_STATUS_OK' on successful execution.


sl_si91x_adc_temperature_sensor_enable#

sl_status_t sl_si91x_adc_temperature_sensor_enable (void )

Enable temp-sensor for ADC.

Parameters
TypeDirectionArgument NameDescription
void[in]

Returns

  • Returns 'SL_STATUS_OK' on successful execution.


sl_si91x_adc_fifo_threshold_configuration#

sl_status_t sl_si91x_adc_fifo_threshold_configuration (sl_adc_config_t adc_config, sl_adc_fifo_thrld_config_t adc_fifo_threshold)

Configuring ADC fifo threshold.

Parameters
TypeDirectionArgument NameDescription
sl_adc_config_t[in]adc_config

: ADC operation configuration structure variable.

sl_adc_fifo_thrld_config_t[in]adc_fifo_threshold

: ADC fifo structure variable like aempty fifo, afull fifo threshold level.

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid

    • SL_STATUS_INVALID_RANGE (0x0028) - Mismatch Range


sl_si91x_adc_threshold_configuration#

sl_status_t sl_si91x_adc_threshold_configuration (sl_adc_threshold_config_t adc_threshold)

Configure the ADC threshold to compare threshold value with ADC data.

Parameters
TypeDirectionArgument NameDescription
sl_adc_threshold_config_t[in]adc_threshold

: ADC threshold configuration structure variables.

Returns

  • Returns 'SL_STATUS_OK' on successful execution.


sl_si91x_adc_read_data#

sl_status_t sl_si91x_adc_read_data (sl_adc_channel_config_t adcchconfig, uint8_t channel_num)

Read the ADC samples when ulp memories are used.

Parameters
TypeDirectionArgument NameDescription
sl_adc_channel_config_t[in]adcchconfig

: ADC channels configuration structure variable.

uint8_t[in]channel_num

channel_num : Channel number

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid

    • SL_STATUS_INVALID_RANGE (0x0028) - Mismatch Range


sl_si91x_adc_read_data_static#

sl_status_t sl_si91x_adc_read_data_static (sl_adc_channel_config_t adc_channel_config, sl_adc_config_t adc_config, uint16_t * adc_value)

Read the ADC samples when static mode is enabled.

Parameters
TypeDirectionArgument NameDescription
sl_adc_channel_config_t[in]adc_channel_config

: ADC channels configuration structure variable.

sl_adc_config_t[in]adc_config

: Store the reading data on adc_value.

uint16_t *N/Aadc_value

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid

    • SL_STATUS_INVALID_RANGE (0x0028) - Mismatch Range


sl_si91x_adc_get_sampling_rate#

uint32_t sl_si91x_adc_get_sampling_rate (uint8_t channel_num)

Read the ADC sampling rate when static mode is enabled.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]channel_num

: Channel number

Returns

  • Returns sampling rate what it get from register


sl_si91x_adc_deinit#

sl_status_t sl_si91x_adc_deinit (sl_adc_config_t adc_config)

De-initialize the ADC.

Parameters
TypeDirectionArgument NameDescription
sl_adc_config_t[in]adc_config

: ADC operation configuration structure variable.

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid


sl_si91x_adc_start#

sl_status_t sl_si91x_adc_start (sl_adc_config_t adc_config)

Start the ADC operation.

Parameters
TypeDirectionArgument NameDescription
sl_adc_config_t[in]adc_config

: ADC operation configuration structure variable.

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid


sl_si91x_adc_stop#

sl_status_t sl_si91x_adc_stop (sl_adc_config_t adc_config)

Stop the ADC operation.

Parameters
TypeDirectionArgument NameDescription
sl_adc_config_t[in]adc_config

: ADC operation configuration structure variable.

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid


sl_si91x_adc_get_version#

sl_adc_version_t sl_si91x_adc_get_version (void )

Get the release, sqa and dev version of ADC.

Parameters
TypeDirectionArgument NameDescription
void[in]

Returns


Macro Definition Documentation#

SL_INTERNAL_DMA#

#define SL_INTERNAL_DMA
Value:
INTERNAL_DMA

SL_ADC_STATIC_MODE_EVENT#

#define SL_ADC_STATIC_MODE_EVENT
Value:
ADC_STATIC_MODE_CALLBACK

SIGN_BIT#

#define SIGN_BIT
Value:
BIT(11)