Watchdog Timer#
Modules#
Enumerations#
Enumeration to represent possible time delays values for WDT interrupt time and system reset time with 32 KHZ clock freq.
Typedefs#
Typedef for the function pointer of the callback function.
Renaming low frequency fsm-clock type enum.
Renaming high frequency fsm-clock type enum.
Functions#
Initialize the Watchdog timer (Power-up WDT and enables it to run during sleep mode).
Configure timer clock sources.
Configure clock sources & timer parameters like interrupt time(WDT restart time), system reset time & window time (another time stamp for WDT restart, if required).
Register Watchdog timer timeout callback and enables NVIC.
Set Watchdog timer interrupt time(upper time-stamp for WDT restart) duration.
Read Watchdog timer interrupt time set value (in terms of power of two)
Set Watchdog timer system-reset time duration.
Read Watchdog timer system-reset time set value (in terms of power of two).
Set Watchdog timer window time value (lower time-stamp for WDT restart).
Read Watchdog timer window time set value (in terms of power of two).
Read Watchdog timer system-reset status.
De-initialize Watchdog timer, mask its interrupt, de-power and disable timer.
Unregister Watchdog timer timeout callback.
Get the release version of Watchdog timer.
Start and enable the Watchdog timer.
Stop Watchdog timer by disabling it.
Restart (kick) an already running Watchdog timer.
Enable the Watchdog timer to reset the system on processor lockup.
Disable the Watchdog timer to reset system on processor lockup.
Enumeration Documentation#
bg_pmu_clock_t#
bg_pmu_clock_t
Enumeration to represent bg-pmu clock sources.
| Enumerator | |
|---|---|
| RO_32KHZ_CLOCK | RO_32KHz_clock. |
| MCU_FSM__CLOCK | mcu_fsm__clock |
time_delays_t#
time_delays_t
Enumeration to represent possible time delays values for WDT interrupt time and system reset time with 32 KHZ clock freq.
| Enumerator | |
|---|---|
| TIME_DELAY_0 | for time delay of 0.03125 milliseconds |
| TIME_DELAY_1 | for time delay of 0.0625 milliseconds |
| TIME_DELAY_2 | for time delay of 0.125 milliseconds |
| TIME_DELAY_3 | for time delay of 0.25 milliseconds |
| TIME_DELAY_4 | for time delay of 0.5 milliseconds |
| TIME_DELAY_5 | for time delay of 1 milliseconds |
| TIME_DELAY_6 | for time delay of 2 milliseconds |
| TIME_DELAY_7 | for time delay of 4 milliseconds |
| TIME_DELAY_8 | for time delay of 8 milliseconds |
| TIME_DELAY_9 | for time delay of 16 milliseconds |
| TIME_DELAY_10 | for time delay of 32 milliseconds |
| TIME_DELAY_11 | for time delay of 64 milliseconds |
| TIME_DELAY_12 | for time delay of 128 milliseconds |
| TIME_DELAY_13 | for time delay of 256 milliseconds |
| TIME_DELAY_14 | for time delay of 512 milliseconds |
| TIME_DELAY_15 | for time delay of 1.024 seconds |
| TIME_DELAY_16 | for time delay of 2.048 seconds |
| TIME_DELAY_17 | for time delay of 4.096 seconds |
| TIME_DELAY_18 | for time delay of 8.192 seconds |
| TIME_DELAY_19 | for time delay of 16.384 seconds |
| TIME_DELAY_20 | for time delay of 32.768 seconds |
| TIME_DELAY_21 | for time delay of 65.536 seconds |
| TIME_DELAY_22 | for time delay of 131.072 seconds |
| TIME_DELAY_23 | for time delay of 262.144 seconds |
| TIME_DELAY_24 | for time delay of 524.288 seconds |
| TIME_DELAY_25 | for time delay of 1048.576 seconds |
| TIME_DELAY_26 | for time delay of 2097.152 seconds |
| TIME_DELAY_27 | for time delay of 4194.304 seconds |
| TIME_DELAY_28 | for time delay of 8388.60 seconds |
| TIME_DELAY_29 | for time delay of 16777.216 seconds |
| TIME_DELAY_30 | for time delay of 33554.432 seconds |
| TIME_DELAY_31 | for time delay of 67108.864 seconds |
| TIME_DELAY_LAST | for time delay value validation |
Typedef Documentation#
watchdog_timer_callback_t#
typedef void(* watchdog_timer_callback_t) (void) )(void)
Typedef for the function pointer of the callback function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | data | (void *)extra parameter for user application |
low_freq_fsm_clock_t#
typedef AON_CLK_T low_freq_fsm_clock_t
Renaming low frequency fsm-clock type enum.
high_freq_fsm_clock_t#
typedef FSM_CLK_T high_freq_fsm_clock_t
Renaming high frequency fsm-clock type enum.
Function Documentation#
sl_si91x_watchdog_init_timer#
void sl_si91x_watchdog_init_timer (void )
Initialize the Watchdog timer (Power-up WDT and enables it to run during sleep mode).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Also un-masks its interrupt & sets RTC clock time-period.
Returns
none
sl_si91x_watchdog_configure_clock#
sl_status_t sl_si91x_watchdog_configure_clock (watchdog_timer_clock_config_t * timer_clk_config_ptr)
Configure timer clock sources.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| watchdog_timer_clock_config_t * | [in] | timer_clk_config_ptr | Pointer to timer clock configuration structure |
Pre-conditions:
Returns
status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - Timer configuration structure members have invalid values, for members watchdog_timer_clock_config_t
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0x0000) - Success, timer clock-source parameters configured properly
sl_si91x_watchdog_set_configuration#
sl_status_t sl_si91x_watchdog_set_configuration (watchdog_timer_config_t * timer_config_ptr)
Configure clock sources & timer parameters like interrupt time(WDT restart time), system reset time & window time (another time stamp for WDT restart, if required).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| watchdog_timer_config_t * | [in] | timer_config_ptr | Pointer to timer clock configuration structure |
Also un-masks its interrupt & sets RTC clock time-period.
Returns
status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - Timer configuration structure members have invalid values, for members watchdog_timer_config_t
SL_STATUS_INVALID_CONFIGURATION (0x0023) - Timer configuration structure member 'system_reset_time' is less than or equal to 'interrupt_time'. It should be greater than interrupt time of timer.
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0x0000) - Success, timer parameters configured properly
sl_si91x_watchdog_register_timeout_callback#
sl_status_t sl_si91x_watchdog_register_timeout_callback (watchdog_timer_callback_t on_timeout_callback)
Register Watchdog timer timeout callback and enables NVIC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| watchdog_timer_callback_t | [in] | on_timeout_callback | (function pointer) Callback function pointer to be called when timer timeout interrupt occurred. |
Returns
status 0 if successful, else error code as follows:
SL_STATUS_NULL_POINTER (0x0022) - Callback function pointer parameter is a null pointer.
SL_STATUS_BUSY (0x0004) - The callback is already registered, the user must unregister the previous callback before registering again
SL_STATUS_OK (0x0000) - Successfully registered timer timer-out callback
sl_si91x_watchdog_set_interrupt_time#
sl_status_t sl_si91x_watchdog_set_interrupt_time (time_delays_t interrupt_time)
Set Watchdog timer interrupt time(upper time-stamp for WDT restart) duration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| time_delays_t | [in] | interrupt_time | (time_delays_t), timer timeout interrupt duration, Number of clock pulses = 2^(interrupt_time), time_delays_t |
Pre-conditions:
Returns
status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - 'interrupt_time' parameter has an invalid value.
SL_STATUS_INVALID_CONFIGURATION (0x0023) - 'interrupt_time' value is less than window time or greater than system reset time
SL_STATUS_OK (0x0000) - Successfully set watchdog timer timeout time value
sl_si91x_watchdog_get_interrupt_time#
uint8_t sl_si91x_watchdog_get_interrupt_time (void )
Read Watchdog timer interrupt time set value (in terms of power of two)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Pre-conditions:
Returns
returns interrupt time (uint8_t) value, time_delays_t
sl_si91x_watchdog_set_system_reset_time#
sl_status_t sl_si91x_watchdog_set_system_reset_time (time_delays_t system_reset_time)
Set Watchdog timer system-reset time duration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| time_delays_t | [in] | system_reset_time | (time_delays_t) timer system-reset duration, Number of clock pulses = 2^(system_reset_time), time_delays_t |
Returns
status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - 'system_reset_time' parameter has an invalid value.
SL_STATUS_INVALID_CONFIGURATION (0x0023) - 'system_reset_time' value is less than window time or interrupt time
SL_STATUS_OK (0x0000) - Successfully set watchdog timer system-reset time value
sl_si91x_watchdog_get_system_reset_time#
uint8_t sl_si91x_watchdog_get_system_reset_time (void )
Read Watchdog timer system-reset time set value (in terms of power of two).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Pre-conditions:
Returns
returns system-reset time (uint8_t) value, time_delays_t
sl_si91x_watchdog_set_window_time#
sl_status_t sl_si91x_watchdog_set_window_time (time_delays_t window_time)
Set Watchdog timer window time value (lower time-stamp for WDT restart).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| time_delays_t | [in] | window_time | (time_delays_t), timer window time, Number of clock pulses = 2^(window_time),time_delays_t |
Pre-conditions:
Returns
status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - 'window_time' parameter has an invalid value.
SL_STATUS_INVALID_CONFIGURATION (0x0023) - 'window_time' value is greater than interrupt time or system reset time
SL_STATUS_OK (0x0000) - Successfully set watchdog timer window time value
sl_si91x_watchdog_get_window_time#
uint8_t sl_si91x_watchdog_get_window_time (void )
Read Watchdog timer window time set value (in terms of power of two).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Pre-conditions:
Returns
returns window time (uint8_t) value, time_delays_t
sl_si91x_watchdog_get_timer_system_reset_status#
boolean_t sl_si91x_watchdog_get_timer_system_reset_status (void )
Read Watchdog timer system-reset status.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Returns
returns true if watchdog timer resets system, else returns false
sl_si91x_watchdog_deinit_timer#
void sl_si91x_watchdog_deinit_timer (void )
De-initialize Watchdog timer, mask its interrupt, de-power and disable timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Returns
none
sl_si91x_watchdog_unregister_timeout_callback#
void sl_si91x_watchdog_unregister_timeout_callback (void )
Unregister Watchdog timer timeout callback.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Pre-conditions:
Returns
none
sl_si91x_watchdog_get_version#
sl_watchdog_timer_version_t sl_si91x_watchdog_get_version ( none)
Get the release version of Watchdog timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [in] | none |
Returns
(sl_watchdog_version_t) type structure
sl_si91x_watchdog_start_timer#
__STATIC_INLINE void sl_si91x_watchdog_start_timer (void )
Start and enable the Watchdog timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Pre-conditions:
Returns
none
sl_si91x_watchdog_stop_timer#
__STATIC_INLINE void sl_si91x_watchdog_stop_timer (void )
Stop Watchdog timer by disabling it.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Pre-conditions:
Returns
none
sl_si91x_watchdog_restart_timer#
__STATIC_INLINE void sl_si91x_watchdog_restart_timer (void )
Restart (kick) an already running Watchdog timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Pre-conditions:
Returns
none
sl_si91x_watchdog_enable_system_reset_on_processor_lockup#
__STATIC_INLINE void sl_si91x_watchdog_enable_system_reset_on_processor_lockup (void )
Enable the Watchdog timer to reset the system on processor lockup.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Pre-conditions:
Returns
none
sl_si91x_watchdog_disable_system_reset_on_processor_lockup#
__STATIC_INLINE void sl_si91x_watchdog_disable_system_reset_on_processor_lockup (void )
Disable the Watchdog timer to reset system on processor lockup.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Pre-conditions:
Returns
none