Structure to hold the parameters of watchdog timer clock-source configurations.

Public Attributes#

uint8_t

low frequency FSM clock source, low_freq_fsm_clock_t

uint8_t

high frequency FSM clock source, high_freq_fsm_clock_t

uint8_t

Public Attribute Documentation#

low_freq_fsm_clock_src#

uint8_t watchdog_timer_clock_config_t::low_freq_fsm_clock_src

low frequency FSM clock source, low_freq_fsm_clock_t


Definition at line 110 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_watchdog_timer.h

high_freq_fsm_clock_src#

uint8_t watchdog_timer_clock_config_t::high_freq_fsm_clock_src

high frequency FSM clock source, high_freq_fsm_clock_t


Definition at line 111 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_watchdog_timer.h

bg_pmu_clock_source#

uint8_t watchdog_timer_clock_config_t::bg_pmu_clock_source

bg_pmu clock source, bg_pmu_clock_t


Definition at line 112 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_watchdog_timer.h