Roam configuration structure.

Public Attributes#

int32_t

RSSI level to trigger roam algorithm, Setting the value to SL_WIFI_NEVER_ROAM will disable roaming configuration.

uint32_t

RSSI level delta change to trigger roam algorithm.

Public Attribute Documentation#

trigger_level#

int32_t sl_wifi_roam_configuration_t::trigger_level

RSSI level to trigger roam algorithm, Setting the value to SL_WIFI_NEVER_ROAM will disable roaming configuration.


Definition at line 59 of file components/protocol/wifi/inc/sl_wifi_types.h

trigger_level_change#

uint32_t sl_wifi_roam_configuration_t::trigger_level_change

RSSI level delta change to trigger roam algorithm.


Definition at line 60 of file components/protocol/wifi/inc/sl_wifi_types.h