Wi-Fi scan configuration.

Note

  • channel_bitmap_2g4 uses the lower 14 bits to represent channels from 1 - 14 where channel 1 = (1 << 0), channel 2 = (1 << 1), etc

Public Attributes#

Scan type to be configured.

uint32_t

Flags for the scan configuration.

uint32_t

Duration in milliseconds between periodic scans.

uint16_t

Bitmap of selected 2.4GHz channels.

uint32_t

Bitmap of selected 5GHz channels.

Public Attribute Documentation#

type#

sl_wifi_scan_type_t sl_wifi_scan_configuration_t::type

Scan type to be configured.


Definition at line 94 of file components/protocol/wifi/inc/sl_wifi_types.h

flags#

uint32_t sl_wifi_scan_configuration_t::flags

Flags for the scan configuration.


Definition at line 95 of file components/protocol/wifi/inc/sl_wifi_types.h

periodic_scan_interval#

uint32_t sl_wifi_scan_configuration_t::periodic_scan_interval

Duration in milliseconds between periodic scans.


Definition at line 96 of file components/protocol/wifi/inc/sl_wifi_types.h

channel_bitmap_2g4#

uint16_t sl_wifi_scan_configuration_t::channel_bitmap_2g4

Bitmap of selected 2.4GHz channels.


Definition at line 97 of file components/protocol/wifi/inc/sl_wifi_types.h

channel_bitmap_5g#

uint32_t sl_wifi_scan_configuration_t::channel_bitmap_5g[8]

Bitmap of selected 5GHz channels.


Definition at line 98 of file components/protocol/wifi/inc/sl_wifi_types.h