Wi-Fi scan result.

Public Attributes#

uint32_t

Number of available scan results.

uint32_t

Reserved.

uint8_t

Channel number of the AP.

uint8_t

Security mode of the AP.

uint8_t

RSSI value of the AP.

uint8_t

AP network type.

uint8_t

SSID of the AP.

uint8_t

BSSID of the AP.

uint8_t

Reserved bytes for future use.

struct sl_wifi_scan_result_t::@0

Array of scan result data.

Public Attribute Documentation#

scan_count#

uint32_t sl_wifi_scan_result_t::scan_count

Number of available scan results.


Definition at line 77 of file components/protocol/wifi/inc/sl_wifi_types.h

reserved#

uint32_t sl_wifi_scan_result_t::reserved

Reserved.


Definition at line 78 of file components/protocol/wifi/inc/sl_wifi_types.h

rf_channel#

uint8_t sl_wifi_scan_result_t::rf_channel

Channel number of the AP.


Definition at line 80 of file components/protocol/wifi/inc/sl_wifi_types.h

security_mode#

uint8_t sl_wifi_scan_result_t::security_mode

Security mode of the AP.


Definition at line 81 of file components/protocol/wifi/inc/sl_wifi_types.h

rssi_val#

uint8_t sl_wifi_scan_result_t::rssi_val

RSSI value of the AP.


Definition at line 82 of file components/protocol/wifi/inc/sl_wifi_types.h

network_type#

uint8_t sl_wifi_scan_result_t::network_type

AP network type.


Definition at line 83 of file components/protocol/wifi/inc/sl_wifi_types.h

ssid#

uint8_t sl_wifi_scan_result_t::ssid[34]

SSID of the AP.


Definition at line 84 of file components/protocol/wifi/inc/sl_wifi_types.h

bssid#

uint8_t sl_wifi_scan_result_t::bssid[6]

BSSID of the AP.


Definition at line 85 of file components/protocol/wifi/inc/sl_wifi_types.h

reserved#

uint8_t sl_wifi_scan_result_t::reserved[2]

Reserved bytes for future use.


Definition at line 86 of file components/protocol/wifi/inc/sl_wifi_types.h

scan_info#

struct sl_wifi_scan_result_t::@0 sl_wifi_scan_result_t::scan_info[]

Array of scan result data.


Definition at line 87 of file components/protocol/wifi/inc/sl_wifi_types.h