PSRAM Driver#

PSRAM Memory Management driver.

Introduction#

PSRAM (Pseudo Static Random Access Memory) is a random-access memory whose internal structure is based on dynamic memory with refresh control signals generated internally, in the standby mode, so that it can mimic the functionality of a static memory. It combines the high density of DRAM with the ease-of-use of true SRAM. The M4 core communicates with the PSRAM via Quad SPI interface.

PSRAM Device Configuration#

The PSRAM Driver offers configuring the following:

  • Read-Write type

    • Normal: This supported only in SPI interface mode. Supports maximum frequency of 33MHz. Uses normal read and normal write command.

    • Fast: Supported in SPI and QPI mode. Uses fast read and normal write.

    • Quad IO: Supported in SPI and QPI mode. Uses fast quad read and write.

  • Interface mode

    • SPI Mode (Serial IO)

    • QPI Mode (Quad IO)

  • Operation frequency Source

    • Interface PLL Clock

    • ULP Reference Clock

    • SoC PLL Clock

    • M4_SOCCLKNOSWLSYNCCLKTREEGATED Clock

Linker configurations#

The text segment, data segment, bss, heap and stack can be placed in PSRAM by installing the respective components present under "PSRAM Linker Configurations" from "SOFTWARE COMPONENTS" GUI. Since PSRAM is already initiliazed in bootloader, these components can be installed and the respective segments can be placed in PSRAM without installing "PSRAM Core" component and without initializing psram from application.

Usage#

PSRAM Driver and QSPI are initiliazed by bootloader with Quad IO read-write type and QPI interface. The application is not required to reinitialize PSRAM device and QSPI unless the configurations required are different from the default set by the bootloader.

The PSRAM device handle "PSRAM_Device" of type sl_psram_info_type_t is defined "in sl_si91x_psram_handle.c".

sl_si91x_psram_uninit assumes that PSRAM was initialized with QPI mode and exits QPI mode within definition. If the PSRAM configuration in bootcode has SPI mode enabled, user is expected to comment the exit QPI mode function call in sl_si91x_psram_uninit.

To reconfigure and initliaze PSRAM, set required configurations from PSRAM Core component and call sl_si91x_psram_init within application.

Modules#

sl_psram_id_type_t

sl_psram_info_type_t

Enumerations#

enum
PSRAM_SUCCESS
PSRAM_FAILURE
PSRAM_UNKNOWN
PSRAM_UNKNOWN_DEVICE
PSRAM_CLOCK_INIT_FAILURE
PSRAM_NOT_INITIALIZED
PSRAM_SUPPORTED_DEVICE
PSRAM_DEVICE_MISMATCH
PSRAM_INVALID_HSIZE
PSRAM_NULL_ADDRESS
PSRAM_INVALID_ADDRESS_LENGTH
PSRAM_AUTO_MODE
PSRAM_MANUAL_MODE
PSRAM_UNSUPPORTED_SECURITY
PSRAM_MAX_SEC_SEGMENT_REACH
}

PSRAM return error code.

enum
DMA_NONE
DMA_DONE
DMA_FAIL
}

PSRAM DMA status enum.

Functions#

Initialize the PSRAM Device

Uninitialize the PSRAM Device

Reset the PSRAM Device

sl_si91x_psram_manual_write_in_blocking_mode(uint32_t addr, void *SourceBuf, uint8_t hSize, uint32_t length)

Write data to PSRAM in manual mode

sl_si91x_psram_manual_read_in_blocking_mode(uint32_t addr, void *DestBuf, uint8_t hSize, uint32_t length)

Read data from PSRAM in manual mode

sl_si91x_psram_manual_write_in_dma_mode(uint32_t addr, void *SourceBuf, uint8_t hSize, uint32_t length, sl_psram_dma_status_type_t *dmastatus)

Write data to PSRAM in manual mode using DMA

sl_si91x_psram_manual_read_in_dma_mode(uint32_t addr, void *DestBuf, uint8_t hSize, uint32_t length, sl_psram_dma_status_type_t *dmaStatus)

Read data from PSRAM in manual mode using DMA

Enable CTR encryption-decryption on PSRAM

Macros#

#define

Read ID command.

#define

Enter QPI interface mode command.

#define

Exit QPI interface mode command.

#define

Reset Enable command.

#define

Reset command.

#define

Burst Length Toggle command.

#define

Mode Register Read command.

#define

Mode Register Write command.

#define

Sleep Entry command.

#define

Sleep Exit chip select low pulse width in us.

#define
tXHS_US (160)

Sleep Exit chip select low to CLK setup in us.

#define
tHS_US (8)

Minimum sleep duration in us.

Enumeration Documentation#

sl_psram_return_type_t#

sl_psram_return_type_t

PSRAM return error code.

Enumerator
PSRAM_SUCCESS

No error.

PSRAM_FAILURE

Generic error.

PSRAM_UNKNOWN

Unknown request.

PSRAM_UNKNOWN_DEVICE

Unknown PSRAM Device.

PSRAM_CLOCK_INIT_FAILURE

Clock init failure.

PSRAM_NOT_INITIALIZED

PSRAM not initialized.

PSRAM_SUPPORTED_DEVICE

PSRAM Device supported.

PSRAM_DEVICE_MISMATCH

PSRAM Device mismatch.

PSRAM_INVALID_HSIZE

Invalid size of element.

PSRAM_NULL_ADDRESS

Null address.

PSRAM_INVALID_ADDRESS_LENGTH

Invalid address length.

PSRAM_AUTO_MODE

PSRAM Auto mode.

PSRAM_MANUAL_MODE

PSRAM Manual mode.

PSRAM_UNSUPPORTED_SECURITY

Unsupported security.

PSRAM_MAX_SEC_SEGMENT_REACH

Maximum secure segment reached.


sl_psram_dma_status_type_t#

sl_psram_dma_status_type_t

PSRAM DMA status enum.

Enumerator
DMA_NONE

DMA status default.

DMA_DONE

DMA transfer completed.

DMA_FAIL

DMA transfer failed.


Function Documentation#

sl_si91x_psram_init#

sl_psram_return_type_t sl_si91x_psram_init (void )

Initialize the PSRAM Device

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Status Code of the operation

Note

  • The configurations for initialization are taken from the PSRAM Device config header file. The selection of configuration file happens implicitely based on the radio board selection.


sl_si91x_psram_uninit#

sl_psram_return_type_t sl_si91x_psram_uninit (void )

Uninitialize the PSRAM Device

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Status Code of the operation


sl_si91x_psram_reset#

sl_psram_return_type_t sl_si91x_psram_reset (void )

Reset the PSRAM Device

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Status Code of the operation


sl_si91x_psram_manual_write_in_blocking_mode#

sl_psram_return_type_t sl_si91x_psram_manual_write_in_blocking_mode (uint32_t addr, void * SourceBuf, uint8_t hSize, uint32_t length)

Write data to PSRAM in manual mode

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]addr

PSRAM address for write operation

void *[in]SourceBuf

Reference of the Source buffer

uint8_t[in]hSize

Size of each element

uint32_t[in]length

Number of elements for write operation

Returns

  • Status Code of the operation


sl_si91x_psram_manual_read_in_blocking_mode#

sl_psram_return_type_t sl_si91x_psram_manual_read_in_blocking_mode (uint32_t addr, void * DestBuf, uint8_t hSize, uint32_t length)

Read data from PSRAM in manual mode

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]addr

PSRAM address for read operation

void *[in]DestBuf

Size of each element

uint8_t[in]hSize

Number of elements for read operation

uint32_t[out]length

Reference of the Destination buffer

Returns

  • Status Code of the operation


sl_si91x_psram_manual_write_in_dma_mode#

sl_psram_return_type_t sl_si91x_psram_manual_write_in_dma_mode (uint32_t addr, void * SourceBuf, uint8_t hSize, uint32_t length, sl_psram_dma_status_type_t * dmastatus)

Write data to PSRAM in manual mode using DMA

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]addr

PSRAM address for write operation

void *[in]SourceBuf

Reference of the Source buffer

uint8_t[in]hSize

Size of each element

uint32_t[in]length

Number of elements for write operation

sl_psram_dma_status_type_t *[out]dmastatus

DMA operation completion status

Returns

  • Status Code of the operation


sl_si91x_psram_manual_read_in_dma_mode#

sl_psram_return_type_t sl_si91x_psram_manual_read_in_dma_mode (uint32_t addr, void * DestBuf, uint8_t hSize, uint32_t length, sl_psram_dma_status_type_t * dmaStatus)

Read data from PSRAM in manual mode using DMA

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]addr

PSRAM address for read operation

void *[in]DestBuf

Size of each element

uint8_t[in]hSize

Number of elements for read operation

uint32_t[out]length

Reference of the Destination buffer

sl_psram_dma_status_type_t *[out]dmaStatus

DMA operation completion status

Returns

  • Status Code of the operation


sl_si91x_psram_enable_encry_decry#

sl_psram_return_type_t sl_si91x_psram_enable_encry_decry (uint16_t keySize)

Enable CTR encryption-decryption on PSRAM

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]keySize

Pass 128/256-Bit size

Returns

  • Status Code of the operation


Macro Definition Documentation#

PSRAM_READ_ID#

#define PSRAM_READ_ID
Value:
(0x9F)

Read ID command.


PSRAM_ENTER_QPI#

#define PSRAM_ENTER_QPI
Value:
(0x35)

Enter QPI interface mode command.


PSRAM_EXIT_QPI#

#define PSRAM_EXIT_QPI
Value:
(0xF5)

Exit QPI interface mode command.


PSRAM_RESET_EN#

#define PSRAM_RESET_EN
Value:
(0x66)

Reset Enable command.


PSRAM_RESET#

#define PSRAM_RESET
Value:
(0x99)

Reset command.


PSRAM_BURST_LEN#

#define PSRAM_BURST_LEN
Value:
(0xC0)

Burst Length Toggle command.


PSRAM_MODE_REG_READ#

#define PSRAM_MODE_REG_READ
Value:
(0xB5)

Mode Register Read command.


PSRAM_MODE_REG_WRITE#

#define PSRAM_MODE_REG_WRITE
Value:
(0xB1)

Mode Register Write command.


PSRAM_HALF_SLEEP#

#define PSRAM_HALF_SLEEP
Value:
(0xC0)

Sleep Entry command.


tXPHS_US#

#define tXPHS_US
Value:
(12)

Sleep Exit chip select low pulse width in us.


tXHS_US#

#define tXHS_US
Value:
(160)

Sleep Exit chip select low to CLK setup in us.


tHS_US#

#define tHS_US
Value:
(8)

Minimum sleep duration in us.