Config Timer#

Modules#

sl_config_timer_config_t

sl_config_timer_ocu_config_t

sl_config_timer_ocu_control_t

sl_config_action_event_t

sl_config_timer_interrupt_flags_t

sl_config_timer_version_t

Enumerations#

enum
SL_COUNTER_16BIT
SL_COUNTER_32BIT
SL_COUNTER_MODE_LAST
}

Enumeration to represent timer modes.

enum
SL_COUNTER_0
SL_COUNTER_1
SL_COUNTER_NUMBER_LAST
}

Enumeration to represent timer counter numbers.

enum
SL_COUNTER0_UP
SL_COUNTER0_DOWN
SL_COUNTER0_UP_DOWN
SL_COUNTER0_DIRECTION_LAST
}

Enumeration to represent timer counter directions.

enum
SL_COUNTER1_UP
SL_COUNTER1_DOWN
SL_COUNTER1_UP_DOWN
SL_COUNTER1_DIRECTION_LAST
}
enum
SL_COUNTER_MODE_32 = COUNTER32_BITMODE
SL_COUNTER0_SOFT_RESET_ENABLE = SOFTRESET_COUNTER_0
SL_COUNTER0_PERIODIC_ENABLE = PERIODIC_ENCOUNTER_0
SL_COUNTER0_TRIGGER_ENABLE = COUNTER0_TRIG
SL_COUNTER0_SYNC_TRIGGER_ENABLE = COUNTER0_SYNC_TRIG
SL_COUNTER0_BUFFER_ENABLE = BUF_REG0EN
SL_COUNTER0_UP_DIRECTION = COUNTER0_UP
SL_COUNTER0_DOWN_DIRECTION = COUNTER0_DOWN
SL_COUNTER0_UP_DOWN_DIRECTION = COUNTER0_UP_DOWN
SL_COUNTER1_SOFT_RESET_ENABLE = SOFTRESET_COUNTER_1
SL_COUNTER1_PERIODIC_ENABLE = PERIODIC_ENCOUNTER_1
SL_COUNTER1_TRIGGER_ENABLE = COUNTER1_TRIG
SL_COUNTER1_SYNC_TRIGGER_ENABLE = COUNTER1_SYNC_TRIG
SL_COUNTER1_BUFFER_ENABLE = BUF_REG1EN
SL_COUNTER1_UP_DIRECTION = COUNTER1_UP
SL_COUNTER1_DOWN_DIRECTION = COUNTER1_DOWN
SL_COUNTER1_UP_DOWN_DIRECTION = COUNTER1_UP_DOWN
SL_COUNTER_PARAM_LAST
}

Enumeration to represent timer-config parameters values.

enum
SL_COUNTER0_OCU_OUTPUT_ENABLE = OUTPUT_OCU_0
SL_COUNTER0_OCU_DMA_ENABLE = OCU_DMA_0
SL_COUNTER0_OCU_8BIT_ENABLE = OCU_8_MODE_0
SL_COUNTER0_OCU_SYNC_ENABLE = OCU_SYNC_WITH_0
SL_COUNTER1_OCU_OUTPUT_ENABLE = OUTPUT_OCU_1
SL_COUNTER1_OCU_DMA_ENABLE = OCU_DMA_1
SL_COUNTER1_OCU_8BIT_ENABLE = OCU_8_MODE_1
SL_COUNTER1_OCU_SYNC_ENABLE = OCU_SYNC_WITH_1
SL_OCU_OUTPUT0_TOGGLE_HIGH = MAKE_OUTPUT_0_HIGH_SEL_0
SL_OCU_OUTPUT0_TOGGLE_LOW = MAKE_OUTPUT_0_LOW_SEL_0
SL_OCU_OUTPUT1_TOGGLE_HIGH = MAKE_OUTPUT_1_HIGH_SEL_1
SL_OCU_OUTPUT1_TOGGLE_LOW = MAKE_OUTPUT_1_LOW_SEL_1
SL_OCU_PARAM_LAST
}

Enumeration to represent timer OCU-config parameters values.

enum
SL_NO_EVENT
SL_EVENT0_RISING_EDGE
SL_EVENT1_RISING_EDGE
SL_EVENT2_RISING_EDGE
SL_EVENT3_RISING_EDGE
SL_EVENT0_FALLING_EDGE
SL_EVENT1_FALLING_EDGE
SL_EVENT2_FALLING_EDGE
SL_EVENT3_FALLING_EDGE
SL_EVENT0_RISING_FALLING_EDGE
SL_EVENT1_RISING_FALLING_EDGE
SL_EVENT2_RISING_FALLING_EDGE
SL_EVENT3_RISING_FALLING_EDGE
SL_EVENT0_LEVEL0
SL_EVENT1_LEVEL0
SL_EVENT2_LEVEL0
SL_EVENT3_LEVEL0
SL_EVENT0_LEVEL1
SL_EVENT1_LEVEL1
SL_EVENT2_LEVEL1
SL_EVENT3_LEVEL1
SL_AND_EVENT
SL_OR_EVENT
SL_EVENT0_RISING_EDGE_AND_EVENT
SL_EVENT0_RISING_EDGE_OR_EVENT
SL_EVENT1_RISING_EDGE_AND_EVENT
SL_EVENT1_RISING_EDGE_OR_EVENT
SL_EVENT2_RISING_EDGE_AND_EVENT
SL_EVENT2_RISING_EDGE_OR_EVENT
SL_EVENT3_RISING_EDGE_AND_EVENT
SL_EVENT3_RISING_EDGE_OR_EVENT
SL_EVENT0_RISING_EDGE_REGISTERED_AND_EVENT
SL_EVENT0_RISING_EDGE_REGISTERED_OR_EVENT
SL_EVENT1_RISING_EDGE_REGISTERED_AND_EVENT
SL_EVENT1_RISING_EDGE_REGISTERED_OR_EVENT
SL_EVENT2_RISING_EDGE_REGISTERED_AND_EVENT
SL_EVENT2_RISING_EDGE_REGISTERED_OR_EVENT
SL_EVENT3_RISING_EDGE_REGISTERED_AND_EVENT
SL_EVENT3_RISING_EDGE_REGISTERED_OR_EVENT
SL_EVENT_LAST
}

Enumeration to represent various timer input events.

enum
START
STOP
CONTINUE
HALT
INCREMENT
CAPTURE
INTERRUPT
OUTPUT
ACTION_LAST
}

Enumeration to represent various timer actions.

enum
SL_CT_EVENT_INTR_0_FLAG = RSI_CT_EVENT_INTR_0_l
SL_CT_FIFO_0_FULL_FLAG = RSI_CT_EVENT_FIFO_0_FULL_l
SL_CT_COUNTER_0_IS_ZERO_FLAG = RSI_CT_EVENT_COUNTER_0_IS_ZERO_l
SL_CT_COUNTER_0_IS_PEAK_FLAG = RSI_CT_EVENT_COUNTER_0_IS_PEAK_l
SL_CT_EVENT_INTR_1_FLAG = RSI_CT_EVENT_INTR_1_l
SL_CT_FIFO_1_FULL_FLAG = RSI_CT_EVENT_FIFO_1_FULL_l
SL_CT_COUNTER_1_IS_ZERO_FLAG = RSI_CT_EVENT_COUNTER_1_IS_ZERO_l
SL_CT_COUNTER_1_IS_PEAK_FLAG = RSI_CT_EVENT_COUNTER_1_IS_PEAK_l
}

Enumeration to represent various timer interrupt flag values.

Typedefs#

typedef OCU_PARAMS_T

Renaming OCU parameters structure type.

typedef WFG_PARAMS_T

Renaming WFG parameters structure type.

typedef RSI_CT_CALLBACK_T

Renaming MCPWM callback structure.

typedef void(*
sl_config_timer_callback_t)(void *callback_flag)

Typedef for the function pointer of the interrupt callback function.

Functions#

void

Initializes config-timer peripheral.

sl_status_t
sl_si91x_config_timer_set_mode(sl_config_timer_mode_t mode)

Set Config-timer mode as 32-bit or 16-bit counters.

sl_status_t
sl_si91x_config_timer_set_configuration(sl_config_timer_config_t *timer_config_ptr)

Configures Config-timer parameters.

void

Reset config-timer parameters and sets default parameter values.

sl_status_t
sl_si91x_config_timer_set_ocu_configuration(sl_config_timer_ocu_config_t *ocu_config_ptr)

Set Config-timer OCU configurations.

void

Reset config-timer OCU parameters Sets 16-bit mode, sets up-counter direction Disables DMA mode, channel sync and 8-bit mode for OCU outputs.

sl_status_t
sl_si91x_config_timer_set_ocu_control(sl_config_timer_ocu_control_t *ocu_params)

Set Config-timer OCU mode control params Sets first and next threshold values for counter outputs.

sl_status_t
sl_si91x_config_timer_set_wfg_configuration(sl_config_timer_wfg_config_t *wfg_config_ptr)

Set Config-timer WFG mode configurations Such as select toggle high, low and peak for counter-0 & counter-1 outputs.

sl_status_t
sl_si91x_config_timer_set_initial_count(sl_config_timer_mode_t mode, uint32_t counter0_initial_value, uint32_t counter1_initial_value)

Set Config-timer initial count as per timer mode.

sl_status_t
sl_si91x_config_timer_set_match_count(sl_config_timer_mode_t mode, sl_counter_number_t counter_number, uint32_t match_value)

Set Config-timer match-count as per timer mode and counter-number.

sl_status_t
sl_si91x_config_timer_get_count(sl_config_timer_mode_t mode, sl_counter_number_t counter_number, uint32_t *count_value)

Get Config-timer current count as per timer mode and counter-number.

sl_status_t
sl_si91x_config_timer_reset_counter(sl_counter_number_t counter_number)

Resets Config-timer counter register value.

sl_status_t
sl_si91x_config_timer_start_on_software_trigger(sl_counter_number_t counter_number)

Starts selected config-timer counter.

sl_status_t
sl_si91x_config_timer_select_action_event(sl_config_timer_action_t action, sl_config_timer_event_t select_event_counter0, sl_config_timer_event_t select_event_counter1)

Selects config timer input events for triggering selected timer-actions.

sl_status_t
sl_si91x_config_timer_configure_action_event(sl_config_action_event_t *event_config_handle)

Configure config timer input-event's AND-event and OR-event for triggering selected timer-action.

sl_status_t
sl_si91x_config_timer_register_callback(sl_config_timer_callback_t on_config_timer_callback, void *callback_flag_value, sl_config_timer_interrupt_flags_t *interrupt_flags)

Register callback of config timer interrupts.

sl_status_t
sl_si91x_config_timer_unregister_callback(sl_config_timer_interrupt_flags_t *interrupt_flags)

Unregisters timer interrupt callback Disables interrupts as per selected interrupt flag.

sl_status_t
sl_si91x_config_timer_resume_halt_event(sl_counter_number_t counter_number)

Resume halt operation of Config-timer counter.

sl_status_t
sl_si91x_config_timer_read_capture(sl_counter_number_t counter_number, uint16_t *capture_value)

Gets Config-timer count value when capture occurs Updates the capture count value of timer to capture_value variable input parameter.

sl_status_t
sl_si91x_config_timer_set_counter_sync(sl_counter_number_t counter_number, uint8_t sync_counter_value)

Sync counter output with other channels, as per sync_counter_value.

sl_status_t
sl_si91x_config_timer_set_output_adc_pin(uint8_t pin1, uint8_t pin2)

This API is used to configure config timer output events for ADC trigger Configures input events for counter0 and counter1 outputs to trigger ADC.

sl_status_t
sl_si91x_config_timer_set_wfg_compare_values(sl_counter_number_t counter_number, sl_config_timer_ocu_params_t *ocu_params)
void

De-initialize config-timer by disabling its clock.

Gets Config timer version It returns API version of Config timer.

Macros#

#define
CT CT0

pointer to CT base address

Enumeration Documentation#

sl_config_timer_mode_t#

sl_config_timer_mode_t

Enumeration to represent timer modes.

Enumerator
SL_COUNTER_16BIT

enum for CT 16-bit mode

SL_COUNTER_32BIT

enum for CT 32-bit mode

SL_COUNTER_MODE_LAST

Last member of enum for validation.


sl_counter_number_t#

sl_counter_number_t

Enumeration to represent timer counter numbers.

Enumerator
SL_COUNTER_0

enum for CT counter-0

SL_COUNTER_1

enum for CT counter-1

SL_COUNTER_NUMBER_LAST

Last member of enum for validation.


sl_counter0_direction_t#

sl_counter0_direction_t

Enumeration to represent timer counter directions.

Enumerator
SL_COUNTER0_UP

CT counter-0 up-counting operation.

SL_COUNTER0_DOWN

CT counter-0 down-counting operation.

SL_COUNTER0_UP_DOWN

CT counter-0 up-down counting operation.

SL_COUNTER0_DIRECTION_LAST

Last member of enum for validation.


sl_counter1_direction_t#

sl_counter1_direction_t
Enumerator
SL_COUNTER1_UP

CT counter-1 up-counting operation.

SL_COUNTER1_DOWN

CT counter-1 down-counting operation.

SL_COUNTER1_UP_DOWN

CT counter-1 up-down counting operation.

SL_COUNTER1_DIRECTION_LAST

Last member of enum for validation.


sl_config_timer_config_values_t#

sl_config_timer_config_values_t

Enumeration to represent timer-config parameters values.

Enumerator
SL_COUNTER_MODE_32

enum for CT 32-bit mode value

SL_COUNTER0_SOFT_RESET_ENABLE

enum for counter-0 soft reset enable value

SL_COUNTER0_PERIODIC_ENABLE

enum for counter-0 periodic mode enable value

SL_COUNTER0_TRIGGER_ENABLE

enum for counter-0 software trigger enable value

SL_COUNTER0_SYNC_TRIGGER_ENABLE

enum for counter-0 sync trigger enable value

SL_COUNTER0_BUFFER_ENABLE

enum for counter-0 buffer enable value

SL_COUNTER0_UP_DIRECTION

enum for counter-0 up-direction enable value

SL_COUNTER0_DOWN_DIRECTION

enum for counter-0 down-direction enable value

SL_COUNTER0_UP_DOWN_DIRECTION

enum for counter-0 up-down direction enable value

SL_COUNTER1_SOFT_RESET_ENABLE

enum for counter-1 soft reset enable value

SL_COUNTER1_PERIODIC_ENABLE

enum for counter-1 periodic mode enable value

SL_COUNTER1_TRIGGER_ENABLE

enum for counter-1 software trigger enable value

SL_COUNTER1_SYNC_TRIGGER_ENABLE

enum for counter-1 sync trigger enable value

SL_COUNTER1_BUFFER_ENABLE

enum for counter-1 buffer enable value

SL_COUNTER1_UP_DIRECTION

enum for counter-1 up-direction enable value

SL_COUNTER1_DOWN_DIRECTION

enum for counter-1 up-direction enable value

SL_COUNTER1_UP_DOWN_DIRECTION

enum for counter-1 up-direction enable value

SL_COUNTER_PARAM_LAST

Last member of enum for validation.


sl_config_timer_ocu_config_values_t#

sl_config_timer_ocu_config_values_t

Enumeration to represent timer OCU-config parameters values.

Enumerator
SL_COUNTER0_OCU_OUTPUT_ENABLE

enum for counter-0 output enable value

SL_COUNTER0_OCU_DMA_ENABLE

enum for counter-0 OCU-DMA mode enable value

SL_COUNTER0_OCU_8BIT_ENABLE

enum for counter-0 OCU-8bit mode enable value

SL_COUNTER0_OCU_SYNC_ENABLE

enum for counter-0 OCU-sync mode enable value

SL_COUNTER1_OCU_OUTPUT_ENABLE

enum for counter-1 output enable value

SL_COUNTER1_OCU_DMA_ENABLE

enum for counter-1 OCU-DMA mode enable value

SL_COUNTER1_OCU_8BIT_ENABLE

enum for counter-1 OCU-8bit mode enable value

SL_COUNTER1_OCU_SYNC_ENABLE

enum for counter-1 OCU-sync mode enable value

SL_OCU_OUTPUT0_TOGGLE_HIGH

enum for counter-0 output toggle high

SL_OCU_OUTPUT0_TOGGLE_LOW

enum for counter-0 output toggle low

SL_OCU_OUTPUT1_TOGGLE_HIGH

enum for counter-1 output toggle high select value

SL_OCU_OUTPUT1_TOGGLE_LOW

enum for counter-1 output toggle low select value

SL_OCU_PARAM_LAST

Last member of enum for validation.


sl_config_timer_event_t#

sl_config_timer_event_t

Enumeration to represent various timer input events.

Enumerator
SL_NO_EVENT

enum for no input event

SL_EVENT0_RISING_EDGE

enum for input-0 rising edge event

SL_EVENT1_RISING_EDGE

enum for input-1 rising edge event

SL_EVENT2_RISING_EDGE

enum for input-2 rising edge event

SL_EVENT3_RISING_EDGE

enum for input-3 rising edge event

SL_EVENT0_FALLING_EDGE

enum for input-0 falling edge event

SL_EVENT1_FALLING_EDGE

enum for input-1 falling edge event

SL_EVENT2_FALLING_EDGE

enum for input-2 falling edge event

SL_EVENT3_FALLING_EDGE

enum for input-3 falling edge event

SL_EVENT0_RISING_FALLING_EDGE

enum for input-0 rising-falling edge event

SL_EVENT1_RISING_FALLING_EDGE

enum for input-1 rising-falling edge event

SL_EVENT2_RISING_FALLING_EDGE

enum for input-2 rising-falling edge event

SL_EVENT3_RISING_FALLING_EDGE

enum for input-3 rising-falling edge event

SL_EVENT0_LEVEL0

enum for input-0 Level-0 event

SL_EVENT1_LEVEL0

enum for input-0 Level-0 event

SL_EVENT2_LEVEL0

enum for input-0 Level-0 event

SL_EVENT3_LEVEL0

enum for input-0 Level-0 event

SL_EVENT0_LEVEL1

enum for input-0 Level-0 event

SL_EVENT1_LEVEL1

enum for input-0 Level-0 event

SL_EVENT2_LEVEL1

enum for input-0 Level-0 event

SL_EVENT3_LEVEL1

enum for input-0 Level-0 event

SL_AND_EVENT

enum for and-event

SL_OR_EVENT

enum for or-event

SL_EVENT0_RISING_EDGE_AND_EVENT

enum for input-0 rising edge and-event

SL_EVENT0_RISING_EDGE_OR_EVENT

enum for input-0 rising edge or-event

SL_EVENT1_RISING_EDGE_AND_EVENT

enum for input-1 rising edge and-event

SL_EVENT1_RISING_EDGE_OR_EVENT

enum for input-1 rising edge or-event

SL_EVENT2_RISING_EDGE_AND_EVENT

enum for input-2 rising edge and-event

SL_EVENT2_RISING_EDGE_OR_EVENT

enum for input-2 rising edge or-event

SL_EVENT3_RISING_EDGE_AND_EVENT

enum for input-3 rising edge and-event

SL_EVENT3_RISING_EDGE_OR_EVENT

enum for input-3 rising edge or-event

SL_EVENT0_RISING_EDGE_REGISTERED_AND_EVENT

enum for input-0 rising edge registered and-event

SL_EVENT0_RISING_EDGE_REGISTERED_OR_EVENT

enum for input-0 rising edge registered or-event

SL_EVENT1_RISING_EDGE_REGISTERED_AND_EVENT

enum for input-1 rising edge registered and-event

SL_EVENT1_RISING_EDGE_REGISTERED_OR_EVENT

enum for input-1 rising edge registered or-event

SL_EVENT2_RISING_EDGE_REGISTERED_AND_EVENT

enum for input-2 rising edge registered and-event

SL_EVENT2_RISING_EDGE_REGISTERED_OR_EVENT

enum for input-2 rising edge registered or-event

SL_EVENT3_RISING_EDGE_REGISTERED_AND_EVENT

enum for input-3 rising edge registered and-event

SL_EVENT3_RISING_EDGE_REGISTERED_OR_EVENT

enum for input-3 rising edge registered or-event

SL_EVENT_LAST

Last member of enum for validation.


sl_config_timer_action_t#

sl_config_timer_action_t

Enumeration to represent various timer actions.

Enumerator
START

enum for timer-start action

STOP

enum for timer-stop action

CONTINUE

enum for timer-continue action

HALT

enum for timer-halt action

INCREMENT

enum for timer-increment action

CAPTURE

enum for timer-capture action

INTERRUPT

enum for timer-interrupt action

OUTPUT

enum for timer-output action

ACTION_LAST

Last member of enum for validation.


sl_config_timer_interrupt_flags_values_t#

sl_config_timer_interrupt_flags_values_t

Enumeration to represent various timer interrupt flag values.

Enumerator
SL_CT_EVENT_INTR_0_FLAG

enum for counter-0 event interrupt enable value

SL_CT_FIFO_0_FULL_FLAG

enum for counter-0 FIFO full interrupt enable value

SL_CT_COUNTER_0_IS_ZERO_FLAG

enum for counter-0 zero-count-value interrupt enable value

SL_CT_COUNTER_0_IS_PEAK_FLAG

enum for counter-0 match-value interrupt enable value

SL_CT_EVENT_INTR_1_FLAG

enum for counter-1 event interrupt enable value

SL_CT_FIFO_1_FULL_FLAG

enum for counter-1 FIFO full interrupt enable value

SL_CT_COUNTER_1_IS_ZERO_FLAG

enum for counter-1 zero-count-value interrupt enable value

SL_CT_COUNTER_1_IS_PEAK_FLAG

enum for counter-1 match-value interrupt enable value


Typedef Documentation#

sl_config_timer_ocu_params_t#

typedef OCU_PARAMS_T sl_config_timer_ocu_params_t

Renaming OCU parameters structure type.


sl_config_timer_wfg_config_t#

typedef WFG_PARAMS_T sl_config_timer_wfg_config_t

Renaming WFG parameters structure type.


sl_config_timer_pwm_callback_t#

typedef RSI_CT_CALLBACK_T sl_config_timer_pwm_callback_t

Renaming MCPWM callback structure.


sl_config_timer_callback_t#

typedef void(* sl_config_timer_callback_t) (void *callback_flag) )(void *callback_flag)

Typedef for the function pointer of the interrupt callback function.

Parameters
TypeDirectionArgument NameDescription
N/Acallback_flag

(void *) parameter for updating flag values


Function Documentation#

sl_si91x_config_timer_init#

void sl_si91x_config_timer_init (void )

Initializes config-timer peripheral.

Parameters
TypeDirectionArgument NameDescription
void[in]

Configures its output GPIO pins. Configures clock as 16 MHz.

Returns

  • none


sl_si91x_config_timer_set_mode#

sl_status_t sl_si91x_config_timer_set_mode (sl_config_timer_mode_t mode)

Set Config-timer mode as 32-bit or 16-bit counters.

Parameters
TypeDirectionArgument NameDescription
sl_config_timer_mode_t[in]mode

sl_config_timer_mode_t for possible values

In 32-bit mode Counter_1 and Counter_0 will be merged and used as a single 32 bit counter. In this mode, Counter_0 modes/triggers/enables will be used.

Returns

  • status 0 if successful, else error-code as follow SL_STATUS_INVALID_MODE (0x0024) - 'mode' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Success, timer-mode is set properly


sl_si91x_config_timer_set_configuration#

sl_status_t sl_si91x_config_timer_set_configuration (sl_config_timer_config_t * timer_config_ptr)

Configures Config-timer parameters.

Parameters
TypeDirectionArgument NameDescription
sl_config_timer_config_t *[in]timer_config_ptr

Pointer to CT config structure sl_config_timer_config_t

Such as 32-bit or 16-bit mode, periodic mode, Counter trigger enable, soft reset enable, buffer enable, sync trigger enable and sets direction for counter0 and counter1. Counter trigger enable is enabled to start the counter. Sync trigger enables the counter to run/active when sync is found. Buffer enable will copy buffer data to Counter Match register. Soft reset valid only when the counter is in two 16 bit counters mode, this resets the counter on the write.

Returns

  • status 0 if successful, else error-code as follow SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer.

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Counter direction parameter has invalid value.

    • SL_STATUS_OK (0x0000) - Success, timer configurations are set properly


sl_si91x_config_timer_reset_configuration#

void sl_si91x_config_timer_reset_configuration (void )

Reset config-timer parameters and sets default parameter values.

Parameters
TypeDirectionArgument NameDescription
void[in]

Sets 16-bit mode, sets up-counter direction Disables periodic mode, soft reset, buffer, sync & software trigger of counters.

Returns

  • none


sl_si91x_config_timer_set_ocu_configuration#

sl_status_t sl_si91x_config_timer_set_ocu_configuration (sl_config_timer_ocu_config_t * ocu_config_ptr)

Set Config-timer OCU configurations.

Parameters
TypeDirectionArgument NameDescription
sl_config_timer_ocu_config_t *[in]ocu_config_ptr

Pointer to CT OCU-config structure sl_config_timer_ocu_config_t

It enables outputs in OCU mode, OCU-DMA mode, channel sync with OCU outputs, 8-bit mode for OCU outputs for both counters.

Returns

  • status 0 if successful, else error-code as follow SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer.

    • SL_STATUS_OK (0x0000) - Success, OCU configurations are set properly.


sl_si91x_config_timer_reset_ocu_configuration#

void sl_si91x_config_timer_reset_ocu_configuration (void )

Reset config-timer OCU parameters Sets 16-bit mode, sets up-counter direction Disables DMA mode, channel sync and 8-bit mode for OCU outputs.

Parameters
TypeDirectionArgument NameDescription
void[in]

Returns

  • none


sl_si91x_config_timer_set_ocu_control#

sl_status_t sl_si91x_config_timer_set_ocu_control (sl_config_timer_ocu_control_t * ocu_params)

Set Config-timer OCU mode control params Sets first and next threshold values for counter outputs.

Parameters
TypeDirectionArgument NameDescription
sl_config_timer_ocu_control_t *[in]ocu_params

Pointer to CT OCU-config structure sl_config_timer_ocu_control_t

Enable DMA support for counters.

Returns

  • status 0 if successful, else error-code as follow SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer.

    • SL_STATUS_OK (0x0000) - Success, OCU mode control params are set properly.


sl_si91x_config_timer_set_wfg_configuration#

sl_status_t sl_si91x_config_timer_set_wfg_configuration (sl_config_timer_wfg_config_t * wfg_config_ptr)

Set Config-timer WFG mode configurations Such as select toggle high, low and peak for counter-0 & counter-1 outputs.

Parameters
TypeDirectionArgument NameDescription
sl_config_timer_wfg_config_t *[in]wfg_config_ptr

Pointer to CT wfg-config structure sl_config_timer_wfg_config_t

Returns

  • status 0 if successful, else error-code as follow SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer.

    • SL_STATUS_OK (0x0000) - Success, WFG mode configurations are set properly.


sl_si91x_config_timer_set_initial_count#

sl_status_t sl_si91x_config_timer_set_initial_count (sl_config_timer_mode_t mode, uint32_t counter0_initial_value, uint32_t counter1_initial_value)

Set Config-timer initial count as per timer mode.

Parameters
TypeDirectionArgument NameDescription
sl_config_timer_mode_t[in]mode

sl_config_timer_mode_t for possible values

uint32_t[in]counter0_initial_value

(uint16_t)

uint32_t[in]counter1_initial_value

(uint16_t)

For 32-bit mode, counter0_initial_value is passes to count value register For 32-bit mode pass counter1 initial-value as zero For 16-bit mode counters, ored value of both initial value is passed to the register

  • l_si91x_config_timer_set_configuration();

Returns

  • status 0 if successful, else error-code as follow SL_STATUS_INVALID_MODE (0x0024) - 'mode' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Success, initial-count is set properly


sl_si91x_config_timer_set_match_count#

sl_status_t sl_si91x_config_timer_set_match_count (sl_config_timer_mode_t mode, sl_counter_number_t counter_number, uint32_t match_value)

Set Config-timer match-count as per timer mode and counter-number.

Parameters
TypeDirectionArgument NameDescription
sl_config_timer_mode_t[in]mode

sl_counter_number_t for possible values

sl_counter_number_t[in]counter_number

sl_config_timer_mode_t for possible values

uint32_t[in]match_value

(uint32_t)

If mode is 32-bit, use counter0 If mode is 16-bit as per passed counter number it updates the match value For 16-bit mode it takes 16-bit match-value only, else through error

  • l_si91x_config_timer_set_configuration();

Returns

  • status 0 if successful, else error-code as follow SL_STATUS_INVALID_MODE (0x0024) - 'mode' parameter value is invalid.

    • SL_STATUS_INVALID_PARAMETER 0x0021) - 'counter_number' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Success, match-value is set properly


sl_si91x_config_timer_get_count#

sl_status_t sl_si91x_config_timer_get_count (sl_config_timer_mode_t mode, sl_counter_number_t counter_number, uint32_t * count_value)

Get Config-timer current count as per timer mode and counter-number.

Parameters
TypeDirectionArgument NameDescription
sl_config_timer_mode_t[in]mode

sl_counter_number_t for possible values

sl_counter_number_t[in]counter_number

sl_config_timer_mode_t for possible values

uint32_t *[in]count_value

*(uint32_t), pointer to the variable to store count value

Updates the count value to count_value variable input parameter.

  • l_si91x_config_timer_set_configuration();

Returns

  • status 0 if successful, else errorcode SL_STATUS_INVALID_MODE (0x0024) - 'mode' parameter value is invalid.

    • SL_STATUS_INVALID_PARAMETER 0x0021) - 'counter_number' parameter value is invalid.

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter 'count_value' is null pointer.

    • SL_STATUS_OK (0x0000) - Success, count-value is read properly


sl_si91x_config_timer_reset_counter#

sl_status_t sl_si91x_config_timer_reset_counter (sl_counter_number_t counter_number)

Resets Config-timer counter register value.

Parameters
TypeDirectionArgument NameDescription
sl_counter_number_t[in]counter_number

sl_counter_number_t for possible values

Resets the Count values of selected counter.

  • l_si91x_config_timer_set_configuration();

Returns

  • status 0 if successful, else error-code as follow SL_STATUS_INVALID_PARAMETER 0x0021) - 'counter_number' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Success, counter resets properly


sl_si91x_config_timer_start_on_software_trigger#

sl_status_t sl_si91x_config_timer_start_on_software_trigger (sl_counter_number_t counter_number)

Starts selected config-timer counter.

Parameters
TypeDirectionArgument NameDescription
sl_counter_number_t[in]counter_number

sl_counter_number_t for possible values

Starts the counter by enabling counter trigger

  • l_si91x_config_timer_set_configuration(),keep software trigger disable here

Returns

  • status 0 if successful, else error-code as follow SL_STATUS_INVALID_PARAMETER 0x0021) - 'counter_number' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Success, timer started properly


sl_si91x_config_timer_select_action_event#

sl_status_t sl_si91x_config_timer_select_action_event (sl_config_timer_action_t action, sl_config_timer_event_t select_event_counter0, sl_config_timer_event_t select_event_counter1)

Selects config timer input events for triggering selected timer-actions.

Parameters
TypeDirectionArgument NameDescription
sl_config_timer_action_t[in]action

sl_config_timer_action_t for possible values

sl_config_timer_event_t[in]select_event_counter0

sl_config_timer_event_t for possible values, (selects input event for triggering counter-0 action )

sl_config_timer_event_t[in]select_event_counter1

sl_config_timer_event_t for possible values, (selects input event for triggering counter-1 action )

Different timer actions are start, stop, continue, halt, increment, capture, interrupt and output.

Returns

  • status 0 if successful, else error-code as follow SL_STATUS_INVALID_PARAMETER 0x0021) - Selected input event or action parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Success, input event is set properly


sl_si91x_config_timer_configure_action_event#

sl_status_t sl_si91x_config_timer_configure_action_event (sl_config_action_event_t * event_config_handle)

Configure config timer input-event's AND-event and OR-event for triggering selected timer-action.

Parameters
TypeDirectionArgument NameDescription
sl_config_action_event_t *[in]event_config_handle

Pointer to CT configure action events structure sl_config_action_event_t

Different timer actions are start, stop, continue, halt, increment, capture, interrupt and output.

Returns

  • status 0 if successful, else error-code as follow SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer.

    • SL_STATUS_INVALID_PARAMETER 0x0021) - and-event or or-event or event-valid-bits value is invalid.

    • SL_STATUS_OK (0x0000) - Success, AND event & OR event set properly


sl_si91x_config_timer_register_callback#

sl_status_t sl_si91x_config_timer_register_callback (sl_config_timer_callback_t on_config_timer_callback, void * callback_flag_value, sl_config_timer_interrupt_flags_t * interrupt_flags)

Register callback of config timer interrupts.

Parameters
TypeDirectionArgument NameDescription
sl_config_timer_callback_t[in]on_config_timer_callback

(function pointer) Callback function pointer to be called when timer interrupt occurred sl_config_timer_callback_t

void *[in]callback_flag_value

(void *) pointer to interrupt flag value variable sl_config_timer_callback_t

sl_config_timer_interrupt_flags_t *[in]interrupt_flags

pointer to interrupt flags structure sl_config_timer_interrupt_flags_t

Enabling respective interrupts as per selected interrupt flag.

Returns

  • status 0 if successful, else error-code as follow SL_STATUS_NULL_POINTER (0x0022) - parameter is a null pointer.

    • SL_STATUS_BUSY (0x0004) - The callback is already registered, unregister previous callback before registering new one.

    • SL_STATUS_OK (0x0000) - Successfully registered timer timer-out callback.


sl_si91x_config_timer_unregister_callback#

sl_status_t sl_si91x_config_timer_unregister_callback (sl_config_timer_interrupt_flags_t * interrupt_flags)

Unregisters timer interrupt callback Disables interrupts as per selected interrupt flag.

Parameters
TypeDirectionArgument NameDescription
sl_config_timer_interrupt_flags_t *[in]interrupt_flags

pointer to interrupt flags structure sl_config_timer_interrupt_flags_t

Returns

  • status 0 if successful, else error-code as follow SL_STATUS_NULL_POINTER (0x0022) - parameter is a null pointer.

    • SL_STATUS_OK (0x0000) - Successfully unregistered timer interrupt callback.


sl_si91x_config_timer_resume_halt_event#

sl_status_t sl_si91x_config_timer_resume_halt_event (sl_counter_number_t counter_number)

Resume halt operation of Config-timer counter.

Parameters
TypeDirectionArgument NameDescription
sl_counter_number_t[in]counter_number

sl_counter_number_t for possible values

Counter will start running from the count where it was halted previously.

Returns

  • status 0 if successful, else error-code as follow SL_STATUS_INVALID_PARAMETER 0x0021) - 'counter_number' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Success, halt operation resumed properly


sl_si91x_config_timer_read_capture#

sl_status_t sl_si91x_config_timer_read_capture (sl_counter_number_t counter_number, uint16_t * capture_value)

Gets Config-timer count value when capture occurs Updates the capture count value of timer to capture_value variable input parameter.

Parameters
TypeDirectionArgument NameDescription
sl_counter_number_t[in]counter_number

sl_counter_number_t for possible values

uint16_t *[in]capture_value

(uint16_t*), pointer to the variable to store count value at capture event.

Returns

  • status 0 if successful, else error-code as follow SL_STATUS_NULL_POINTER (0x0022) - The parameter 'capture_value' is null pointer.

    • SL_STATUS_INVALID_PARAMETER 0x0021) - 'counter_number' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Success, capture count-value is read properly


sl_si91x_config_timer_set_counter_sync#

sl_status_t sl_si91x_config_timer_set_counter_sync (sl_counter_number_t counter_number, uint8_t sync_counter_value)

Sync counter output with other channels, as per sync_counter_value.

Parameters
TypeDirectionArgument NameDescription
sl_counter_number_t[in]counter_number

sl_counter_number_t for possible values

uint8_t[in]sync_counter_value

(uint8_t)

  • l_si91x_config_timer_set_configuration();

Returns

  • status 0 if successful, else error-code as follow SL_STATUS_INVALID_PARAMETER 0x0021) - 'counter_number' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Success, counter output synced properly


sl_si91x_config_timer_set_output_adc_pin#

sl_status_t sl_si91x_config_timer_set_output_adc_pin (uint8_t pin1, uint8_t pin2)

This API is used to configure config timer output events for ADC trigger Configures input events for counter0 and counter1 outputs to trigger ADC.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]pin1

Counter0 output event for ADC trigger (0 to 31) sl_config_timer_event_t

uint8_t[in]pin2

Counter1 output event for ADC trigger (0 to 31) sl_config_timer_event_t

  • l_si91x_config_timer_set_configuration();

Returns

  • status 0 if successful, else error-code as follow SL_STATUS_INVALID_PARAMETER 0x0021) - 'pin_1' or 'pin_2' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Success, ADC trigger events set properly


sl_si91x_config_timer_set_wfg_compare_values#

sl_status_t sl_si91x_config_timer_set_wfg_compare_values (sl_counter_number_t counter_number, sl_config_timer_ocu_params_t * ocu_params)
Parameters
TypeDirectionArgument NameDescription
sl_counter_number_tN/Acounter_number
sl_config_timer_ocu_params_t *N/Aocu_params

sl_si91x_config_timer_deinit#

void sl_si91x_config_timer_deinit (void )

De-initialize config-timer by disabling its clock.

Parameters
TypeDirectionArgument NameDescription
void[in]

Returns

  • none

Note

  • Unregisters the callback and disables all config timer interrupts.


sl_si91x_config_timer_get_version#

sl_config_timer_version_t sl_si91x_config_timer_get_version (void )

Gets Config timer version It returns API version of Config timer.

Parameters
TypeDirectionArgument NameDescription
void[in]

Returns

  • (sl_config_version_t) type structure


Macro Definition Documentation#

CT#

#define CT
Value:
CT0

pointer to CT base address