Serial Input-Output#

Modules#

sl_sio_version_t

sl_sio_spi_t

sl_sio_uart_t

sl_sio_i2c_t

Enumerations#

enum
SL_SIO_SPI_TX_DONE
SL_SIO_SPI_RX_DONE
}

SIO-SPI Events.

enum
SL_SIO_UART_TX_DONE
SL_SIO_UART_RX_DONE
SL_SIO_UART_PARITY_ERR
SL_SIO_UART_FRAMING_ERR
SL_SIO_UART_RECEIVE_CHAR
}

SIO-UART Events.

enum
SL_SIO_SPI_MODE_0 = 0
SL_SIO_SPI_MODE_3 = 3
}

SIO-SPI modes configurations.

enum
SL_SIO_SPI_BIT_8 = 8
SL_SIO_SPI_BIT_16 = 16
}

SIO-SPI bit width configurations.

enum
SL_SIO_SPI_LSB_FIRST = 0
SL_SIO_SPI_MSB_FIRST = 1
}

SIO-SPI MSB/LSB first configurations.

enum
SL_SIO_UART_BIT_8 = 8
SL_SIO_UART_BIT_16 = 16
}

SIO-UART bit length configurations.

enum
SL_SIO_UART_EVEN_PARITY = 0
SL_SIO_UART_ODD_PARITY = 1
}

SIO-UART parity configurations.

enum
SL_SIO_UART_STOP_BIT_1 = 1
SL_SIO_UART_STOP_BIT_2 = 2
}

SIO-UART stop bit configurations.

Typedefs#

typedef stc_sio_spi_cfg_t

SIO-SPI configuration structure.

typedef stc_sio_spi_xfer_t

SIO-SPI Transfer structure.

typedef stc_sio_i2s_config_t

SIO-I2S configuration structure.

typedef stc_sio_i2s_xfer_t

SIO-I2S Transfer structure.

typedef stc_sio_uart_config_t

SIO-UART configuration structure.

typedef sio_i2s_func_ptr_t

SIO-I2S callback function pointer.

typedef sio_Spi_func_ptr_t

SIO-SPI callback function pointer.

typedef sio_Uart_func_ptr_t

SIO_UART callback function pointer.

typedef stc_sio_i2c_config_t

SIO-I2C configuration structure.

Functions#

sl_status_t

Initialize the SIO module.

sl_status_t
sl_si91x_sio_spi_init(sl_sio_spi_config_t *configuration)

Initialize the SIO-SPI module.

void

This API is used to De-initialize SIO module.

sl_status_t
sl_si91x_sio_spi_pin_initialization(sl_sio_spi_t *sio_spi_init)

Initialize SIO SPI pins and clock.

sl_status_t
sl_si91x_sio_uart_pin_initialization(sl_sio_uart_t *sio_uart_init)

Initialize SIO UART pins and clock.

sl_status_t
sl_si91x_sio_i2c_pin_initialization(sl_sio_i2c_t *sio_i2c_init)

Initialize SIO I2C pins and clock.

sl_status_t
sl_si91x_sio_spi_cs_assert(uint8_t chip_select_num)

Assert the SIO SPI chip select.

sl_status_t
sl_si91x_sio_spi_cs_deassert(uint8_t chip_select_num)

De-assert the SIO SPI chip select.

sl_status_t
sl_si91x_sio_spi_register_event_callback(sl_sio_spi_callback_t callback_event)

Register the user callback function.

void

Un-register the user callback function, i.e., clear the callback function address and disables IRQ handler.

sl_status_t
sl_si91x_sio_spi_transfer(sl_sio_spi_xfer_config_t *xfer_config)

Transfer the SIO SPI data.

Get the SIO version.

sl_status_t
sl_si91x_sio_uart_init(sl_sio_uart_config_t *configuration)

Initialize SIO-UART, i.e., set baud rate, parity, channel selection, stop bits, and data length.

sl_status_t
sl_si91x_sio_uart_send(const void *buffer, uint16_t length)

Send the data over SIO-UART in non-blocking mode.

sl_status_t
sl_si91x_sio_uart_send_blocking(const void *buffer, uint16_t length)

Send the data over SIO-UART in blocking mode.

sl_status_t
sl_si91x_sio_uart_read(void *data_buffer, uint16_t num_bytes)

Read data from SIO-UART in non-blocking mode.

sl_status_t
sl_si91x_sio_uart_read_blocking(void *data_buffer, uint16_t num_bytes)

Read data from UART in blocking mode.

sl_status_t
sl_si91x_sio_uart_register_event_callback(sl_sio_uart_callback_t callback_event)

Register the user callback function.

sl_status_t
sl_si91x_sio_i2c_write(stc_sio_i2c_config_t *configuration, uint8_t address, uint8_t *data, uint16_t length)

Write data using SIO-I2C.

sl_status_t
sl_si91x_sio_i2c_read(stc_sio_i2c_config_t *configuration, uint8_t address, uint8_t *data, uint16_t length)

Read data using SIO-I2C.

sl_status_t
sl_si91x_sio_i2c_transfer(stc_sio_i2c_config_t *configuration, uint8_t address, uint8_t *tx_buffer, uint16_t tx_length, uint8_t *rx_buffer, uint16_t rx_length)

Transfer data using SIO-I2C.

void

Generate I2C start in SIO.

void

Generate I2C stop in SIO.

void

Un-register the user callback function.

void

Used when UART receive is done.

sl_status_t
sl_si91x_sio_configure_interrupt(en_sio_channels_t channel, interrupt_flag_t flag)

Configure pin detection mode to be considered for GPIO interrupt.

sl_status_t
sl_si91x_sio_match_pattern(en_sio_channels_t channel, pattern_match_t pattern, uint8_t slice, uint32_t slice_pattern)

Match the pattern with data to be detected.

sl_status_t
sl_si91x_sio_shift_clock(uint32_t divider, en_sio_channels_t channel)

Generate the shift clock.

sl_status_t
sl_si91x_sio_select_clock(en_sio_channels_t channel, clock_type_t clock)

Select SIO peripheral clock.

sl_status_t
sl_si91x_sio_position_counter(en_sio_channels_t channel, uint32_t data_shift)

Shift the number of bits.

sl_status_t
sl_si91x_sio_control_flow(en_sio_channels_t channel, flow_control_t flow_control)

Enable/disable the flow control bit.

sl_status_t
sl_si91x_sio_reverse_load(en_sio_channels_t channel, reverse_load_t reverse)

Load data to buffer in reverse order.

sl_status_t
sl_si91x_sio_set_interrupt(en_sio_channels_t channel)

Enable the common swap interrupt.

sl_status_t
sl_si91x_sio_clear_interrupt(en_sio_channels_t channel)

Disable the common swap interrupt.

sl_status_t
sl_si91x_sio_mask_interrupt(en_sio_channels_t channel)

Mask the common swap interrupt.

sl_status_t
sl_si91x_sio_unmask_interrupt(en_sio_channels_t channel)

Unmask the common swap interrupt.

uint32_t

Read the common swap interrupt status.

sl_status_t
sl_si91x_sio_set_shift_interrupt(en_sio_channels_t channel)

Enable the common shift interrupt.

sl_status_t
sl_si91x_sio_clear_shift_interrupt(en_sio_channels_t channel)

Disable the common shift interrupt.

sl_status_t
sl_si91x_sio_mask_shift_interrupt(en_sio_channels_t channel)

Mask the common shift interrupt.

sl_status_t
sl_si91x_sio_unmask_shift_interrupt(en_sio_channels_t channel)

Unmask the common shift interrupt.

uint32_t

Read the common shift interrupt status.

sl_status_t
sl_si91x_sio_edge_select(en_sio_channels_t channel, edge_select_t edge_sel)

Select edge of the clock cycle for sampling bits.

uint32_t
sl_si91x_sio_read_buffer(en_sio_channels_t channel)

Read SIO buffer register.

sl_status_t
sl_si91x_sio_write_buffer(en_sio_channels_t channel, uint32_t data)

Write into SIO buffer register.

Macros#

#define

SIO-SPI channel 0.

#define

SIO-SPI channel 1.

#define

SIO-SPI channel 2.

#define

SIO-SPI channel 3.

#define

SIO-SPI channel 4.

#define

SIO-SPI channel 5.

#define

SIO-SPI channel 6.

#define

SIO-SPI channel 7.

Enumeration Documentation#

sl_sio_spi_event_t#

sl_sio_spi_event_t

SIO-SPI Events.

Enumerator
SL_SIO_SPI_TX_DONE

SIO-SPI Transfer done event.

SL_SIO_SPI_RX_DONE

SIO-SPI Receive done event.


sl_sio_uart_event_t#

sl_sio_uart_event_t

SIO-UART Events.

Enumerator
SL_SIO_UART_TX_DONE

SIO-UART transfer done event.

SL_SIO_UART_RX_DONE

SIO-UART receive done event.

SL_SIO_UART_PARITY_ERR

SIO-UART parity error.

SL_SIO_UART_FRAMING_ERR

SIO-UART framing error.

SL_SIO_UART_RECEIVE_CHAR

SIO-UART receive character.


sl_sio_spi_mode_t#

sl_sio_spi_mode_t

SIO-SPI modes configurations.

Enumerator
SL_SIO_SPI_MODE_0

SIO-SPI mode 0.

SL_SIO_SPI_MODE_3

SIO-SPI mode 3.


sl_sio_spi_bit_width_t#

sl_sio_spi_bit_width_t

SIO-SPI bit width configurations.

Enumerator
SL_SIO_SPI_BIT_8

SIO-SPI bit width 8.

SL_SIO_SPI_BIT_16

SIO-SPI bit width 16.


sl_sio_spi_msb_lsb_t#

sl_sio_spi_msb_lsb_t

SIO-SPI MSB/LSB first configurations.

Enumerator
SL_SIO_SPI_LSB_FIRST

SIO-SPI LSB first.

SL_SIO_SPI_MSB_FIRST

SIO-SPI MSB first.


sl_sio_spi_bit_length_t#

sl_sio_spi_bit_length_t

SIO-UART bit length configurations.

Enumerator
SL_SIO_UART_BIT_8

SIO-SPI bit length 8.

SL_SIO_UART_BIT_16

SIO-SPI bit length 16.


sl_sio_spi_parity_t#

sl_sio_spi_parity_t

SIO-UART parity configurations.

Enumerator
SL_SIO_UART_EVEN_PARITY

SIO-SPI even parity.

SL_SIO_UART_ODD_PARITY

SIO-SPI odd parity.


sl_sio_spi_stop_bit_t#

sl_sio_spi_stop_bit_t

SIO-UART stop bit configurations.

Enumerator
SL_SIO_UART_STOP_BIT_1

SIO-UART stop bit 1.

SL_SIO_UART_STOP_BIT_2

SIO-UART stop bit 2.


Typedef Documentation#

sl_sio_spi_config_t#

typedef stc_sio_spi_cfg_t sl_sio_spi_config_t

SIO-SPI configuration structure.


sl_sio_spi_xfer_config_t#

typedef stc_sio_spi_xfer_t sl_sio_spi_xfer_config_t

SIO-SPI Transfer structure.


sl_sio_i2s_config_t#

typedef stc_sio_i2s_config_t sl_sio_i2s_config_t

SIO-I2S configuration structure.


sl_sio_i2s_xfer_config_t#

typedef stc_sio_i2s_xfer_t sl_sio_i2s_xfer_config_t

SIO-I2S Transfer structure.


sl_sio_uart_config_t#

typedef stc_sio_uart_config_t sl_sio_uart_config_t

SIO-UART configuration structure.


sl_sio_i2s_callback_t#

typedef sio_i2s_func_ptr_t sl_sio_i2s_callback_t

SIO-I2S callback function pointer.


sl_sio_spi_callback_t#

typedef sio_Spi_func_ptr_t sl_sio_spi_callback_t

SIO-SPI callback function pointer.


sl_sio_uart_callback_t#

typedef sio_Uart_func_ptr_t sl_sio_uart_callback_t

SIO_UART callback function pointer.


sl_sio_i2c_config_t#

typedef stc_sio_i2c_config_t sl_sio_i2c_config_t

SIO-I2C configuration structure.


Function Documentation#

sl_si91x_sio_init#

sl_status_t sl_si91x_sio_init (void )

Initialize the SIO module.

Parameters
TypeDirectionArgument NameDescription
void[in]

It initializes the SIO GPIO's and enables the SIO module clock. Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_FAIL (0x0001) - Fail, SIO initialization failed

    • SL_STATUS_OK (0x0000) - Success, SIO initialization successful


sl_si91x_sio_spi_init#

sl_status_t sl_si91x_sio_spi_init (sl_sio_spi_config_t * configuration)

Initialize the SIO-SPI module.

Parameters
TypeDirectionArgument NameDescription
sl_sio_spi_config_t *[in]configuration

- Pointer to SIO-SPI configuration structure sl_sio_spi_config_t

It configures the SPI mode, bit length, bit order, SIO frequency, and the SIO channels for the SPI transfer lines.

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_OK (0x0000) - Success, SPI initialization done properly


sl_si91x_sio_deinit#

void sl_si91x_sio_deinit (void )

This API is used to De-initialize SIO module.

Parameters
TypeDirectionArgument NameDescription
void[in]

Returns

  • none


sl_si91x_sio_spi_pin_initialization#

sl_status_t sl_si91x_sio_spi_pin_initialization (sl_sio_spi_t * sio_spi_init)

Initialize SIO SPI pins and clock.

Parameters
TypeDirectionArgument NameDescription
sl_sio_spi_t *[in]sio_spi_init

: Pointer to the structure of type sl_sio_spi_t

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_OK - Success

    • SL_STATUS_NULL_POINTER - The parameter is a null pointer


sl_si91x_sio_uart_pin_initialization#

sl_status_t sl_si91x_sio_uart_pin_initialization (sl_sio_uart_t * sio_uart_init)

Initialize SIO UART pins and clock.

Parameters
TypeDirectionArgument NameDescription
sl_sio_uart_t *[in]sio_uart_init

: Pointer to the structure of type sl_sio_uart_t

This holds the UART Tx, Rx pins configuration. Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_OK - Success

    • SL_STATUS_NULL_POINTER - The parameter is a null pointer


sl_si91x_sio_i2c_pin_initialization#

sl_status_t sl_si91x_sio_i2c_pin_initialization (sl_sio_i2c_t * sio_i2c_init)

Initialize SIO I2C pins and clock.

Parameters
TypeDirectionArgument NameDescription
sl_sio_i2c_t *[in]sio_i2c_init

: Pointer to the structure of type sl_sio_i2c_t

This holds the I2C SDA, SCL pins configuration. Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_OK - Success

    • SL_STATUS_NULL_POINTER - The parameter is a null pointer


sl_si91x_sio_spi_cs_assert#

sl_status_t sl_si91x_sio_spi_cs_assert (uint8_t chip_select_num)

Assert the SIO SPI chip select.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]chip_select_num

- Chip select number (0 to 7)

This tells peripheral that it should wake up and receive / send data and is also used when multiple peripherals are present to select the one you'd like to communicate with.

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_OK (0x0000) - Success


sl_si91x_sio_spi_cs_deassert#

sl_status_t sl_si91x_sio_spi_cs_deassert (uint8_t chip_select_num)

De-assert the SIO SPI chip select.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]chip_select_num

- Chip select number (0 to 7)

This is used to disable after the last byte is transmitted / received.

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_OK (0x0000) - Success


sl_si91x_sio_spi_register_event_callback#

sl_status_t sl_si91x_sio_spi_register_event_callback (sl_sio_spi_callback_t callback_event)

Register the user callback function.

Parameters
TypeDirectionArgument NameDescription
sl_sio_spi_callback_t[in]callback_event

- Pointer to the function sl_sio_spi_callback_t which needs to be called at the time of interrupt.

It registers the callback, i.e., stores the callback function address and pass to the variable that is called in Interrupt Handler. If another callback is registered without unregistering previous callback then, it returns an error code, so it is mandatory to unregister the callback before registering another callback. It will returns error if any callback is already registered.

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_BUSY (0x0004) - Driver is busy


sl_si91x_sio_spi_unregister_event_callback#

void sl_si91x_sio_spi_unregister_event_callback (void )

Un-register the user callback function, i.e., clear the callback function address and disables IRQ handler.

Parameters
TypeDirectionArgument NameDescription
void[in]

Returns

  • none


sl_si91x_sio_spi_transfer#

sl_status_t sl_si91x_sio_spi_transfer (sl_sio_spi_xfer_config_t * xfer_config)

Transfer the SIO SPI data.

Parameters
TypeDirectionArgument NameDescription
sl_sio_spi_xfer_config_t *[in]xfer_config

- Pointer to SIO-SPI transfer configuration structure sl_sio_spi_xfer_config_t

It is used to make the SIO-SPI transfer in non-blocking mode.

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_OK (0x0000) - Success


sl_si91x_sio_get_version#

sl_sio_version_t sl_si91x_sio_get_version (void )

Get the SIO version.

Parameters
TypeDirectionArgument NameDescription
void[in]

It is used to get the release, SQA and DEV version of the SIO module. Returns


sl_si91x_sio_uart_init#

sl_status_t sl_si91x_sio_uart_init (sl_sio_uart_config_t * configuration)

Initialize SIO-UART, i.e., set baud rate, parity, channel selection, stop bits, and data length.

Parameters
TypeDirectionArgument NameDescription
sl_sio_uart_config_t *[in]configuration

- Pointer to SIO-UART configuration structure sl_sio_uart_config_t

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_OK (0x0000) - Success, UART initialization done properly


sl_si91x_sio_uart_send#

sl_status_t sl_si91x_sio_uart_send (const void * buffer, uint16_t length)

Send the data over SIO-UART in non-blocking mode.

Parameters
TypeDirectionArgument NameDescription
const void *[in]buffer

- data pointer to send

uint16_t[in]length

- data length

Transmit bytes from the buffer using an interrupt service. Will return immediately, but cannot be called again until the previous call has finished.

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_OK (0x0000) - Success


sl_si91x_sio_uart_send_blocking#

sl_status_t sl_si91x_sio_uart_send_blocking (const void * buffer, uint16_t length)

Send the data over SIO-UART in blocking mode.

Parameters
TypeDirectionArgument NameDescription
const void *[in]buffer

- data pointer to send

uint16_t[in]length

- number of bytes to send

Transmit bytes from the buffer using a blocking send byte function. Does not return until all bytes are sent.

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_OK (0x0000) - Success


sl_si91x_sio_uart_read#

sl_status_t sl_si91x_sio_uart_read (void * data_buffer, uint16_t num_bytes)

Read data from SIO-UART in non-blocking mode.

Parameters
TypeDirectionArgument NameDescription
void *[out]data_buffer

- data buffer pointer to read

uint16_t[in]num_bytes

- number of bytes read

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_OK (0x0000) - Success


sl_si91x_sio_uart_read_blocking#

sl_status_t sl_si91x_sio_uart_read_blocking (void * data_buffer, uint16_t num_bytes)

Read data from UART in blocking mode.

Parameters
TypeDirectionArgument NameDescription
void *[out]data_buffer

- data buffer pointer to read

uint16_t[in]num_bytes

- number of bytes read

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_OK (0x0000) - Success


sl_si91x_sio_uart_register_event_callback#

sl_status_t sl_si91x_sio_uart_register_event_callback (sl_sio_uart_callback_t callback_event)

Register the user callback function.

Parameters
TypeDirectionArgument NameDescription
sl_sio_uart_callback_t[in]callback_event

- Pointer to the function sl_sio_uart_callback_t which needs to be called at the time of interrupt.

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_BUSY (0x0004) - Driver is busy


sl_si91x_sio_i2c_write#

sl_status_t sl_si91x_sio_i2c_write (stc_sio_i2c_config_t * configuration, uint8_t address, uint8_t * data, uint16_t length)

Write data using SIO-I2C.

Parameters
TypeDirectionArgument NameDescription
stc_sio_i2c_config_t *[in]configuration

- pointer to the I2C configuration structure stc_sio_i2c_config_t in SIO module

uint8_t[in]address

- slave address

uint8_t *[in]data

- pointer to the data

uint16_t[in]length

- data length

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_i2c_read#

sl_status_t sl_si91x_sio_i2c_read (stc_sio_i2c_config_t * configuration, uint8_t address, uint8_t * data, uint16_t length)

Read data using SIO-I2C.

Parameters
TypeDirectionArgument NameDescription
stc_sio_i2c_config_t *[in]configuration

- pointer to the I2C configuration structure stc_sio_i2c_config_t in SIO module

uint8_t[in]address

- slave address

uint8_t *[out]data

- pointer to the data

uint16_t[in]length

- data length

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_i2c_transfer#

sl_status_t sl_si91x_sio_i2c_transfer (stc_sio_i2c_config_t * configuration, uint8_t address, uint8_t * tx_buffer, uint16_t tx_length, uint8_t * rx_buffer, uint16_t rx_length)

Transfer data using SIO-I2C.

Parameters
TypeDirectionArgument NameDescription
stc_sio_i2c_config_t *[in]configuration

- Pointer to the I2C configuration structure stc_sio_i2c_config_t in SIO module

uint8_t[in]address

- Slave address

uint8_t *[in]tx_buffer

- Pointer to the data transmit buffer

uint16_t[in]tx_length

- TX data length

uint8_t *[out]rx_buffer

- Pointer to the data receive buffer

uint16_t[in]rx_length

- RX data length

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_i2c_generate_start#

void sl_si91x_sio_i2c_generate_start (void )

Generate I2C start in SIO.

Parameters
TypeDirectionArgument NameDescription
void[in]

Returns

  • none


sl_si91x_sio_i2c_generate_stop#

void sl_si91x_sio_i2c_generate_stop (void )

Generate I2C stop in SIO.

Parameters
TypeDirectionArgument NameDescription
void[in]

Returns

  • none


sl_si91x_sio_uart_unregister_event_callback#

void sl_si91x_sio_uart_unregister_event_callback (void )

Un-register the user callback function.

Parameters
TypeDirectionArgument NameDescription
void[in]

Returns

  • none


sl_si91x_sio_uart_rx_done#

void sl_si91x_sio_uart_rx_done (void )

Used when UART receive is done.

Parameters
TypeDirectionArgument NameDescription
void[in]

Returns

  • none


sl_si91x_sio_configure_interrupt#

sl_status_t sl_si91x_sio_configure_interrupt (en_sio_channels_t channel, interrupt_flag_t flag)

Configure pin detection mode to be considered for GPIO interrupt.

Parameters
TypeDirectionArgument NameDescription
en_sio_channels_t[in]channel

- SIO channel to be selected en_sio_channels_t

interrupt_flag_t[in]flag

- GPIO interrupt generated interrupt_flag_t

  • Rise edge: 0

  • Fall edge: 1

  • Level 0: 2

  • Level 1: 3

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_match_pattern#

sl_status_t sl_si91x_sio_match_pattern (en_sio_channels_t channel, pattern_match_t pattern, uint8_t slice, uint32_t slice_pattern)

Match the pattern with data to be detected.

Parameters
TypeDirectionArgument NameDescription
en_sio_channels_t[in]channel

- SIO channel to be selected en_sio_channels_t

pattern_match_t[in]pattern

- Pattern match bit to be enabled for pattern match to take place pattern_match_t

  • Pattern match disable: 0

  • Pattern match enable: 1

uint8_t[in]slice

- Slice number (0,1,2,8,9,10) to select

uint32_t[in]slice_pattern

- Pattern to match for selected slice

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_shift_clock#

sl_status_t sl_si91x_sio_shift_clock (uint32_t divider, en_sio_channels_t channel)

Generate the shift clock.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]divider

- Desired clock frequency configuration

en_sio_channels_t[in]channel

- SIO channel to be selected en_sio_channels_t

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_select_clock#

sl_status_t sl_si91x_sio_select_clock (en_sio_channels_t channel, clock_type_t clock)

Select SIO peripheral clock.

Parameters
TypeDirectionArgument NameDescription
en_sio_channels_t[in]channel

- SIO channel to be selected en_sio_channels_t

clock_type_t[in]clock

- Clock used for shift operations clock_type_t

  • Internal clock: 0

  • External clock: 1

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_position_counter#

sl_status_t sl_si91x_sio_position_counter (en_sio_channels_t channel, uint32_t data_shift)

Shift the number of bits.

Parameters
TypeDirectionArgument NameDescription
en_sio_channels_t[in]channel

- SIO channel to be selected en_sio_channels_t

uint32_t[in]data_shift

- Number of shifts to happen before reloading register with data. Value to be set = (total no. of valid bits in shift register/ no. of bits per shift) - 1

Number of shifts to happen before reloading the shift register with data/pausing the operation. i.e. value to be set = (total no. of valid bits in shift register/ number of bits per shift) – 1

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_control_flow#

sl_status_t sl_si91x_sio_control_flow (en_sio_channels_t channel, flow_control_t flow_control)

Enable/disable the flow control bit.

Parameters
TypeDirectionArgument NameDescription
en_sio_channels_t[in]channel

- SIO channel to be selected en_sio_channels_t

flow_control_t[in]flow_control

- It decides whether to continue data shifting based on data present in shift register validation flow_control_t

  • Flow control disable: 0

  • Flow control enable: 1

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_reverse_load#

sl_status_t sl_si91x_sio_reverse_load (en_sio_channels_t channel, reverse_load_t reverse)

Load data to buffer in reverse order.

Parameters
TypeDirectionArgument NameDescription
en_sio_channels_t[in]channel

- SIO channel to be selected en_sio_channels_t

reverse_load_t[in]reverse

- If data to be shifted out MSB first, it is to be set reverse_load_t

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_set_interrupt#

sl_status_t sl_si91x_sio_set_interrupt (en_sio_channels_t channel)

Enable the common swap interrupt.

Parameters
TypeDirectionArgument NameDescription
en_sio_channels_t[in]channel

- SIO channel to be selected en_sio_channels_t

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_clear_interrupt#

sl_status_t sl_si91x_sio_clear_interrupt (en_sio_channels_t channel)

Disable the common swap interrupt.

Parameters
TypeDirectionArgument NameDescription
en_sio_channels_t[in]channel

- SIO channel to be selected en_sio_channels_t

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_mask_interrupt#

sl_status_t sl_si91x_sio_mask_interrupt (en_sio_channels_t channel)

Mask the common swap interrupt.

Parameters
TypeDirectionArgument NameDescription
en_sio_channels_t[in]channel

- SIO channel to be selected en_sio_channels_t

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_unmask_interrupt#

sl_status_t sl_si91x_sio_unmask_interrupt (en_sio_channels_t channel)

Unmask the common swap interrupt.

Parameters
TypeDirectionArgument NameDescription
en_sio_channels_t[in]channel

- SIO channel to be selected en_sio_channels_t

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_get_interrupt_status#

uint32_t sl_si91x_sio_get_interrupt_status (void )

Read the common swap interrupt status.

Parameters
TypeDirectionArgument NameDescription
void[in]

Returns

  • returns interrupt status


sl_si91x_sio_set_shift_interrupt#

sl_status_t sl_si91x_sio_set_shift_interrupt (en_sio_channels_t channel)

Enable the common shift interrupt.

Parameters
TypeDirectionArgument NameDescription
en_sio_channels_t[in]channel

- SIO channel to be selected en_sio_channels_t

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_clear_shift_interrupt#

sl_status_t sl_si91x_sio_clear_shift_interrupt (en_sio_channels_t channel)

Disable the common shift interrupt.

Parameters
TypeDirectionArgument NameDescription
en_sio_channels_t[in]channel

- SIO channel to be selected en_sio_channels_t

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_mask_shift_interrupt#

sl_status_t sl_si91x_sio_mask_shift_interrupt (en_sio_channels_t channel)

Mask the common shift interrupt.

Parameters
TypeDirectionArgument NameDescription
en_sio_channels_t[in]channel

- SIO channel to be selected en_sio_channels_t

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_unmask_shift_interrupt#

sl_status_t sl_si91x_sio_unmask_shift_interrupt (en_sio_channels_t channel)

Unmask the common shift interrupt.

Parameters
TypeDirectionArgument NameDescription
en_sio_channels_t[in]channel

- SIO channel to be selected en_sio_channels_t

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_shift_interrupt_status#

uint32_t sl_si91x_sio_shift_interrupt_status (void )

Read the common shift interrupt status.

Parameters
TypeDirectionArgument NameDescription
void[in]

- SIO channel to be selected en_sio_channels_t

Returns

  • returns shift interrupt status


sl_si91x_sio_edge_select#

sl_status_t sl_si91x_sio_edge_select (en_sio_channels_t channel, edge_select_t edge_sel)

Select edge of the clock cycle for sampling bits.

Parameters
TypeDirectionArgument NameDescription
en_sio_channels_t[in]channel

- SIO channel to be selected en_sio_channels_t

edge_select_t[in]edge_sel

- Select the edge for bit sample to start edge_select_t

  • Positive edge: 0

  • Negative edge: 1

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer

    • SL_STATUS_OK (0X000) - Success


sl_si91x_sio_read_buffer#

uint32_t sl_si91x_sio_read_buffer (en_sio_channels_t channel)

Read SIO buffer register.

Parameters
TypeDirectionArgument NameDescription
en_sio_channels_t[in]channel

- SIO channel to be selected en_sio_channels_t

Returns

  • returns data from buffer


sl_si91x_sio_write_buffer#

sl_status_t sl_si91x_sio_write_buffer (en_sio_channels_t channel, uint32_t data)

Write into SIO buffer register.

Parameters
TypeDirectionArgument NameDescription
en_sio_channels_t[in]channel

- SIO channel to be selected en_sio_channels_t

uint32_t[in]data

- Data to be written to buffer

Returns

  • returns status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer

    • SL_STATUS_OK (0X000) - Success


Macro Definition Documentation#

SL_SIO_CH_0#

#define SL_SIO_CH_0
Value:
0

SIO-SPI channel 0.


SL_SIO_CH_1#

#define SL_SIO_CH_1
Value:
1

SIO-SPI channel 1.


SL_SIO_CH_2#

#define SL_SIO_CH_2
Value:
2

SIO-SPI channel 2.


SL_SIO_CH_3#

#define SL_SIO_CH_3
Value:
3

SIO-SPI channel 3.


SL_SIO_CH_4#

#define SL_SIO_CH_4
Value:
4

SIO-SPI channel 4.


SL_SIO_CH_5#

#define SL_SIO_CH_5
Value:
5

SIO-SPI channel 5.


SL_SIO_CH_6#

#define SL_SIO_CH_6
Value:
6

SIO-SPI channel 6.


SL_SIO_CH_7#

#define SL_SIO_CH_7
Value:
7

SIO-SPI channel 7.