BJT Temperature Sensor#
Enumerations#
Functions#
Initialize the BJT temperature sensor.
Read data from the BJT temperature sensor.
Enable or disable the BJT temperature sensor.
Configure the BJT temperature sensor.
Configure band gap for BJT temperature sensor.
Convert the sensor reading to temperature in Celsius/Fahrenheit/Kelvin.
De-initialize the BJT temperature sensor.
Enumeration Documentation#
sl_bjt_temperature_sensor_enum_t#
sl_bjt_temperature_sensor_enum_t
| Enumerator | |
|---|---|
| SL_BJT_DEGREE_CELSIUS | Temperature in degree celsius. |
| SL_BJT_FAHRENHEIT | Temperature in fahrenheit. |
| SL_BJT_KELVIN | Temperature in kelvin. |
sl_bjt_temperature_sensor_state_t#
sl_bjt_temperature_sensor_state_t
| Enumerator | |
|---|---|
| SL_BJT_TEMPERATURE_SENSOR_DISABLE | Temperature sensing disable. |
| SL_BJT_TEMPERATURE_SENSOR_ENABLE | Temperature sensing enable. |
| SL_BJT_TEMPERATURE_SENSOR_LAST | Last member of enum for validation. |
Function Documentation#
sl_si91x_bjt_temperature_sensor_init#
sl_status_t sl_si91x_bjt_temperature_sensor_init (adc_ch_config_t sl_bjt_temperature_sensor_channel_config, adc_config_t sl_bjt_temperature_sensor_config)
Initialize the BJT temperature sensor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| adc_ch_config_t | [in] | sl_bjt_temperature_sensor_channel_config | BJT channels configuration structure channel number, sampling rate and sample length. |
| adc_config_t | [in] | sl_bjt_temperature_sensor_config | BJT configuration sets the operation mode and number of channels. |
Performs ADC initialization and configuration, sets the register callback and starts the ADC.
Returns
Status 0 if successful, else error code:
SL_STATUS_OK (0x0000) - Success
SL_STATUS_FAIL (0x0001) - Fail
SL_STATUS_INVALID_PARAMETER(0x0021) - invalid parameter
SL_STATUS_INVALID_RANGE(0x0028) - invalid range
SL_STATUS_INVALID_COUNT(0x002B) - invalid count
sl_si91x_bjt_temperature_sensor_read_data#
sl_status_t sl_si91x_bjt_temperature_sensor_read_data (double * temp_data)
Read data from the BJT temperature sensor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| double * | [out] | temp_data | Temperature measurement data to convert |
Pre-condition:
Returns
Status 0 if successful, else error code:
SL_STATUS_OK (0x0000) - Success
SL_STATUS_FAIL (0x0001) - Fail
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
SL_STATUS_INVALID_RANGE (0x0028) - Mismatch Range
sl_si91x_bjt_temperature_sensor_state#
sl_status_t sl_si91x_bjt_temperature_sensor_state (sl_bjt_temperature_sensor_state_t state)
Enable or disable the BJT temperature sensor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bjt_temperature_sensor_state_t | [in] | state | Value indicating whether to enable or disable the BJT temperature sensor:
|
Pre-conditions:
Returns
Status 0 if successful, else error code:
SL_STATUS_OK on success
SL_STATUS_INVALID_PARAMETER (0x0021) , The parameter is an invalid argument
sl_si91x_bjt_temperature_sensor_set_channel_configuration#
sl_status_t sl_si91x_bjt_temperature_sensor_set_channel_configuration (adc_ch_config_t sl_bjt_temperature_sensor_channel_config)
Configure the BJT temperature sensor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| adc_ch_config_t | [in] | sl_bjt_temperature_sensor_channel_config | BJT channel configuring positive input to BJT value |
Pre-condition:
Returns
Status 0 if successful, else error code:
SL_STATUS_OK on success
SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
SL_STATUS_INVALID_RANGE (0x0028) - Mismatch Range
sl_si91x_bjt_temperature_sensor_bg_set_channel_configuration#
sl_status_t sl_si91x_bjt_temperature_sensor_bg_set_channel_configuration (adc_ch_config_t sl_bjt_temperature_sensor_channel_config)
Configure band gap for BJT temperature sensor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| adc_ch_config_t | [in] | sl_bjt_temperature_sensor_channel_config | Band gap channel configuring positive input to OPAMP value |
Pre-condition:
Returns
Status 0 if successful, else error code:
SL_STATUS_OK (0x0000) - Success
SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
SL_STATUS_INVALID_RANGE (0x0028) - Mismatch Range
sl_si91x_get_bjt_temperature_sensor_conversion#
sl_status_t sl_si91x_get_bjt_temperature_sensor_conversion (double * temp_data, sl_bjt_temperature_sensor_enum_t current_temperature_mode)
Convert the sensor reading to temperature in Celsius/Fahrenheit/Kelvin.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| double * | [out] | temp_data | Temperature measurement data to convert |
| sl_bjt_temperature_sensor_enum_t | [in] | current_temperature_mode | Current temperature mode |
Returns
Status 0 if successful, else error code:
SL_STATUS_OK (0x0000) - Success
SL_STATUS_FAIL (0x0001) - Fail
SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
sl_si91x_bjt_temperature_sensor_deinit#
sl_status_t sl_si91x_bjt_temperature_sensor_deinit (adc_config_t sl_bjt_temperature_sensor_config)
De-initialize the BJT temperature sensor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| adc_config_t | [in] | sl_bjt_temperature_sensor_config | De-initializing the BJT configuration |
Pre-condition:
Returns
Status 0 if successful, else error code:
SL_STATUS_OK (0x0000) - Success
SL_STATUS_FAIL (0x0001) - Fail