You are viewing documentation for version:
Structure to hold the port and pin of SIO UART. 
Public Attribute Documentation#
uart_tx_port#
uint8_t sl_sio_uart_t::uart_tx_port
SIO UART TX port. 
uart_tx_pin#
uint8_t sl_sio_uart_t::uart_tx_pin
SIO UART TX pin. 
uart_tx_mux#
uint8_t sl_sio_uart_t::uart_tx_mux
SIO UART TX mux. 
uart_tx_pad#
uint8_t sl_sio_uart_t::uart_tx_pad
SIO UART TX pad. 
uart_rx_port#
uint8_t sl_sio_uart_t::uart_rx_port
SIO UART RX port. 
uart_rx_pin#
uint8_t sl_sio_uart_t::uart_rx_pin
SIO UART RX pin. 
uart_rx_mux#
uint8_t sl_sio_uart_t::uart_rx_mux
SIO UART RX mux. 
uart_rx_pad#
uint8_t sl_sio_uart_t::uart_rx_pad
SIO UART RX pad.